Initializing the MxFE Platform Using ACE or DPG Lite

2022-07-27

In this step-by-step tutorial, the initialization process is shown using Analog Devices’ ADS9 high speed carrier card and the AD9082 MxFE® evaluation board. Required hardware connections are overviewed, along with a few extra options depending on use case. The FPGA image associated with the ADS9 board is loaded using the ACE software GUI. Loading using DPG Lite is also shown. Either ACE or DPG Lite can be used to initialize; using both is not required. This process is required before any steps shown in the subsequent videos.

Initializing the MxFE Platform Using ACE or DPG Lite

2022-07-27

In this step-by-step tutorial, the initialization process is shown using Analog Devices’ ADS9 high speed carrier card and the AD9082 MxFE® evaluation board. Required hardware connections are overviewed, along with a few extra options depending on use case. The FPGA image associated with the ADS9 board is loaded using the ACE software GUI. Loading using DPG Lite is also shown. Either ACE or DPG Lite can be used to initialize; using both is not required. This process is required before any steps shown in the subsequent videos.

Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目