Abstract
MAX6650和MAX6651是利用风扇转速反馈控制无刷直流风扇转速的风扇转速调节器,典型应用中,风扇一般采用5V至12V供电。本应用笔记主要介绍如何利用MAX6650和MAX6651控制高压风扇,以24V和48V风扇为例。
MAX6650和MAX6651是工作于5V或12V常规电压的风扇速度控制器,通过产生一个直流电压驱动无刷直流(BLDC)风扇。通过监测风扇的测速信号测量风扇速度,然后调整风扇的驱动电压得到所要求的风扇转速。通常情况下,将正电源接到风扇的供电电源端VFAN (一般为12V或5V),风扇的电源负端则由N沟道MOSFET控制,以调整供电电压。
有些应用需要采用比MAX6650和MAX6651更高供电电压的风扇,当这些IC与高压风扇配合使用时,主要难点在于确保它们输入引脚的驱动电压正确地限定在可接受的工作范围内,这可以通过加入一系列的外部电阻实现。
图1是MAX6651控制12V直流无刷风扇的典型电路(本文以MAX6651电路设计为例,MAX6650的引脚定义完全相同)。OUT驱动外部N沟道MOSFET的栅极,FB输入在MOSFET漏极闭合反馈回路。该电压的变化范围为0V到VFAN (本例中为12V)。风扇转速计通常为漏极开路输出,通过外部电阻上拉到VFAN。TACH0可以接受转速计信号,并根据FB电压调整它的逻辑电平。因此,当风扇转速计输出电压随风扇的驱动电平变化时,这个逻辑电平也会跟着变化。FB和TACH的输入可以接受的最高电压是13.2V,所以VFAN的额定电压可以达到12V。
图1. MAX6651的12V典型工作电路
采用MAX6651控制24V风扇时,可以使用图2电路。与图1相比,唯一的变化是额外增加了两对电阻,用来将TACH0和FB的电压衰减到12V或更低。同样,图3电路可以进一步衰减输入电压,从48V降至12V甚至更低。
图2. 用MAX6651驱动24V风扇
图3. 用MAX6651驱动48V风扇