CN0060: Low Cost Differential Video Receiver Using the ADA4851 Amplifier and the ADV7180 Video Decoder

Engineered. Tested. Ready to Integrate.Learn More

CIRCUIT OVERVIEW

Circuit Note PDF, 10/2010 (pdf, 119 kB)
Benefits & Features
  • Unipolar, Differential Video Receiver
  • Analog Video Decoder
  • Optimized for Composite Video Frequencies
Products Used
    Applications: 
  • Asset Tracking
  • Consumer
  • Infotainment
  • Video Surveillance
Add to Signal Chain Designer Explore in Signal Chain Designer
Design Resources
Connectivity Options
This circuit supports 3rd party connectivity.

CIRCUIT FUNCTION AND BENEFITS

The circuit described in this document and shown in Figure 1 provides a low cost, low power, unipolar, differential receiver using the ADA4851-1 for an incoming video signal before being digitized by the ADV7180 video decoder. This circuit eliminates common-mode noise and phase noise caused by ground potential difference from an incoming video signal and is well suited for automotive infotainment and vision safety systems.

Figure 1. Low Cost Differential Video Receiver Using the ADA4851-1 Simplified Schematic: Decoupling and All Connections Not Shown)

The ADA4851 family of amplifiers along with the ADV7180 video decoder are all automotive qualified which makes both products ideal for auto-vision applications. Low power, low cost, high speed, and fast settling make these amplifiers well suited for many video applications where these requirements are very important. Figure 1 shows only a single amplifier for simplicity; the amplifier circuit can be repeated for each input as many times as needed.

CIRCUIT DESCRIPTION

The ADA4851-1 is a single (also available as a dual or quad amplifier in a single package), 130 MHz, low power, low cost, high speed, voltage feedback, rail-to-rail output amplifier that has an operating supply range of +3 V to +5 V. In Figure 1, the ADA4851-1 is configured as a low cost differential-to-single-ended receiver for video signals.

This configuration is a standard four-resistor difference amplifier optimized for composite video frequencies, with a differential-to-single-ended gain of 1. The amplifier only amplifies the difference between the two inputs, while eliminating the common-mode noise between the incoming signals and allowing the reconstruction of the original signal. Using low value, high accuracy resistors and a high CMRR amplifier provides the exceptional performance.

A critical design consideration that is important to note about this architecture is its dependence on resistor matching for the common-mode rejection (CMR) of this circuit design. The CMR can be calculated using the following formula:

CMR

where KR is a single resistor tolerance in fractional form (for example, 1% = 0.01). It is assumed that the amplifier has significantly higher CMR performance. This formula shows that if 54 dB or better CMR is desired, then R1, R2, R3, and R4 must have a matching tolerance of 0.1% or better.

To prevent the incoming signal from violating the amplifier input and output voltage range, it is necessary to add a dc offset. This is conveniently done by connecting R4 to the 1.8 V analog supply voltage (AVDD_1.8V) also used by the ADV7180, which helps keep the cost low. To prevent supply noise from coupling into the video signal stream, be sure to have adequate bypassing on this supply (AVDD_1.8V), as shown in Figure 1.

Some automotive applications require ac-coupled inputs to protect the input to the amplifier from a short to a voltage higher than its supply voltage. The input impedance of 1 kΩ (R2 and R3) with the 22 μF capacitors (C1 and C2) sets a high-pass corner frequency pole at approximately 7 Hz. If a lower frequency is desired, increasing the capacitor value decreases the corner frequency proportionally. For example, using 47 μF capacitors results in a 3.4 Hz high-pass corner frequency.

A function that is often overlooked but very important is buffering. For example, many automotive customers use low cost amplifiers to protect more expensive and complex devices, such as video decoders and encoders. Amplifiers with ac-coupled inputs, as shown in Figure 1, help protect such devices from overvoltage and ESD damage.

The ADV7180 automatically detects and converts standard analog baseband television signals compatible with worldwide NSTC, PAL, and SECAM standards into 4:2:2 component video data compatible with the 8-bit ITU-R.656 interface standards. The accurate 10-bit analog-to-digital conversion provides professional quality video performance for consumer applications with true 8-bit data resolution. Three analog video input channels accept standard composite, S-Video, or component video signals, supporting a wide range of consumer video sources. AGC and clamp-restore circuitry allow an input video signal peak-to-peak range of up to 1.0 V.

The circuit must be constructed on a multilayer PC board with a large area ground plane. Proper layout, grounding, and decoupling techniques must be used to achieve optimum performance (see MT-031 Tutorial and MT-101 Tutorial).

COMMON VARIATIONS

There are a few options for supplying the dc bias voltage for the ADA4851-1. The ADR12x family of voltage references has a wide range of values that can be used. Another method is to add one more resistor to form a voltage divider in conjunction with R4. Be sure that the parallel combination of R4 and the new R5 matches the value of the RF feedback resistor.

If better CMR performance at high frequencies and higher input impedance are desired, the ADA4851-1 can be replaced with the AD8130 differential line receiver.

SAMPLE PRODUCTS USED IN THIS CIRCUIT

Product Description Available Product Models to Sample
ADA4851-1 Low Cost, High Speed, Rail-to-Rail, Output Op Amp (Single) ADA4851-1YRJZ-RL7 ADA4851-1WYRJZ-R7
ADV7180 10-Bit, 4× Oversampling SDTV Video Decoder ADV7180KST48Z ADV7180WBCP32Z-RL ADV7180BST48Z ADV7180WBSTZ ADV7180KCP32Z ADV7180WBCPZ ADV7180BSTZ ADV7180BCPZ ADV7180WBST48Z ADV7180BCP32Z ADV7180WBCP32Z
content here.
content here.
Send Feedback X
content here.
content here.

Send Feedback

Close