Selecting SPI Clock Modes for Interfacing the MAX1132 ADC with the MAXQ2000 Microcontroller

Feb 17 2023

Figure 1

   

MAX1132 Overview

The MAX1132 is a 200ksps, 16-bit ADC. The MAXQ2000can interface with the MAX1132 in a variety of SPI clock modes: 8-bit, 16-bit, or a combination of both. To maximize the performance of the ADC, it is important to determine which mode to use during early stages of development. It is obvious that a 16-bit ADC with 16 clock frames should use 16-bit mode; however, in a scenario where the ADC uses 24 clock frames, the SPI clock mode must be evaluated closely. This application note provides test results for 8-bit mode, 16-bit mode, and combination mode; the results indicate that combination mode is optimal when the MAX1132 uses 24 clock frames.

Hardware Overview

This application circuit utilizes the MAX1132EVKIT and MAXQ2000-KIT.

Figure 1 presents the MAX1132 EV kit schematic, and Figure 2 illustrates the configuration of the system. To interface the MAX1132 EV kit with the MAXQ2000-KIT, connect SCLK, CS-bar, DOUT, and DIN from the MAX1132 EV kit to the MAXQ2000-KIT, as shown in Figure 2. In addition, a +5V supply is applied on the AVDD and AGND terminals of the EV kit. JU1 of the EV kit must be installed on 1–2 (ON) position. Apply an analog signal up to +12V on JU2, and the rest of the jumpers are left open. SW3 of the MAXQ2000-KIT must be turned off for proper operation of the system.

Note: The suffix "-bar" (CS-bar) indicates the active-low functionality of the CS pin.

Figure 1. The schematic for the MAX1132 EV kit

Figure 1. The schematic for the MAX1132 EV kit

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Resources


Video
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project