Considerations for Selecting an RS-485 Transceiver in Electronic Power Meters
Abstract
Automatic meter reading technology provides a communication port to power meters, allowing them to be read electronically and remotely. This application note discusses the various features of Maxim's RS-485 transceivers that make them well suited for communication ports in electronic power meters.
Automatic meter reading is becoming increasingly popular in electronic power meters. This technology provides a communications port to the power meter, allowing it to be read electronically and, in most cases, remotely. This allows power utilities to save both money and time. The key to making this technology work is to ensure the communications link is both safe and robust. RS-485 is a simple, cheap, reliable communications specification that is well suited for automatic meter reading. The following article discusses the numerous features of Maxim's RS-485 transceivers that make them ideal for electronic power meters.
Figure 1. An example block diagram of an electronic power meter with an RS-485 port.
Figure 1 shows an example block diagram of an electronic power meter using an RS-485 port. The port is electrically isolated from the MCU and analog front-end by the use of optocouplers and a transformer. This isolation provides protection and robustness against electrical surges on the RS-485 lines.
The pullup and pulldown resistors on the A and B lines serve to define the state of the receiver in the event of a cable disconnect. Using these resistors, the receiver output is always high when the cable is disconnected, which can have many advantages. In the Figure 1 system, the IrDA circuit has an open-drain output. Consider what would happen if the RS-485 transceiver were to incorrectly pull the line low when the cable becomes disconnected. In this case, the optocoupler's output transistor would be on and would hold the bus low, preventing any communication between the open-drain IrDA module and the MCU. By guaranteeing a high output on cable disconnects, the system can use other open-drain devices on the same UART bus.
The PTC and TVS combine to provide differential-mode overvoltage protection in the event that one of the RS-485 wires gets shorted to the main power line (for example, 220VAC).
The isolated circuitry is powered by an additional winding on the flyback transformer. In the Figure 1diagram, the flyback has two outputs: the first is for powering the MCU and analog front-end. The second is electrically isolated and provides power to the RS-485 port. Observe that if a battery backup is used with the flyback power supply shown above, it would be effectively "diode OR-ed" in with the supply for the MCU (VCC in the diagram). This means that the isolated_VCC would not be present when operating from battery. Therefore, the RS-485 circuit is not "on", so the meter cannot be communicated with during power outages and has no way to tell anyone that power has gone out.
The following are features of Maxim's RS-485 transceivers that can help improve/simplify the design of the RS-485 port electronic power meters. For more information on devices that include all these features, refer to the MAX3070E (3.3V) or MAX13085E (5V) data sheet.
Fail-Safe The RS-485 standard defines the threshold for the high and low signal to be ±200mV, but leaves the range between these levels as indeterminate. This presents problems under three conditions:
- All the transmitters on the bus are disabled and therefore high impedance. This means the differential voltage between the receiver inputs is 0V due to the termination resistors on the bus.
- There is a short circuit between the RS-485 wires. Again, the differential voltage between the wires is 0V.
- There is an open circuit, or the power meter is disconnected. Again, the differential voltage is 0V because the transceiver itself has a high-impedance resistance between the inputs, forcing it to 0V.
Slew-Rate Limiting Because the data rates for most power-meter applications are in the 1kbps to 19.2kbps range, fast edge rates are unnecessary and only serve to generate unwanted radiated emissions. By controlling the edge rates of the driver in an RS-485 transceiver, the emissions at higher frequencies can be reduced. Lower slew rates also reduce data errors due to imperfect terminations and stubs, etc. (see Figures 2 and 3).
Figure 2. The driver output waveform and FFT plot of the MAX3485E/MAX3490E/MAX3491E transmitting a 125kHz signal.
The MAX3485E/MAX3490E/MAX3491E are not slew-rate limited and can therefore support higher data rates. However, the faster edges necessary for the higher data rates generate larger, higher frequency harmonics. These harmonics can increase radiated EMI and are less tolerant of imperfect terminations.
Figure 3. The driver output waveform and FFT plot of MAX3483E/MAX3488E transmitting a 125kHz signal.
The MAX3483E and MAX3488E are slew-rate limited and therefore have reduced maximum data rates of 250kbps or less. This is usually more than adequate for power meter applications. The reduced slew rates get lower as the frequency harmonics become higher. This reduces EMI and imperfect termination issues.
Hot-Swap In multidrop systems, such as RS-485, it is important that only a single transmitter is enabled and transmitting. If two or more transmitters are enabled, there will be bus contention and therefore data errors. A robust system is able to tolerate a certain amount of data errors using software, but the hardware designer is still responsible for minimizing these errors in the first place. Maxim's hot-swap features are designed to address two common situations where there can be unintentional bus contentions:
- A transceiver is initially powered up on an already active bus.
- A transceiver is on a card that is hot plugged into an already active system.
Maxim's hot-swap feature solves this problem by using a two-step sequence. During the first 10µs, the RS-485 transceiver is powered up, and a strong pulldown of 600µA through a 5kΩ resistor is used to pull the DE pin low. A strong pulldown is used to discharge any capacitance on the DE pin. After 10µs, a 100µA pulldown is used to maintain the logic-level low against leakage currents and noise. This 100µA pulldown current remains active until the DE pin is pulled high by an external source. Once the pin is high, the 100µA current source is disabled and the RS-485 transceiver operates normally (see Figure 4). This feature ensures that the transmitter on the RS-485 transceiver is tristated, preventing any unintentional bus contention.
Figure 4. A simplified block diagram of Maxim's hot-swap circuitry on the DE pin.
Extended ESD Protection ESD is a problem for all semiconductor devices, and RS-485 transceivers are no different. Maxim products designated with an "E" include extended ESD which, in the case of the MAX3070E and MAX13085E, is ±15kV using the Human Body Model (HBM).
Isolation The MAX3535 is a monolithic, isolated, 3.3V or 5V, self-powered RS-485 transceiver. It includes capacitive isolation, integrates the RS-485 transceivers, and uses an internal H-bridge driver with an external "off-the-shelf" transformer to provide a monolithic, isolated RS-485 solution in a 16-pin SO package. This greatly reduces the design effort by eliminating the need for an extra winding on the flyback power supply and opto couplers. Furthermore, because the MAX3535 is self-powered, the RS-485 port can remain functional even when the meter is operating from battery power. The MAX3535E also includes hot-swap, fail-safe, extended ESD, and slew-rate limiting (Figure 5).
Figure 5. A typical application circuit for the MAX3535E.
Electronic power meters have been manufactured for many years, but the inclusion of automated meter reading functionality is a relatively recent event. The features of Maxim's RS-485 transceivers help to improve the cost, robustness, simplicity, and size of the electronic power-meter design.
Related to this Article
Products
PRODUCTION
+5.0V, ±15kV ESD-Protected, Fail-Safe, Hot-Swap, RS-485 Transceivers
PRODUCTION
+3.3V, ±15kV ESD-Protected, Fail-Safe, Hot-Swap, RS-485/RS-422 Transceivers
RECOMMENDED FOR NEW DESIGNS
+3V to +5V, 2500VRMS Isolated RS-485/RS-422 Transceivers with ±15kV ESD Protection