Connecting the Agere Ultramapper Device Family to Maxim T3/E3 LIUs

Mar 24 2004

Figure 1

   

Abstract

This application note shows how to connect our T3/E3 line interface units (LIUs) in clear-channel, transMUX, and map/demap applications with the Agere Ultramappers.

Introduction

This application note shows a how to connect the Maxim DS3150or DS315x series of T3/E3 LIUs to the Agere Ultramappers. The DS3150 and DS315x series of T3/E3 LIUs perform all the functions necessary for interfacing at the physical layer to T3 and E3 lines. The DS3150 is a Hardware only, single port T3/E3 LIU, while the DS3151, DS3152, DS3153and DS3154 offer both Hardware and CPU Bus modes in 1, 2, 3, or 4 ports respectively. This application note will illustrate connecting to the DS3150 with the connection to the DS315x series being similar.

The Agere Ultramapper Device Family includes the following: Ultramapper, UltramapperLite, Ultramapper Full Transport, and Ultraframer. This application note will discuss applications that pertain only to the following Agere devices: UltramapperLite and Ultraframer.

The following diagrams will illustrate Maxim T3/E3 LIUs from the DS315x series or multiples of the DS3150. Depending on the linecard/system design, the designer will need to choose which of the five Maxim LIUs to utilize.

Applications

T3/E3 Clear Channel Application

In this application, two UltramapperLites are configured to terminate/transmit twelve T3/E3 signals from/to T3/E3 mapped STS-12/STM-4 signals.

Figure 1. T3/E3 clear channel application.

Figure 1. T3/E3 clear channel application.

T3/E3 TransMUX Application

In this application, four UltramapperLites are configured to transMUX between two different scenarios: between one VT1.5/VC11 mapped STS-12 and twelve T1 channelized T3 signals; and between one VT2/VC12 mapped STS-12 and twelve E1 channelized E3 signals.

Figure 2. T3/E3 TransMUX application.

Figure 2. T3/E3 TransMUX application.

T3/E3 and T1/E1 Map/Demap Application

In this application, one Ultraframer is configured to map/demap between three channelized T3/E3 signals and 84/48 T1/E1 signals.

Figure 3. T3/E3 and T1/E1 Map/Demap application.

Figure 3. T3/E3 and T1/E1 Map/Demap application.

T3/E3 and DS0/E0 Map/Demap Application

In this application, one Ultraframer is configured to map/demap between three channelized T3/E3 signals and upto 2016/1536 timeslots of DS0/E0 signals.

Figure 4. T3/E3 and DS0/E0 Map/Demap application.

Figure 4. T3/E3 and DS0/E0 Map/Demap application.

Maxim T3/E3 Line Interface Unit Configuration

With the Agere Ultramapper in M13/E13 MUX/DeMUX applications, a free-running 44.736MHz T3 or 34.368MHz E3 clock should be provided to pin DS3DATAOUTCLK for M13/E13 functionality. In SONET/SDH to T3/E3 applications where DS3/E3 Digital Jitter Attenuator is used on the receive path: SONET/SDH ↔ TMUX/STS-1LT ↔ SPE ↔ (DS3/E3 Digital Jitter Attenuator) ↔ T3/E3; the DS3DATAOUT input is not needed for M13/E13 functionality. Instead, a free-running 44.736MHz DS3XCLK clock and a 34.368MHz E3XCLK clock are required for T3/E3 Digital Jitter Attenuator functionality. The Agere Ultramapper T3/E3 line interface is straightforward to connect to the Maxim T3/E3 LIUs. As far as T3/E3 connections are concerned, there are no differences between the master Ultramapper and slave Ultramapper.

The interface between a T3/E3 analog line and a Line Interface Unit can be in either bipolar or unipolar mode. Table 1 lists the register settings of the Agere Ultramapper for DS3/E3 Bipolar/Unipolar control.

Table 1. Agere Ultramapper DS3/E3 Bipolar/Unipolar Control Bits
Block Name Register Name Address Description
SPEMPR SPEMPR_TDS3_BIPOLAR 0x19 [1] Transmit DS3/E3 Bipolar/Unipolar. Note this is valid only if register 0x0018 [13:12] = 11.
SPEMPR SPEMPR_RDS3_BIPOLAR 0x19 [0] Receive DS3/E3 Bipolar/Unipolar. Note this is valid only if register 0x0018 [5:4] = 11.
DS3DJA DS3DJA_DS3_BIPOLAR 0x15 [5:0] Per Channel Control Bit
1: HBD3 or B3ZS.
0: Unipolar.
DS3DJA DS3DJA_DS3_B3ZS 0x14 [5:0] Per Channel Control Bit
1: B3ZS coding.
0: HDB3 coding.
M13 M13_BIPOLAR 0x5D [0] 1: B3ZS encoding/decoding, i.e., DS3 I/O is in dual-rail mode where each rail carries a polarity of a bipolar I/O.
0: DS3 I/O is a single-rail, unencoded NRZ signal.
E13 E13_TE3_BIPOLAR 0x23 [2] 1: E3 output is HDB3 encoded and dual-rail.
0: E3 output is single-rail unencoded.
E13 E13_RE3_IN_CTL 0x26 [5:4] 00: HDB3 decode disabled (input data on positive rail only).
01: HDB3 decoder enabled, input on P/N rails.
10: HDB3 decoder disabled (input data on positive rail only).
11: HDB3 decoder disabled, negative input rail carries HDB3 error count from external LIU.

Conclusion

This application note has shown how to connect our T3/E3 LIUs to the Agere Ultramapper Device Family.

If you have further questions about connecting any of our T3/E3 LIUs, then please contact the Telecommunication Applications support team.

Maxim DS3/E3 LIU Information

For more information about our T3/E3 LIUs, please consult the data sheet.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project