Digital Sterilization Monitor for Autoclaves

Aug 23 2015

Abstract

Maxim’s digital sterilization monitor is a precision, electronic-based solution designed to monitor and record the applied temperature profile during an autoclave sterilization cycle. The DS1922F datalogger can be placed anywhere inside an autoclave where it measures and records temperature into its internal memory. Once the sterilization cycle is complete, the DS1922F is simply removed from the sterilization chamber and docked into a reader to download the captured data to a PC. Then, companion PC software automatically displays the temperature measurements, indicates whether the sterilization cycle was successful based on required parameters of temperature and time, and securely stores the cycle data to satisfy regulatory and liability requirements. Read full article.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project