Overview
Product Details
This evaluation board is obsolete and no longer recommended.
The CVT-ADC-FMC-INTPZB was developed in 2012 to serve as a temporary bridge between certain legacy ADI Tyco connector EVBs and the newer, industry-standard FMC-style connectors on certain COTS Xilinx FPGA platforms. The interposer was only verified for compatibility between specific ADI Converter EVBs and specific 3rd-party Xilinx COTS FPGA platforms listed here: https://wiki.analog.com/resources/alliances/xilinx#ad-adc-fmc_adapter_board
Please note that the CVT-ADC-FMC-INTPZ only supported the small subset of converter boards listed at the above link.
At this point the majority of the legacy Tyco eval brds previously supported by the CVT-ADC-FMC-INTPZ have either been obsolesced or redesigned using the new FMC-compatible connector. The decision was made to obsolete the interposer since it was no longer required/universally supported.
Markets and Technologies
Applicable Parts
Documentation & Resources
-
High Speed ADC FMC Interposer Evaluation Board Schematic Board10/20/2014PDF176 K
-
High Speed ADC FMC Interposer Evaluation Board Bill of Materials10/20/2014XLSX18 K
-
High Speed ADC FMC Interposer Evaluation Board Layout Board10/20/2014ZIP765 K