Resource Library
How to Write an Industry-Standard EEPROM (24C04) Using the MAX2990 I²C Interface
Abstract
Article and sample firmware code describe how to use the I2C interface on the MAX2990 power-line communications modem to interface with an external EEPROM 24C04.
Introduction
This application note and the sample firmware code describe how the I2C interface on MAX2990 power-line communications modem can be used to interface with an external EEPROM 24C04. The I2C bus is controlled by the MAX2990 (master) and the 24C04 EEPROM is the slave. The schematic below shows the hardware configuration used in this example.

Firmware Description
I2C Interface Initialization
Whenever the I2C module is enabled, SCL and SDA must be configured as open-drain. This configuration is necessary for the I2C communication to operate properly. Since the I2C is an alternate function for a GPIO port, firmware must ensure that the pullup on the SCL and SDA inputs is disabled (by writing a zero to that port controller output bit) during initialization.
The example has the 250kHz clock frequency. First you need to set up the I2C interface in the MAX2990 as shown below:
PO1_bit.Bit2 = 0; // Disables the GPIO function of the PO1_bit.Bit3 = 0; // I2C pins I2CCN_bit.I2CEN = 0; // Makes sure that I2C is disabled // to allow the changing of the I2C settings I2CCN_bit.I2CMST = 1; // Sets the I2C engine to master mode I2CCN_bit.I2CEA = 0; // 7-bit address mode I2CCK_bit.I2CCKL = 0x40; // 2µs CLK-low, to define I2C frequency I2CCK_bit.I2CCKH = 0x40; // 2µs CLK-high, to define I2C frequency I2CTO = 200; // I2C_TIMEOUT I2CST = 0x400; // Resets I2C status register I2CCN_bit.I2CEN = 1; // Enables the I2C engine
Write Mode
To write to a 24C04 EEPROM, you have to write the following bytes through the I2C interface:
- Address of the I2C EEPROM (0xA0 in this example)
- Address of the memory location in the EEPROM
- Data bytes (address will increase automatically)
In this example we try to write the following bytes, starting from location 0x00, into the EEPROM: 0x12, 0x34, 0x56, 0x78, and 0x90.
i2c_init_write(); // Sets the MAX2990 I2C Engine into write mode i2c_write(0x50); // 24C04 write (adr = 0b1010 000 0) = 0xA0 // The MAX2990 I2C engine shifts the I2C address by // 1 bit, because it will generate the R/W bit // automatically i2c_write(0x00); // word address location i2c_write(0x12); // data1 i2c_write(0x34); // data2 i2c_write(0x56); // data3 i2c_write(0x78); // data4 i2c_write(0x90); // data5 I2C_STOP; // Sends I2C stop-condition

Read Mode
To read back the data, we wrote from the EEPROM. It is important that we give the 24C04 enough time to write. This typically takes several milliseconds after the "stop-condition." Consult the data sheet of your IC to make sure that you use the correct timing.
i2c_init_write(); // Sets the MAX2990 I2C engine into write mode i2c_write(0x50); // 24C04 write (adr = 0b1010 000 0) = 0xA0 // The MAX2990 I2C engine shifts the I2C address by // 1 bit, because it will generate the R/W bit // automatically i2c_write(0x00); // word address location i2c_init_read(); // Sets the MAX2990 I2C engine into read mode i2c_write(0x50); // 24C04 read (adr = 0b1010 000 1) = 0xA1 // The MAX2990 I2C engine shifts the I2C address by // 1 bit, because it will generate the R/W bit // automatically unsigned char data[5]; // Array to store the received data i2c_read(data[0]); // Reads 1 byte from I2C and writes it to the array i2c_read(data[1]); // Reads 1 byte from I2C and writes it to the array i2c_read(data[2]); // Reads 1 byte from I2C and writes it to the array i2c_read(data[3]); // Reads 1 byte from I2C and writes it to the array i2c_read(data[4]); // Reads 1 byte from I2C and writes it to the array I2C_STOP; // Sends I2C stop-condition
Now we examine the following functions which were used to read and write the EEPROM.
i2c_init_write(void) i2c_init_read(void) i2c_write(UINT8 data) i2c_read(UINT8 *data)

void i2c_init_write(void)
{
I2CCN_bit.I2CMODE = 0; // I2C transmit mode
I2CCN_bit.I2CACK = 1; // Creates I2C NACK so that slave can create ACK
I2C_START; // Generates I2C START condition
while( I2CCN_bit.I2CSTART == 1 ); // Waits until the START condition
// was put to the I2C bus
I2CST_bit.I2CSRI = 0; // Resets the I2C interrupt flag
}
int i2c_init_read(void)
{
I2CCN_bit.I2CMODE = 1; // I2C read-mode
I2CCN_bit.I2CACK = 0; // Creates I2C ACK after receive
I2C_START; // Generates I2C START condition
while( I2CCN_bit.I2CSTART == 1 ); // Waits until the START condition
I2CST_bit.I2CSRI = 0; // Resets the I2C interrupt flag
}
void i2c_write(UINT8 data)
{
I2CBUF = data; // Puts the data on the I2C bus
while( I2CST_bit.I2CTXI == 0 ); // Waits for transfer complete
I2CST_bit.I2CTXI = 0; // Resets the I2C transmit complete
// interrupt flag
}
void i2c_read(UINT8 *data)
{
I2CBUF = 0xff; // Puts "all ones" on the I2C bus so that slave can pull
// the bus down to generate zeros
while( !I2CST_bit.I2CRXI ); // Waits for receive complete
I2CST_bit.I2CRXI=0; // Resets the I2C receive complete
// interrupt flag
*data = I2CBUF; // Writes the data to the pointer
}