Abstract
This circuit monitors a resistance value in a noisy or otherwise hostile environment. Connected across the secondary winding of an isolation transformer, the unknown resistance reflects to the primary where it forms a voltage divider with a 2.2kΩ resistor. The divider produces a reduced-amplitude clock signal that is capacitively coupled, rectified, and filtered to produce a dc output voltage corresponding to the monitored resistance.
A similar version of this article appeared in the April 24, 2008 issue of Electronic Design magazine.
The circuit of Figure 1 can monitor resistance in a noisy or otherwise hostile environment. Isolation and good common-mode rejection ratio (CMRR) are provided by the transformer (T1).
Figure 1. This circuit monitors the value of a galvanically isolated resistance.
Resistance across the secondary winding is reflected to the primary, where it forms a voltage divider with resistor R1. The divider produces a reduced-amplitude clock signal that is coupled through C2, rectified by D1 and D2, and filtered by C3 and R2. The result, at the inputs of the quad voltage monitor (IC1, MAX6338) is a dc voltage that varies with the monitored resistance as follows.
Secondary Resistance (kΩ) |
VDC at IC1 Inputs (V) |
0.5 | 1.40 |
1 | 1.90 |
2 | 3.00 |
3 | 3.60 |
4 | 4.00 |
5 | 4.30 |
6 | 4.50 |
7 | 4.65 |
8 | 4.80 |
9 | 4.90 |
10 | 5.05 |