ADIsimCLK™ Reference Design Files
Once ADIsimCLK is installed, users may take advantage of saved design files with the extension, ".clk". These clk files can serve as Reference Designs or starting points for a clock distribution design. The .clk files have been saved in ZIP format in the table below.
Download Instructions: The clk files do not need to be saved to any particular folder. One option is to create a folder with an easy name to remember such as "ADIsimCLK Designs". Save any or all of the files below to such a folder. Another option is for users to save these files directly to "Program Files/Applied Radio Labs/ADIsimCLK/Lib/ReferenceDesigns/". Any .clk file placed in this folder will appear on the "How do you want to start ADIsimCLK" dialogue box under "Start with a Reference Design".
Opening Saved Files: Once the clk files have been saved to the user's hard drive, the files may be opened by choosing "Open an existing design file" from the ADIsimCLK dialogue box, "How do you want to start ADIsimCLK". Click "OK" and then browse to the folder where the reference design files have been saved. An alternative way to open a saved file is via the File pull down menu. Select "Open" and browse to desired file. Lastly, if the user has saved the clk files to the "Program Files/Applied Radio Labs/ADIsimCLK/Lib/ReferenceDesigns/" described above, then the reference design option will appear in the opening dialogue box under "Start with a Reference Design".
File Description | Design Notes | Reference Design Files (.clk) | Date Posted |
AD9510 Quick Start | [pdf, 24,576] | [zip, 49,152] | 2005-Aug-22 |
AD9511 Quick Start | [pdf, 20,480] | [zip, 45,056] |
2005-Aug-22 |
AD9512 Quick Start | [pdf, 24,576] | [zip, 40,960] | 2005-Aug-22 |
AD9513 Quick Start | [pdf, 20,480] | [zip, 32,768] | 2005-Aug-22 |
AD9514 Quick Start | [pdf, 20,480] | [zip, 36,864] | 2005-Aug-22 |
AD9515 Quick Start | [pdf, 20,480] | [zip, 32,768] | 2005-Aug-22 |
AD9510 Datasheet comparison CLK1 = 245.76MHz |
[pdf, 32,768] | [zip, 131,072] | 2005-Aug-22 |
AD9510 Datasheet comparison CLK1 = 491.52MHz |
[pdf, 28,672] | [zip, 110,592] | 2005-Aug-22 |
AD9510 Datasheet comparison CLK1 = 622.08MHz |
[pdf, 28,672] |
[zip, 131,072] | 2005-Aug-22 |