Abstract
Maxim Integrated's PPG Algorithms includes a complete solution for wellness applications including vital sign measurement (Heart rate, interbeat interval, SpO2. and respiration rate), activity tracking and well-being applications (Sleep quality assessment, stress level measurement, sports coaching ) The envisioned product targets health and wellness applications for continuous 24/7 monitoring with utmost accuracy and optimized power management.
Introduction
Maxim's health and wellness algorithms are available for customers who aim to create wearable devices with the state-of-the-art functions and with faster time to market. The Wearable Heart Rate Monitoring (WHRM) product includes heart rate (HR) and activity tracking algorithms, especially for the heart rate detection, cardiac beat detection, step measurement, and activity classification. The envisioned product targets health and wellness applications for continuous 24/7 monitoring with optimized power management and the provision of accurate heart rate (HR) and interbeat interval (IBI) detection, step detection, and sample-by-sample activity classification. The SpO2 measurement algorithm provides oxygen saturation of the subject with the best-in-class accuracy. These algorithms are available with MAX32664B/C Biometric Sensor Hub to provide a complete embedded solution communication with Maxim's optical sensor products.
The respiration rate measurement (RRM) algorithm contributes with subject respiration rate which is another vital sign of the subject. Sleep quality assessment and sports coaching algorithms provide a general insight of the subject's wellness. These algorithms are available for various platforms by processing the outputs of MAX32664B/C Biometric Sensor Hub.
Maxim's WHRM Solution
Heart rate is the frequency of heart contractions that is measured in beats per minute (BPM). The pulse rate is the number of times the arteries create a measurable pulse due to the blood pressure change created by heart contractions. Normally, the photoplethysmographic (PPG) signal provides information about the pulse rate rather than the heart rate. However, we use "heart rate" which is a standard in the market.
Maxim WHRM algorithm utilizes synchronized 3-axis accelerometer and PPG data to provide several end-user-friendly fitness tracking outputs like heart rate and activity-related statistics, e.g., step count, burned calories, and activity class of a user. The PPG signal can be obtained from contractions of ventricles in finger, wrist, ear, toe, chest, etc.
Input Parameters
The Maxim HRM solution accepts additional user information of the subject as input parameters. These parameters include age, height, weight, and gender information that are accepted from a person. These details are obtained at the initialization of the algorithm as shown in Table 1.
These input parameters (Table 1) are optional and default average values are used.
User Inputs | Notes |
Age | the age of the person in years |
Height | the height of the person in cm |
Weight | the weight of the person in kg |
Gender | the gender of the person |
Measurement Quality Metric
There are critical factors which affect the performance of PPG-based HRM like periodic/nonperiodic motion, electronic noise, mechanical/strap design, ambient light, melanin/skin color, low blood perfusion, etc.
Therefore, in order to report reliable heart rate, the quality of the measurement is the key factor. In validation phase, the report of the algorithm can be compared with an electrocardiogram (ECG)-based device and the quality/performance of the measurement can be calculated. However, in real-life conditions, there will not be a reference device to evaluate the quality of the measurement. Maxim's WHRM solution provides a measurement quality metric which enables evaluation of the heart rate reports sample by sample in real time.
Maxim's HR measurement quality metric scores the measurement between 0 and 100:
- 100%: Perfect measurement quality
- 75%: Good enough measurement quality
- 50%: Mostly good enough measurement quality
- 25%: Poor measurement quality
- 0%: Unreliable measurement
Each heart rate value is reported with a measurement quality value in the algorithm so the heart rate report can be evaluated in real time. A sample of a challenging data set (Table 2) consists of a large number of data sequences with different activities like reclining, sitting, standing, sleeping, jogging, treadmill normal, fast, incline walking, treadmill/irregular walking, indoor/outdoor biking, running, elliptical machine, rowing, daily life, and overall (all activities/data points).
Rest (Reclining, Sitting, Standing, Sleeping) | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
±5 BPM Accuracy [%] | 98.77 | 98.28 | 97.75 | 97.42 | 97.34 |
Mean Absolute Error [BPM] | 0.99 | 1.08 | 1.18 | 1.24 | 1.24 |
Reporting Coverage [%] | 82.80 | 94.07 | 97.61 | 99.36 | 100.00 |
Walking | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
±5 BPM Accuracy [%] | 94.48 | 92.49 | 91.24 | 90.21 | 89.77 |
Mean Absolute Error [BPM] | 1.67 | 1.86 | 1.98 | 2.18 | 2.26 |
Reporting Coverage [%] | 64.04 | 84.07 | 93.34 | 97.99 | 100.00 |
Running | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
± 5 BPM Accuracy [%] | 96.39 | 95.03 | 92.11 | 88.61 | 86.57 |
Mean Absolute Error [BPM] | 1.36 | 1.67 | 2.07 | 2.63 | 3.04 |
Reporting Coverage [%] | 55.12 | 72.79 | 82.46 | 91.15 | 100.00 |
Biking | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
± 5 BPM Accuracy [%] | 95.81 | 94.22 | 92.27 | 90.41 | 89.71 |
Mean Absolute Error [BPM] | 1.55 | 1.78 | 1.94 | 2.11 | 2.17 |
Reporting Coverage [%] | 60.20 | 80.17 | 89.97 | 96.83 | 100.00 |
Overall | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
± 5 BPM Accuracy [%] | 96.62 | 95.28 | 94.02 | 92.78 | 92.07 |
Mean Absolute Error [BPM] | 1.34 | 1.53 | 1.68 | 1.88 | 1.99 |
Reporting Coverage [%] | 67.13 | 84.45 | 92.16 | 96.94 | 100.00 |
Daily LIFE | |||||
Data Points with Measurement Quality Metric | = 100 | = 75 | = 50 | = 25 | = 0 |
± 5 BPM Accuracy [%] | 97.40 | 95.20 | 93.60 | 92.90 | 91.10 |
Mean Absolute Error [BPM] | 1.34 | 1.41 | 1.47 | 1.61 | 1.82 |
Reporting Coverage [%] | 53.00 | 75.00 | 88.00 | 96.00 | 100.00 |
± 5 Error Band Accuracy
It is the percentage of the valid data points which have absolute error of = 5 BPM with respect to the reference device output (ECG chest strap). This metric is calculated in 1Hz.
Mean Absolute Error
Mean absolute error (MAE) is the average of the absolute difference of each Maxim HRM algorithm and the reference device output (ECG chest strap). This metric is calculated in 1Hz.
Reporting Coverage
It is the percentage of the valid data points which the measurement quality metric is greater than a certain threshold.
Algorithm Outputs
Heart Rate
Maxim's HRM outputs showing the heart rate measurement with a quality metric have the properties as shown in Table 3.
Maxim's Heart Rate Monitoring | |
Parameter | Description |
Measurement Unit | BPM – beats per minute |
Update Frequency | 1Hz |
HR Report Range | 30 BPM–210 BPM |
Sensor Inputs | PPG and 3-axis Accelerometer |
Activity Type | All (tested with lying down, sitting, standing, sleeping, jogging, walking, biking, elliptical machine, rowing, and daily life) |
First Reporting Time | 5s–15s |
Input Parameters | See Input Parameters section |
Outputs | Heart rate in BPM, measurement quality score between 0 and 100 |
Sampled Mode Heart Rate
The sampled mode heart rate consists of switching on the optical signal during short-time intervals and obtain an estimation of the heart rate as fast as possible. There are two key factors in the sampled mode heart rate measurement:
- evaluate when a short-time estimation is reliable (to turn off the light-emitting diodes [LEDs])
- obtain a reliable estimation with minimal information about the history of the measurement
The algorithm outputs are obtained when the short-time estimation is reliable with the help of the measurement quality metric. The heart rate is calculated between 5 seconds and 20 seconds based on the signal quality and activity type. The update rate of the heart rate report is controlled by the user in sampled mode and no measurement is applied between two sampled mode heart rate measurements, which enable power saving. See Table 4.
Parameter | Description |
Measurement Unit | BPM – beats per minute |
Update Frequency | Configurable (e.g., 1 measurement per 1 minute, 1 measurement per 10 minutes, etc.) |
HR Report Range | 30 BPM –210 BPM |
Sensor Inputs | PPG and 3-axis accelerometer |
Activity Type | All |
First Reporting Time | 5s–20s |
Input Parameters | See the Input Parameters section |
Outputs | Heart rate in BPM, measurement quality score between 0 and 100 |
Interbeat Interval
The time interval between the individual heartbeats is called an interbeat interval. It is a crucial health indicator. It is the primary input for the heart rate variability that is used for heart health and autonomous nervous system health. It may also be used in a wide spectrum of applications, such as clinical practice, sleep quality measurement, and stress and recovery analysis.
Maxim's IBI accuracy in resting condition is as follows:
MAE 7ms, extra beat detection of 3%, missed beat of 2%, and with 95% of coverage See Table 5.
Parameter | Interbeat Interval |
Measurement Unit | Milliseconds |
Update Frequency | Every heartbeat |
IBI Report Range | 285ms–2000ms |
Sensor Inputs | PPG and 3-axis accelerometer |
Activity Type | Resting |
First Reporting Time | 5s–15s |
Input Parameters | See Input Parameters section |
Outputs | IBI in ms, Measurement Quality Score in discrete percentage: 0% No output 25% Bad signal 50% Moderate 75% Good 100% Perfect |
Signal Requirements
- Proper sensor to skin coupling should be satisfied. The watch should fit snugly and comfortably.
- Accelerometer and PPG signal sampling rate should be 25Hz, with sampling interval between 38ms and 43ms.
- Accelerometer to PPG synchronization should be within 25ms, with reference to the sample timestamps.
- There should be accelerometer and PPG data point drops for no more than one sample per minute.
Reference Device
- Heart Rate—Consider using an ECG chest strap with a minimum of 250Hz sampling rate, such as Polar H10.
Signal Quality Requirement
Maxim's algorithm expects the signal quality with peak signal-to-noise ratio (pSNR*) > 15dB at rest and 6dB during exercise on each of the green PPG channels to achieve the accuracy numbers shown in Table 2. The HR frequency is the dominant frequency in the PPG spectrogram.
*Note: For pSNR calculation (also known as AC signal SNR), signal power is defined to be the power of the signal at the heartbeat frequency in addition to its second and third harmonics. The noise power is defined to be the power of all other signal components, including motion artifacts.
Activity Classifier
Maxim's activity type metric outputs the user activity state in continuous mode. The activity type metric is enhanced with machine learning-based algorithm with the large dataset of real data. The activity classifier is an independent module that does not require the PPG input to function. See Table 6.
Parameter | Description |
Unit | Activity Type |
Activity Types | Rest Walk Run Bike Other |
Sensor Inputs | 3-axis Accelerometer |
First Reporting Time | 2s |
Table 7 shows an example for the performance of Maxim's activity classifier.
Activity Type | Accuracy [%] | Recall | Precision |
Rest | 99 | 0.93 | 1.00 |
Walk—Indoor | 96 | 0.97 | 0.91 |
Run —Indoor | 98 | 0.93 | 0.96 |
Walk—Outdoor | 95 | 0.95 | 0.99 |
Bike—Outdoor | 98 | 0.85 | 0.95 |
Energy Expenditure
Maxim's energy expenditure (EE) metric outputs the energy expenditure depending on the activity type of that moment in time. Maxim HRM algorithm is able to output both passive EE (basal metabolic rate—BMR), active EE (active metabolic rate—AMR) and total EE that corresponds to a sum of passive and active EE rates in metabolic equivalent of task (MET—kcal/kg/h) metric. See Table 8.
Parameter | Maxim HRM EE |
Definition | Accumulated EE since the last reset of algorithm |
Measurement Unit | kcal |
Sensor Inputs | 3-axis Accelerometer |
Input Parameters | Age, Gender, Height, Weight, Activity |
Output | BMR AMR Total EE |
Step Counts
Maxim's step counting feature outputs the total step counts based on the wrist motion for both walking and running considered to be separate activities. See Table 9.
Parameter | Maxim Step Count |
Measurement Unit | Number of Steps |
Sensor Inputs | 3-axis Accelerometer |
Output | Total Walking Steps Total Running Steps |
Table 10 shows an example for the performance of Maxim's step counting feature.
Activity Type | Absolute Percent Error of Step Counts (%) |
Walk—Indoor | 0.90 |
Run—Indoor | 4.18 |
Walk—Outdoor | 6.45 |
Cadence
The cadence is expressed as the number of steps per minute that is detected in rhythmic activities such as walking, running, and biking. See Table 11.
Parameter | Maxim Cadence |
Measurement Unit | Steps/minute |
Sensor Inputs | 3-axis Accelerometer |
Suitable Activity | Walking, Running, Biking |
Update Frequency | 25Hz |
Output | Cadence |
SpO2 - Blood Oxygen Saturation
The SpO2, also known as blood oxygen saturation, is a measure of the amount of oxy-hemoglobin relative to the total amount of hemoglobin in the arterial blood. The SpO2 level is reported in terms of percentage. It has been considered as one of the five vital signs indicating the status of the body's life-sustaining functions in addition to the heart rate, respiratory rate, blood pressure, and body temperature. Maxim's SpO2 measurement solution functions as a drop-in module for wrist-worn health bands as well as finger-based pulse oximetry devices. The specifications of SpO2 algorithm are summarized in Table 12.
Parameter | SpO2 |
Measurement Unit | Percentage (%) |
Input Sampling Frequency | 25Hz |
Update Frequency | 1Hz |
Range | 70%–100% |
Accuracy (RMSE) | 3.5% |
Sensor Inputs | PPG, 3-axis accelerometer |
Suitable Activity | Rest, Sleep |
First Reporting Time | ~20s |
Output | SpO2, signal quality flags, motion flag |
Maxim SpO2 Algorithm Requirements
The necessary operating conditions for SpO2 algorithm are as follows:
- The sensor to skin coupling should be proper.
- The wearable device should fit snugly and comfortably.
- The user should place the wearable device on the wrist gently without a need for extra pressing to obtain the signal. No over- or under-pressing should be done.
- Subjects should not squeeze their arms, hold anything during measurement, or wear other devices on the same wrist.
- Subjects should be free of deformities or abnormalities or other health issues that can prevent proper use of the device under test.
- Subjects shall be free of known heart arrhythmias such as atrial fibrillation, atrial flutter, paroxysmal supraventricular tachycardia (PSVT), ventricular tachycardia, ventricular fibrillation, premature atrial contraction, bradyarrhythmia, premature ventricular contractions (PVCs), long QT syndrome, sinus node dysfunction and heart block.
- Accelerometer-to-PPG data acquisition synchronization should be within 25ms, with reference to the sample timestamps.
- There should not be any accelerometer or PPG data point drop.
The minimum signal quality requirements for SpO2 algorithm are as follows:
- Perfusion index range
- PI = 0.2%
- Sampling rate
- Red/IR PPG 25Hz
- Signal continuity
- Greater than 30s of continuous RED/IR PPG signal with 'Low PI', 'Low SNR,' and 'Motion' flags set off
- Signal-to-noise ratio
- PPG signal quality with AC SNR > 35dB (time domain) and pSNR > 10dB (frequency domain) at rest where
- AC SNR is defined as: SNR = 20 * Log (PAC / PNoise) where PAC is "peak-to-peak amplitude of PPG pulse" and PNoise is "RMS of AFE noise
- For pSNR calculation, the signal power is defined to be the power of the signal at heartbeat frequency in addition to its second and third harmonics. The noise power is defined to be the power of all other signal components, including motion artifacts.
Respiration Rate
The respiration rate is a vital sign indicating the health and wellness and can be an input for several applications, such as sleep quality assessment, stress level estimation, and energy exposure estimation, etc. Maxim RRM algorithm is a wearable solution to measure the user's respiration rate by the PPG signal gathered from the wrist or fingertip. See Table 13.
Parameter | Respiration Rate |
Measurement Unit | 1 breath per minute (brpm) |
Input Sampling Frequency | 25 samples per s |
Update Frequency | 25Hz |
Range | 6brpm–30brpm |
Accuracy (MAE) | 1.6brpm (At rest) |
Sensor Inputs | PPG |
Suitable Activity | Rest, Sleep |
Latency | ~60s |
Output | Respiration rate, Output confidence level (0%–100%) |
Sleep Quality Assessment
Sleep is restoration process of the body; efficiency of the restoration is directly correlated to the amount of time spent at each sleep phase. Absence of any of the sleep phases or lack in the durations of the sleep phases can cause severe diseases and problems with cognitive skills. Hence, tracking of the sleep phases is vital for human beings. Maxim sleep quality assessment (SQA) algorithm delivers automatic tracking of sleep through the wearable devices. See Table 14 and Table 15.
Parameter | Sleep Wake State |
Measurement Unit | Sleep State |
Input Sampling Frequency | 1 sample per second |
Update Frequency | Every 30s |
Range | Sleep/Wake |
Accuracy | 92% |
Input Parameters | Heart Rate, IBI, Accelerometer Magnitude, Activity |
Suitable Activity | Rest, Sleep |
First Reporting Time | Up to 5min |
Latency | Up to 30min |
Configuration Parameters | Age, Gender, Weight, Resting Heart Rate |
Output | Sleep/Wake State, Latency Report, Update Flag |
PARAMETER | Sleep Phase State |
Measurement Unit | Sleep Phases |
Input Sampling Frequency | 1 sample per second |
Update Frequency | Every 5min |
Range | Light/Deep/Rapid Eye Movement |
Accuracy | 66% |
Input Parameters | Heart Rate, Interbeat Interval, Accelerometer Magnitude, Activity |
Suitable Activity | Sleep |
First Reporting Time | Up to 30min |
Latency | Up to 30min |
Configuration Parameters | Age, Gender, Weight, Resting Heart Rate |
Output | Sleep Phase, Update Flag |
Sports Coaching
To achieve a healthy life, sports need to be a part of the individuals' lives. People need to plan and keep a track of their sports performance and the frequency to adjust their lifestyle so that they can keep themselves healthy. With the widespread use of wearable devices, people have started to use them for keeping a track of their vital signs (heart rate, SpO2 level, etc.) and sports activities (walking, running, biking, etc.). As the next step, wearable devices need to serve people to track their sports activities.
VO2 MAX is the maximum rate of oxygen consumption that a user can reach during an exercise. The VO2 MAX of a subject is an indicator of the subject's fitness level.
The fitness age is a metric that interprets the subject's VO2 MAX score in terms of the human age.
Parameter | VO2 MAX |
Measurement Unit | 1ml/min/kg |
Input Sampling Frequency | 25 samples per second |
Update Frequency | 1 output per session |
Range | 0–100 |
Sensor Inputs | PPG |
Suitable Activity | Rest (Relax) |
First Reporting Time | Up to 6min |
Input Parameters | Age, Gender, Weight, Height |
Output | VO2 MAX, Fitness Age |
EPOC is the amount of oxygen required to restore the subject's body to its homeostasis. Homeostasis is the state of the living body where it is steady both physically and chemically. Therefore, EPOC is an indicator of the training effect on the user's body. See Table 17.
Parameter | Excess Post-Exercise Oxygen Consumption (EPOC) |
Measurement Unit | 1ml/kg |
Input Sampling Frequency | 25 samples per second |
Update Frequency | 1 output per session |
Range | 0–200 |
Sensor Inputs | PPG |
Suitable Activity | Rest (After Exercise) |
First Reporting Time | Up to 5min |
Input Parameters | Age, Gender, Weight, Height, Exercise intensity, Exercise duration, Elapsed time after exercise |
Output | EPOC, Recovery Time |
The recovery time is the time required for the human body to reach homeostasis. During recovery time, the body repairs and prepares for the next training which is necessary to increase the sports performance in a healthy way. See Table 18.
Parameter | Recovery Time |
Measurement Unit | Minutes |
Input Sampling Frequency | 25 samples per second |
Update Frequency | 1 output per session |
Range | 0–? |
Sensor Inputs | PPG |
Suitable Activity | Rest (After Exercise) |
First Reporting Time | Up to 5min |
Input Parameters | Age, Gender, Weight, Height |
Output | Recovery Time |
Readiness Score is an HRV-based metric. It represents the physical state of the body and measures how ready is the body for the next training. See Table 19.
PARAMETER | Readiness Score |
Measurement Unit | No units |
Input Sampling Frequency | 25 samples per second |
Update Frequency | 1 output per session |
Range | 1–100 |
Sensor Inputs | PPG |
Suitable Activity | Rest |
First Reporting Time | Up to 5min |
Input Parameters | Age, Gender, Weight, Height |
Output | Readiness Score |
Heart Rate Variability
The heart rate variability (HRV) is a very important indicator of a person's health. Maxim HRV algorithm uses IBI information to generate various HRV metrics. These metrics are especially crucial for sports coaching and stress assessment. Please see Table 20 for algorithm specifications.
PARAMETER | HRV |
Measurement Unit | ms for time domain metrics ms2 for frequency domain metrics |
Inputs | Beat-to-beat duration in ms along with timestamp information (Remark: The algorithm can handle missing IBI values up to 20%, and occasional extra ones, which occur at most once in 10 seconds.) |
Input Range | 300ms–2000ms |
Outputs | Time domain metrics: AVNN, SDNN, RMSSD, pNN50 Frequency domain metrics: ULF, VLF, LF, HF. LF/HF, TOTPWR |
Output Update Rate | Configurable: 1 second to 6 minutes Default value: 30 seconds |
Latency | HRV is a window-based calculation. Window size is configurable: 25s–360s. Default Value: 300s |
Suitable Activity | Rest, Sleep |
Stress Monitoring
Daily life stress is one of the important issues of modern life. Mainly, two kinds of stress phenomena exist as acute and chronic stress. Acute stress arises because of pressure from the recent past and near future. For example, exercise challenges or any kind of sudden anxiety can induce acute stress. On the other hand, chronic stress results from the long-term pressures like socioeconomic conditions, ongoing problems in relations, etc. Maxim Stress Monitoring algorithm provides a quick stress assessment for acute stress of the subjects using wearable devices. See Table 21 for the algorithm specifications.
PARAMETER | Stress Score |
Measurement Unit | No units |
Input Sampling Frequency | 25 samples per second |
Update Frequency | 1 output per session |
Range | 0–18 |
Suitable Activity | Rest |
Input Parameters | Time domain HRV metrics (AVNN, SDNN, RMSSD, pNN50) Freq domain HRV metrics (ULF, VLF, LF, HF, TOTPWR) |
Output | Stress score (See Table 22), stress class, stress percentage |
Stress Score | DESCRIPTION |
0-8 | Represent stressful scores from highest to lowest levels where sympathetic system is dominant |
9-18 | Represent nonstressful scores from highest to lowest levels where parasympathetic system is dominant |
Automatic Exposure Control
The Automatic exposure control (AEC) algorithm is responsible for optimizing Maxim's PPG sensor analog front-end settings for optimum power consumption and heart rate measurement performance. Please see Table 23 for the algorithm specifications.
Parameter | AEC |
Inputs | PPG and Accelerometer Data |
Input Frequency | 25Hz |
Outputs | Analog front-end settings:
|
Output Update Rate | 25Hz |
Latency | None |
Suitable Activity | Rest for smart target level computation, all other activities for matching the LED level to the target |