35V Hot Swappable Supercapacitor Backup Power Controller Provides Uninterrupted Power, Protection & Monitoring

Jan 24 2018 - MILPITAS, CA
  • NORWOOD, MA – January 24, 2018 – Analog Devices announces the Power by Linear LTC3351, a supercapacitor charger and backup power controller IC that includes hot swap front-end protection and all the features necessary to provide a complete, standalone capacitor-based backup power solution. The LTC3351's integrated hot swap controller and circuit breaker use N-channel MOSFETS to provide a low loss power path from the input to the output, plus foldback current limiting to reduce inrush current. The device enables reliable short term uninterrupted power in the event of a main power failure for applications such as solid-state drives (SSDs) and nonvolatile dual in-line memory modules (NVDIMMs) data backup, power fail alarms in medical and industrial applications and "dying gasp" power fail indicators. The LTC3351 provides PowerPath control, capacitor stack charging and balancing, protection and capacitor health monitoring. Other applications include high current 12V ride-through supplies and short term uninterruptible power supplies (UPS) for servers, mass storage and high availability systems.


     

    The LTC3351 features a 4.5V to 35V input voltage range and over 10A of charge/backup current capability. The device also provides balancing and overvoltage protection for a series stack of one to four supercapacitors. The LTC3351's synchronous step-down controller enables constant current/constant voltage charging of the capacitor stack at up to 5V per cell. In backup mode, the step-down converter runs in reverse as a synchronous step-up DC/DC to deliver power from the supercapacitor stack to the system supply to be backed up. The hot swap controller provides programmable UV/OV thresholds, PCIe compatible start-up timing and a precision threshold /RETRY input.

    The LTC3351 includes an accurate 16-bit analog-to-digital converter (ADC) which continuously monitors input and output voltage and current. In addition, the internal measurement system monitors parameters associated with the backup capacitors themselves, including capacitor stack voltage, capacitance and stack ESR (equivalent series resistance) to ensure adequate energy storage and power delivery during backup. By monitoring the actual capacitance of the backup supercapacitors, the LTC3351 provides longer capacitor life by enabling the system to set the capacitor voltage to a minimum value while ensuring the required backup energy is maintained. All system parameters and fault status can be monitored via a 2-wire I2C interface, and alarm levels can be set to alert the system to a sudden change in any of these measured parameters.

    The LTC3351 is available in a thermally enhanced 44-lead, low profile (0.75mm) 4mm x 7mm QFN package. The device operates over a –40°C to 125°C junction temperature range and is available from stock. For more information, visit www.linear.com/product/LTC3351.


    Summary of Features: LTC3351

    • Integrated Hot Swap Controller with Circuit Breaker
    • High Efficiency Synchronous Step-Down CC/CV Charging of One to Four Series Supercapacitors
    • Step-Up Backup Mode Provides Greater Utilization of Stored Energy in Supercapacitors
    • 16-Bit ADC for Monitoring System Voltages/Currents, Capacitance & ESR
    • Programmable Undervoltage & Overvoltage Thresholds to 35V
    • VIN: 4.5V to 35V, VCAP(n): Up to 5V per Capacitor, Charge/Backup Current: >10A
    • Programmable Input Current Limit Prioritizes System Load Over Capacitor Charge Current
    • All N-FET Charger Controller & PowerPath Controller
    • Compact 44-Lead 4mm × 7mm QFN Package

    Pricing & Availability

    Product Production Availability Price Each Per 1,000 Package
    LTC3351 Now Starts at $5.25 4mm × 7mm 44-Lead QFN

     

    About Analog Devices

    Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com.

    Follow ADI on Twitter at http://www.twitter.com/ADI_News

    Subscribe to Analog Dialogue, ADI’s monthly technical journal, at:
    http://www.analog.com/library/analogDialogue/

    All registered trademarks and trademarks are the property of their respective owners.


    Contacts:

    John Hamburger
    Analog Devices, Inc.
    john.hamburger@analog.com
    Tel: 408-432-1900 ext 2419

    Doug Dickinson
    Analog Devices, Inc.
    douglas.dickinson@analog.com
    Tel: 408-432-1900 ext 2233


    Download Word Version

    Download PDF Version

  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is a leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
Stay Informed