Powering the Next Generation of NVIDIA AI Factories with MGX

Powering the Next Generation of NVIDIA AI Factories with MGX

As AI workloads accelerate, the shift toward AI factories are driving unprecedented rack-level power density. At the center of this transition is NVIDIA MGX™, an open modular architecture that enables faster system design, improved scalability and rapid deployment of next-generation AI infrastructure.

As a valued member of the MGX ecosystem, Analog Devices, Inc. (ADI) is working alongside NVIDIA to help enable this transformation, delivering the power technologies required to support increasingly demanding AI factory deployments.

800v hotswap 800v 6 v 5 28 2026pr

The Shift to 800 VDC: Enabling AI Factory Scale
As AI factories push for ever-higher performance, traditional 48 V architectures can no longer sustain the power demands of modern GPU clusters. To keep performance scaling, MGX-based AI factories are moving to 800 VDC rack-level architectures, which reduce current and power losses, enable more compact distribution and support scalable designs targeting megawatt-class racks. This shift in power architecture is foundational for future NVIDIA platforms where continued performance gains depend directly on power delivery efficiency.

MGX and Modular Power Architecture
The open, modular nature of MGX extends beyond compute into power delivery.

New architectures are increasingly disaggregating power from the compute rack, enabling:

  • Flexible system configurations aligned with evolving GPU platforms
  • Faster adoption of new technologies across the ecosystem
  • Optimized use of rack space for compute

800 VDC Hot Swap: Enabling Always-On AI Infrastructure
AI factories operate continuously, making live serviceability essential.

Hot swap controllers play a critical role by enabling safe insertion and removal of server trays without interrupting operation. At 800 VDC, this introduces new challenges, including:

  • Precise control of high-energy inrush currents
  • Robust fault detection and system protection
  • Real-time telemetry for system monitoring

ADI: Enabling 800 VDC Power for MGX Systems
ADI is extending its leadership in power protection, control, and telemetry to support next-generation AI infrastructure.

Building on decades of innovation, ADI is developing high-voltage hot swap and DC-DC solutions that deliver:

  • High-density integration for advanced compute platforms
  • Fast, accurate protection in high-voltage environments
  • Advanced telemetry for system optimization and predictive maintenance

Enabling the Future of AI Factories
As AI infrastructure evolves toward modular, open architectures built on NVIDIA MGX, 800 VDC power delivery becomes a cornerstone of scalability and efficiency.

Through continued collaboration within the MGX ecosystem, ADI is helping enable the next generation of AI factories—delivering the protection, conversion and intelligence required to power advanced AI systems with confidence.

All trademarks and registered trademarks are the property of their respective owners.