Many robotics teams eventually confront the same question: the silicon looks promising, the benchmark numbers are compelling, and the demo runs cleanly. So why does it still take eighteen months to get a deployable robot out the door? The answer is rarely the processor. It is everything that surrounds it.
The real question for autonomous robotics developers today is not which compute module offers the highest peak throughput. It is ‘how do we get from a pile of promising silicon to a working, validated, production-oriented robot faster?’
From Microcontrollers to AI-Enabled Compute: The New Autonomy Stack
Autonomous robotics architectures are changing. Systems that once ran on distributed microcontrollers, with each managing a narrow slice of sensing, motion, or communications, are converging toward a more centralized, AI-enabled robotics compute.
The AMD Kria™ AI Robotics Developer Platform reflects this shift. It offers a turnkey, open, and fully integrated platform for autonomous robotics, addressing the full robotics spectrum, from factory robots and AMRs to mobile manipulators and humanoids. The Kria AI Robotics Developer Platform accelerates developers’ path from concept to design and prototype. The compute power comes from the Kria AI SOM, which features a CPU, iGPU, NPU and unified memory resources on a single, integrated device. An FPGA and an ADI sensing and connectivity stack complement the SOM in the offering.
The platform is supported by the AMD Robotics Software Suite built on AMD ROCm software. It features an open-source runtime stack, including Linux, ROS 2, PyTorch, TensorFlow, Docker, and hardware-accelerated perception libraries that developers are familiar with.
That familiarity matters. For many robotics programs, x86 Linux is not a compromise; it is the right development environment, and teams move faster when they are not wasting time learning proprietary SDKs.

The Integration Challenge That Slows Robotics Programs
Even on a capable compute platform, integration work consumes vast amounts of time that has nothing to do with autonomy. These challenges are well-understood, yet each one must be solved from scratch on new hardware designs. Five common challenges often emerge across projects:
1) Multi-Camera Wiring Complexity
Robots that rely on visual perception often need four, six, or more camera feeds. Managing the cabling for that many sensors while maintaining signal integrity, time-alignment, per-camera power delivery, and routing everything back to a central compute node — all quickly become a mechanical and electrical design problem in its own right.
2) Localization in Real Environments
Inertial sensing is essential where cameras and LiDAR degrade, such as low-light warehouses, reflective floors, and featureless corridors. Integrating a high-stability IMU with correct timestamping and ROS 2 driver support is more than a procurement decision; it is a calibration and software integration effort.
3) Depth Processing Overhead
Depth sensors generate dense 3D data that must be filtered, aligned, and fused with other sensor streams in real time. Without hardware-accelerated pipelines, this work competes directly with navigation and planning on the host CPU.
4) Safety-Critical Motion Control
Precise actuation requires more than sending velocity commands over a bus. Motor-control interfaces, isolated field-bus connections, encoder feedback, and current sensing must all be integrated and validated as a system under the vibration and temperature variation of real deployment.
5) ROS 2 Bring-Up Time
The most underestimated cost in any robotics program is the time required to expose hardware subsystems through ROS 2. Every sensor and actuator needs a driver, a hardware binding, a ROS 2 node, tested message types, and validated timing. Teams building from commodity boards write all of this themselves.
The result: teams waste valuable time selecting parts, building carrier hardware, porting Linux drivers, validating sensor timing, wiring cameras, and exposing interfaces to ROS 2, one subsystem at a time.
A Robot-Ready Nervous System, Not Just a Brain
AMD is taking a different approach to enabling autonomous robotics, by combining its new Kria AI Robotics Developer Platform with solutions from ADI. Rather than optimizing a single layer and leaving the rest to the developer, the collaboration delivers what a robot actually needs: a verified, system-level foundation that functions like a nervous system, not just a brain.
The Kria AI SOM is paired with an open robotics carrier card design, enabled by ADI, that features an FPGA and common robotics interfaces. These include high-speed camera connectivity with Gigabit Multimedia Serial Link (GMSL™) (a proven solution from the automotive space), inertial sensing, CAN-FD, RS-485, gigabit and multi-gigabit Ethernet, Automotive Audio Bus (A2B) for low latency audio transport., battery-management hooks, and motor-control expansion.
The standardized COM-HPC-style architecture means developers are not locked into a one-off carrier design. When compute requirements change, teams migrate the SOM, while the rest of the platform stays intact.
As autonomous robots mature to real-world deployment, safety and reliability are no longer an option. Robots must overcome vision-degraded environments, which is where the ADIS16607 IMU from ADI shines. ADI’s research in advanced sensor fusion shows promising results significantly improving system robustness on leading datasets when combining vision with IMU as a second modality.
The compute story goes beyond raw TOPS. Robotics workloads are mixed: low-precision transformer inference for perception models, support for high-precision classical algorithms, numerical optimization, calibration, and development workflows. The integrated x86 GPU and NPU architecture in the AMD Kria AI SOM is designed to handle both.
ADI contributes the robot’s physical interfaces into the platform: high-stability inertial sensing, deterministic depth processing, long-reach camera links that consolidate multiple feeds over single coaxial runs, isolated industrial communications for motor control, and battery-management reference designs for 48 V robot power.
Starting From a Validated Foundation, Not a Blank Slate
The most important story emerging from the platform is also the simplest: customers are not starting from a blank Linux slate.
The AMD Kria AI Robotics Developer Platform provides a pre-validated hardware and software base with ADI drivers already integrated. Interfaces are characterized, the ROS 2 environment is ready, and the path from development kit to production SOM to deployed robot system is documented. Developers can start building autonomy on day one instead of spending their first weeks on carrier board bring-up.
For many programs, that head start is measured in months.
The Future is a More Complete System
The robots deployed in warehouses, factories, and logistics operations today are not held back by compute benchmarks. They are held back by the time and cost of building everything around the compute. Yes, there is always room to run more AI, but the underlying layers have been a patchwork for too long.
ADI and AMD are building the platform that solves that integration problem: a robot-ready nervous system with validated compute, sensing, connectivity, motor control, and ROS 2 software, designed to work together from day one. If your team is moving from prototype to production, we want to help you get there faster. Visit https://www.amd.com/en/products/system-on-modules/kria/ai/robotics-developer-platform.html