Dual DC/DC Controller for DDR Power with Differential VDDQ Sensing and ±50mA VTT Reference

2012-06-01

Figure 1

   

Introduction

The LTC3876 is a complete DDR power solution, compatible with DDR1, DDR2, DDR3 and DDR4 lower voltage standards. The IC includes VDDQ and VTT DC/ DC controllers and a precision linear VTT reference. A differential output sense amplifier and precision internal reference combine to offer an accurate VDDQ supply. The VTT controller tracks the precision VTTR linear reference with less than 20mV total error. The precision VTTR reference maintains 1.2% regulation accuracy, tracking one-half VDDQ over temperature for a ±50mA reference load.

The LTC3876 features controlled on-time, valley current mode control, allowing it to accept a wide 4.5V to 38V input range, while supporting VDDQ outputs from 1.0V to 2.5V, and VTT and VTTR outputs from 0.5V to 1.25V. Its phase-locked loop (PLL) can be synchronized to an external clock between 200kHz and 2MHz. It also features voltage-tracking soft-start, PGOOD and fault protection.

High Efficiency, 4.5V to 14V Input, Dual Output DDR Power Supply

Figure 1 shows a DDR3 power supply that operates from a 4.5V to 14V input. Figure 2 shows efficiency curves for discontinuous and forced continuous modes of operation.

 

1.5V VDDQ/20A 0.75V VTT/10A DDR3 Power Supply

Figure 1. 1.5V VDDQ/20A 0.75V VTT/10A DDR3 Power Supply

 

 

Effi ciency of Circuit in Figure 1 (VDDQ = 1.5V, fSW = 400kHz, L = 470nH)

Figure 2. Efficiency of Circuit in Figure 1 (VDDQ = 1.5V, fSW = 400kHz, L = 470nH)

 

Load-Release Transient Detection

As output voltages drop, a major challenge for switching regulators is to limit the overshoot in VOUT during a load-release transient. The LTC3876 uses the DTR pin to monitor the first derivative of the ITH voltage to detect load release transients. Figure 3 shows how this pin is used for transient detection.

 

Functional Diagram of DTR Connection for Load Transient Detection

Figure 3. Functional Diagram of DTR Connection for Load Transient Detection

 

The two RITH resistors establish a voltage divider from INTVCC to SGND, and bias the DC voltage on the DTR pin (at steady-state load or ITH voltage) slightly above half of INTVCC. For a given CITH1, this divider does not change compensation performance as long as RITH1/ RITH2 equals RITH that would normally be used in conventional single-resistor OPTI-LOOP® compensation.

The divider sets the RC time constant needed for the DTR duration. The DTR sensitivity can be adjusted by the DC bias voltage difference between DTR and half INTVCC. This difference could be set as low as 100mV, as long as the ITH ripple voltage with DC load current does not trigger the DTR. If the load transient is fast enough that the DTR voltage drops below half of INTVCC, a load release event is detected. The bottom gate (BG) is turned off, so that the inductor current flows through the body diode in the bottom MOSFET.

Note that the DTR feature causes additional losses on the bottom MOSFET, due to its body diode conduction. The bottom FET temperature may be higher with a load of frequent and large load steps—an important design consideration. Test results show a 20°C increase when a continuous 100%-to-50% load step pulse chain with 50% duty cycle and 100kHz frequency is applied to the output.

VTT Reference (VTTR)

The linear VTT reference, VTTR, is specifically designed for large DDR memory systems by providing superior accuracy and load regulation for up to ±50mA output load. VTTR is the buffered output of the VTT differential reference resistor divider. VTTR is a high output linear reference, which tracks the VTT differential reference resistor divider and equals half of the remote-sense VDDQ voltage.

Connect VTTR directly to the DDR memory VREF input. Both input and output supply decoupling are important to performance and accuracy. A 2.2μF output capacitor is recommended for most typical applications. It is suggested to use no less than 1μF and no more than 47μF on the VTTR output. The VTTR power comes from the VTTRVCC pin. The typical recommended input VTTRVCC RC decoupling filter is 2.2μF and 1Ω. When VDDQSNS is tied to INTVCC, the VTTR linear reference output is 3-stated and VTTR becomes a reference input pin, with voltage from another LTC3876 in a multiphase application.

 

Load Release Comparison

Figure 4. Load Release Comparison

 

VTT Supply

The VTT supply reference is connected internally to the output of the VTTR VTT reference output. The VTT supply operates in forced continuous mode and tracks VDDQ in start-up and in normal operation regardless of the MODE/PLLIN settings. In start-up, the VTT supply is enabled coincident with the VDDQ supply. Operating the VTT supply in forced continuous mode allows accurate tracking in start-up and under all operating conditions.

Conclusion

The LTC3876 is a complete high efficiency and high accuracy solution for DDR memory power supplies. The unique controlled on-time architecture allows extremely low step-down ratios while maintaining a fast, constant switching frequency. The wide input voltage range of 4.5V–38V and programmable, synchronizable switching frequency from 200kHz to 2MHz gives designers the flexibility needed to optimize their systems.

关于作者

Ding Li

关联至此文章

产品

产品分类

资源

最新视频 21

Subtitle
了解更多