概览

优势和特点

  • AD9083 的全功能评估板
  • 使用 ACE 软件进行控制的 PC 软件
  • AD9528 的板载时钟用于管理套件和 FPGA 时钟
  • 选择切换到外部直接时钟

产品详情

AD9083EBZ评估板提供在各种模式和配置下运行AD9083所需的全部支持电路。还介绍了用于与这些器件接口的应用软件。AD9083EBZ评估板连接至ADI的ADS8-V3EBZ,使用ACE软件进行评估。

ACE软件允许用户在多种模式下设置AD9083,并捕捉模数转换器(ADC)数据实施分析。

软件

驱动/参考代码

API Device Drivers

设计工具

Companion Transport Layer RTL Code Generator Tool (Rev. 1.0)
This command line executable tool generates a Verilog module which implements the JESD204 receive transport layer. The user specifies in a configuration file one or more modes to be supported by the transport layer module. These modes are defined as a set of JESD204 parameter values: L, M, F, S, N', and CF. The transport layer converts JESD204 lane data output from a JESD204 link layer IP to a data bus with a fixed width, containing interleaved virtual converter samples. Both JESD204B and JESD204C link layers are supported.
JESD204x Frame Mapping Table Generator
The JESD204x Frame Mapping Table Generator tool consists of two Windows executables that will allow the user to input any valid combination of JESD204x parameters (L, M, F, S, NP) in order to output a .csv file that illustrates the frame mapping of the JESD204x mode in table format. There is an executable that allows the user to input a single JESD204x mode and another, that allows the user to input the parameters for multiple JESD204x modes in a specified .csv format in order to output a .csv file that illustrates the frame mapping of each of the JESD204x modes that were input into separate tables.

ACE软件

ZIP
26 MB
ACE plug-in for Board.AD9083 1.2021.29300 [Aug 16 21]
Plugin to evaluate the AD9083EBZ evaluation board for the AD9083 high-speed ADC.
EXE
122 MB
ACE Installer Software 1.26.3240.1417 [Jun 21 22]
Analysis | Control | Evaluation (ACE) Software. Requires internet access. Run this executable to install ACE onto your computer. Required before installing the plug-in(s) above. Once ACE is installed, double-click on the plug-in package to install the plug-in.

硬件 (2)

控制器板

在线购买

所示报价为单片价格

所示报价为单片价格。所列的美国报价单仅供预算参考,指美元报价(每片美国离岸价),如有修改恕不另行通知。由于地区关税、商业税、汇率及手续费原因,国际报价可能不同。