利用5G

5G尚处于发展早期,推出的首批商用网络之一为数百万用户提供下一代电话服务。但这只是5G应用的冰山一角。让所有事物都实现互联会彻底改变其本质,从而打造一个充满全新可能的新世界。利用5G应用,未来可能会出现哪些突破性的市场应用?就像一条正在建设中的高速公路,您不知道一旦建好,会涌现哪些类型的业务,或者会如何改变我们的生活。

以下,我们从当前的角度,开始解析5G的未来。


5G可能造成的影响,作者:Joe Barry

Joe Barry介绍了ADI对利用新5G市场应用的影响。凭借出色的技术专业知识、深厚的客户伙伴关系,以及预测未来市场需求的能力,ADI在利用5G方面发挥重要作用。

打造未来的工厂

Enabling the Factory of the Future

5G无线网络可以帮助工厂实现更高的可靠性,缩短延迟时间,提高效率。在人与机器人共存的世界里,更强的连接可以改善人机互动,并降低事故风险。

为农村地区提供高质量的医疗服务

Delivering High-Quality Healthcare to Rural Areas

通用5G连接可以借助可穿戴生物传感器对患者实施远程监测,进行生命体征检测,并将信息传输给基于云的诊断引擎。该系统接收、解析信息,在出现异常信号时迅速采取行动——挽救生命。

推动全自动驾驶汽车的发展

Driving Progress Toward Fully Autonomous Vehicles

5G的实时速度可以做到将车辆外的信息,例如车流模式、路上行人、其他车辆,甚至路况等信息进行综合分析。由此,提高安全性和挽救生命。

5G环境和救生优势

5G’s Environmental and Lifesaving Benefits

ADI认为,在未来采用5G时,远程监测将有助于确保清洁用水,减少食物短缺,并通过及时发出洪水、地震和泥石流预警来改善公共安全。


无论未来如何发展,ADI公司将始终帮助创新者重新设计系统,解锁商业模式,以及发展新兴应用。ADI不仅推动2G、3G和4G通信发展,为每一项大型5G现场测试提供助力,还创造领先技术,让5G成为现实

随着突破性应用不断涌现,富有远见的企业也拥有了更多改变世界的机会。在这个新世界中创新会遇到许多复杂挑战,为了应对这些挑战,就需要与了解市场情况,具备深厚的领域知识和工程团队的合作伙伴合作,以帮助厘清5G变革的复杂性。50多年以来,ADI始终在面向未来创新,且专注于交付核心传感和测量技术,以更快的速度、更低的成本和更低的风险将新的5G应用推向市场。

5G不止是提供更快的视频流传输

5G的发展潜力将会重塑现有市场,并开拓新的市场。最令人振奋的是可能实现高质量医疗,创建人与机器人和谐共存的环境,并且加速实现安全的全自动驾驶汽车。

阅读ADI CEO Vincent Roche发布的文章

Three Ways 5G Is More Than Just Fast Video Streaming

2020 5G趋势和预测

ADI无线系统总经理Alberto Van Burgh表示,2020年将为5G推出带来重大进展,并对全球商业产生广泛影响。Van Burgh先生预测了B2B和B2C行业的新机遇,包括专用网络的大规模扩张,工厂环境中机器人的先进用途以及家庭快速互联网的固定无线接入。

了解接下来会发生什么

5G Trends and Predictions for 2019 from Analog Devices