| タイトル |
コンテンツの種類 |
ファイル形式 |
|
ADN2816: Continuous Rate 10 Mb/s to 675 Mb/s Clock and Data Recovery IC Data Sheet (Rev C, 02/2012) (pdf, 447 kB)
|
データシート |
PDF
|
|
AN-657: ADN2812 Evaluation Board
(pdf, 690 kB)
|
アプリケーション・ノート |
PDF
|
|
Clock and Data Recovery ICs Ease Optical Network Design
|
関連記事 |
HTML
|
CDR ICs Accommodate Changing Bit Rate Requirements
(eeProductCenter, 2/8/2005)
|
関連記事 |
HTML
|
|
RFシステムの開発の簡素化と設計期間を短縮するRF設計ツールの新バージョンを発表 (02 Jun 2011)
|
プレス・リリース |
HTML
|
|
クロック&タイミング
|
メディア掲載一覧 |
HTML
|
|
Clock and Timing ICs
(pdf, 4970 kB)
|
メディア掲載一覧 |
PDF
|
|
Rarely Asked Questions...アナログ・デバイセズに寄せられた珍問/難問集
|
RAQ(珍問/難問集) |
HTML
|
|
外形寸法図のBSCとは?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Pwr Dissとは?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
ICの寿命や製品保証の資料は?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
デシケータ管理条件
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
使用温度の規定の見方は?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why do I see reference spurs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why is my phase noise shape changing when I change the PLL settings?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why doesn't the PLL make my reference input and the clock outputs line up?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I optimize my PLL loop for the best phase noise and/or jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
My loop is not locking. How do I debug this?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How long does it take for the PLL to lock?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Help! My PLL came unlocked over temperature.
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I choose between active and passive filter in PLL loop?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Should I reference the passive filter to ground? or supply?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do the PLLs in the AD951x parts compare to other ADI PLLs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How does the clock clean-up function of the AD951x parts work?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why do I want to run a fast PFD frequency?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is it ok for me to connect the same power supply to both the charge pump and distribution power supply pins?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why can't I use a bandpass filter for my loop filter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Should I tie my loop filter to ground or PLL supply?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
The loop filter was working great until I changed the divide ratio in PLL. What happened?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I use a VCO with a supply greater than 5V?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What suppliers do you recommend for VCO/VCXOs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Do VCXOs have better phase noise and jitter performance than VCOs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I know which VCO will work best with the AD9510?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is there an advantage to running a higher VCO frequency than the output frequency?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I determine if a VCO is good enough for my purpose?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is there any difference between the nature of an oscillator's phase noise and the phase noise from a clock chip?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Do different divide ratios cause variations in jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I have a clocking scheme which requires several different division ratios simultaneously. I have a frequency plan, but I'm concerned about crosstalk. How much of a problem is this with your clock distribution chips?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Do divide ratios change the propagation delay?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I want to use the phase offset feature on the AD9510 dividers to generate two signals 90° out of phase. How accurate is the phase offset?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
On the AD951x clock ICs, does the phase offset (coarse delay) affect the jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why doesn't the mini-divider support the divide ratio I want?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I want to use the variable delay adjust, but the jitter is too high. What can I do?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I changed the coarse phase adjust in the evaluation software, but nothing happened. What's going on?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the difference between the coarse phase adjust and the fine delay adjust?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the fine delay adjust which is available on certain LVDS/CMOS outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Does the fine delay adjust affect the jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why is the fine delay adjust not available on all the outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is there a way to cause Input/Output rising edges to be synchronous (zero delay) with the AD9510/11?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Will the AD9510 work without a reference input signal?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What are the best clock sources for a distribution-only design?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I am not using the CLK1 input on the AD9510. Can I just leave it floating?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How good does my input signal need to be?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I turned off my reference but the Digital Lock Detect (DLD) still says I'm locked.
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I shift the threshold on clocks for single-ended inputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
The reference input is differential, but my reference is single-ended. Do I need to convert to differential to drive the AD9510?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Will differential or single-ended inputs/outputs improve my jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why should I use differential rather than single-ended?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I feed a single-ended signal into a differential input?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why do you recommend AC coupling, rather than DC coupling, at the clock inputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Are the ADI clock parts stand-alone clock sources or do I still have to buy a clock source to drive these parts?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Which provides better performance - a clock source with sinewave output, or one with differential square wave outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
On the AD9510, what is the relationship between clock output jitter and CLK1/CLK2 input slew rate?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I'm trying to write to the part in single-byte mode, but I can't write anything. What am I doing wrong?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I use the 951X clocks to drive a mixer (RF LO)?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
My applications are RF, not for clocking data converters. Can ADI's 951X ICs be used for RF applications?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I have an input present at the clock input, but I'm not seeing an output?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What happens to the AD9510/11 clock outputs if the Reference Input (REFIN) signal goes away?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What clock frequency comes out of the AD9510 outputs when you first apply power to the device?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is it possible to impedance match a clock output if it is heavily loaded? (e.g. CL=100pF)
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I ran the AD9510 outputs at 1.4 GHz and they seem to work fine. Is there a problem running them at 1.4 GHz?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What should I do with unused channels on the AD9510?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I tri-state the AD9510 outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
On the AD9510, how can I make sure that the duty cycle of output clocks stays within 40% to 60% duty cycle window?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the effect of distributing harmonically related clocks (on chip or on board) in terms of jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is there any reason to use a transformer on a differential clock output to obtain a "clean" single-ended clock output?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What are some of the advantages/disadvantages of using LVPECL vs. LVDS outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Does the AD9510 support 2.5V PECL?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How much bandwidth is required to process a PECL or LVDS output?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
If I use only one of the PECL differential outputs and the unused output is terminated in 50Ω, how will this affect the phase noise or jitter of the single-ended output?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
If I change the level of PECL output, does it affect the jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the best way to terminate LVPECL outputs to get lowest jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is it okay to AC-couple PECL or LVDS outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the fan-out capability of the CMOS, LVDS, and LVPECL outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What is the proper termination (value and location) for outputs?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Are outputs short-circuit protected?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Are the CMOS drivers on the clock devices complementary?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Some of the schematics in the AD951x data sheets show an LVPECL termination scheme which is different from the classic termination often seen (50 Ω to Vs - 2V, or the Thevenin equivalent thereof). How does this work, and how did you chose 200 Ω for the resistors? Can I use 100 ohms to improve the slew rate (or jitter)?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I have pulled SYNCB low, but I still have output from a channel. Why?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why can I not get the same output amplitude or rise and fall times as stated in your datasheet?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
The AD9510 datasheet says to use an external pull-up resistor on the FUNCTION pin. Why do I need this and what range of resistors will work?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
May I use the AD9540 for spread spectrum clocking?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I get two clock outputs from the AD9540?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What's the advantage of a DDS-based clock generator?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why does the AD9540 require special filtering on its analog output. What are the requirements of this filter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I'm working with optical networks - SONET/SDH. Do ADI's clock chips support these applications?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
On my board, I can't get the same low jitter numbers that are shown in the datasheet. Am I doing something wrong?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do you determine the bandwidth over which phase noise is integrated to obtain jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Using the "ADC SNR method", what is the equivalent bandwidth for the jitter specification?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do harmonic spurs in the output spectrum affect jitter (random or deterministic)?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
When a jitter number is specified without an associated bandwidth, what bandwidth should be assumed?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do you specify jitter?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I use the clock part for jitter clean-up?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
If jitter can be calculated from phase noise measurements, is it possible to calculate phase noise from jitter numbers?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Does jitter vary with different clock frequencies? How about phase noise?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I sure can't measure jitter with femtosecond resolution on my scope! How do you do it? How much confidence do you have in the jitter figures that you are quoting for these parts?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Do you guarantee performance shown in ADIsimCLK?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Who do I contact for technical support on ADIsimCLK?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Should I use the minimum charge pump current settings in order to minimize power?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I run CMOS outputs at 5V?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Can I use different power supply voltages for the PECL output drivers?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Is .01 uF sufficient for power supply pin bypass?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
My application has pretty tight power consumption requirements. I am very interested in the capabilities of the AD9510, but I don't need every feature. Is it possible to turn off the unused features and save power?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
Why don't you spec psrr and cmrr in the datasheet?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I get two AD951x (with PLL) to synchronize to the same reference input edge?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
I really need >10 clock outputs. Can I use multiple chips together and still guarantee that all output clocks are synchronized to REFIN?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How do I synchronize multiple clock devices?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What happens if I run the part in an ambient environment which exceeds 85°C?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
How can I determine the die temperature of your device?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
My circuit board has both an analog GND and a digital GND. How should I connect the AD9510 pins labeled GND?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
What PCB layout recommendations do you have for the of the exposed paddle on the bottom side of the LFCSP package?
|
FAQ(よくある質問) & RAQ(珍問/難問集) |
HTML
|
|
半導体用語集
|
用語集 |
HTML |