ANALOG DEVICES’ NEW BLACKFIN AUDIO STARTER KIT HELPS REDUCE TIME TO MARKET FOR NEXT-GENERATION AUDIO PRODUCTS

VisualAudio Designer™ Release 2.5 for Blackfin® and SHARC® debuts

AES Convention, San Francisco, CA (10/06/2006) - At the Audio Engineering Society (AES) Convention this week, Analog Devices, Inc. (NYSE: ADI) is tuning into the needs of developers creating next-generation audio applications by introducing the Blackfin® Audio Starter Kit. The starter kit offers a complete package of development software and hardware to enable feature-rich products and fast time to market for embedded audio designs that use Blackfin -- in a spectrum of applications such as premium audio players, personal media players, and professional audio effects processors. The kit features the latest release of Analog Devices’ award-winning VisualAudio Designer™ graphical development tool, also available separately for both Blackfin and SHARC® Processors.

“The new Audio Starter Kit joins our Multimedia Starter Kit, introduced this summer, in an expanding suite of development tools for Blackfin,” said Jerry McGuire, general manager, Convergent Platforms and Services Group, Analog Devices, Inc. “The Blackfin Audio Starter Kit with VisualAudio Designer takes care of the fundamentals so engineers can focus on product differentiation. What’s more, it lets developers experience the advantages of Blackfin in the context of their own applications so they can make informed processor selection decisions early in the evaluation process.”

The 16/32-bit architecture of Blackfin combines control, signal, and multimedia processing in a single core with performance that meets or beats the competition’s DSP product range -- and provides better power, cost, and memory efficiency. As a result, Blackfin has gained adoption in audio-intensive applications including digital home entertainment, networked and streaming media, automotive telematics and infotainment, and digital radio and mobile TV.

Blackfin Audio Starter Kit
The Blackfin Audio Starter Kit software includes the Blackfin SDK (Software Development Kit), which is geared to get projects off to a rapid start by supplying audio algorithms, pre-built binary and source code, fully functional applications, and how-to documentation. Algorithms supported by the starter kit under the appropriate licensing conditions include MP3, WMA, AAC, Dolby Digital (AC3), Dolby Pro Logic IIx, Dolby Virtual Speaker, Dolby Headphone, DTS-ES, DTS Neo:6; Ogg Vorbis and Speex codecs; and high-speed Blackfin and PC communication drivers and utilities. Standard Blackfin development hardware is provided as well: EZ-KIT Lite® evaluation kits and EZ-Extender® daughter boards.

Notably, the Blackfin Audio Starter Kit also includes the company’s award-winning VisualDSP++® integrated development and debug environment (IDDE) and award-winning VisualAudio Designer, a graphical development tool that generates product-ready code optimized for MIPS and memory usage.

The Blackfin Audio Starter Kit will be available in December for the ADSP-BF537. Users that already have the ADSP-BF537 EZ-KIT Lite and the USB-LAN EZ-Extender and Audio EZ-Extender daughter boards may download the Blackfin SDK free of charge. Details are available at http://www.analog.com/processors/platforms/index.html.

VisualAudio Designer 2.5
VisualAudio Designer addresses every step in the typical audio product development cycle, from design through initial tuning, porting to target hardware, final tuning, and automated testing. The main elements of VisualAudio Designer are a PC-based graphical audio design tool with real-time tuning support, a code generation engine with optimized routing and memory allocation, and support for ADI’s EZ-KIT Lite evaluation kit. Source code, detailed documentation, and examples round out its capabilities.

With Release 2.5 of VisualAudio Designer -- also available independently of the starter kit for both ADI’s Blackfin and SHARC Processors -- comes an expanded library of 400+ time-saving audio modules. These range from basics such as mixers, filters, and delays, to specialized algorithms such as decoders, effects, and spectral processing. The audio blocks are highly optimized and make extensive use of processor features such as SIMD (Single Instruction Multiple Data).

Additional improvements introduced in VisualAudio Designer 2.5 include frequency domain and control rate signal types and modules; enhanced support for decoders, encoders, and matrix processors; and an expanded external COM interface.

VisualAudio Designer 2.5 will be available in December. To learn more, visit www.analog.com/visualaudio.

A Convergent Future Demands Blackfin-Class Processing
Analog Devices’ Blackfin embodies a new breed of 16/32-bit embedded processor with the industry’s highest performance and power efficiency for applications where a convergence of capabilities -- multi-format audio, video, voice, and image processing; multi-mode baseband and packet processing; and real-time security and control processing -- are critical. It is this powerful combination of software flexibility and scalability that has gained Blackfin widespread adoption in convergent applications such as digital home entertainment, networked and streaming media, automotive telematics and infotainment, and digital radio and mobile TV.

About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Blackfin, VisualAudio, SHARC, VisualDSP++, EZ-KIT Lite, and EZ-Extender are registered trademarks of Analog Devices, Inc. VisualAudio Designer is trademark of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners.

Editor's Contact Information:

Jessen Wehrwein
781/461-3337

jessen.wehrwein@analog.com

沪ICP备09046653号
Send Feedback X
content here.
content here.

Send Feedback

Close