ANALOG DEVICES INTRODUCES INDUSTRY’S FIRST SINGLE- PACKAGE SOLUTION FOR DATA AND POWER ISOLATION
ADI extends iCoupler® family of digital isolators with a complete solution that dramatically reduces board space and cost for industrial, instrumentation and power applications.
Norwood, MA (03/20/2006) -
Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications, is extending its industry-leading family of iCoupler® digital isolators with the industry’s first products that provide both data and power isolation in a single package. Unlike existing solutions that require the configuration of separate signal and power circuitry involving multiple components, this advancement provides designers of industrial, instrumentation, and power systems with a simple, low-cost, space-saving alternative. The products incorporate ADI’s new proprietary isoPower™ technology that integrates a micro-power supply with independent signal channels. This eliminates the need for complex, sizeable, and costly combinations of optocouplers, transformers and other components, thereby reducing cost by as much as 70 percent and board space by as much as 80 percent.
Announced today, the ADuM5240, ADuM5241 and ADuM5242 are dual-channel isolators incorporating isoPower technology. These new products, provided in 8-lead SOIC (small-outline integrated circuit) packaging, integrate an isolated power supply with two digital signal channels to create a complete isolation solution for low-power applications found in factory automation equipment, instrumentation and secondary control power supplies. In such applications, where designers are under great pressure to reduce size, cost and development time, the ADuM524x product family simplifies the challenge of isolated designs with a single-component solution. As with all iCoupler products, these new devices will carry regulatory safety approvals from the major North American and European agencies upon product release.
“ADI’s iCoupler digital isolation products have a solid five-year track record of safe, reliable operation in a wide variety of applications. Since 2001 when we first introduced the breakthrough iCoupler products, which proved far superior to optocouplers, iCoupler usage has grown to more than 50 million isolation channels in the field,” said Dick Meaney, vice president, precision signal processing group, Analog Devices. “We are now leveraging our iCoupler technology to solve a challenging problem: isolating power along with data in a small space at a low cost. Our new iCoupler products with isoPower capabilities enable customers to achieve these savings as well as reduce development time.”
About the ADuM524x iCoupler Digital Isolators with isoPower Technology
The ADuM524x products incorporate the isoPower technology, which integrates an isolated DC/DC converter with two channels of digital signal isolation in an 8-lead SOIC. Intended for low-power applications, the integrated DC/DC converter provides up to 50 mW of isolated, regulated power at 5 V. The ADuM524x devices operate with a supply voltage ranging from 2.7 V to 5.5 V with the internal DC/DC converter enabled at supply voltages above 4.5 V. The signal channels have excellent timing specifications with propagation delay less than 55 nanoseconds and channel-to-channel matching better than three nanoseconds. All three ADuM24x products carry a 2.5 KV isolation rating.
Each product varies by the directionality of each channel. The ADuM5240 has two signal outputs on the same side as the power output. The ADuM5241, with signal channels in each direction, is ideal for bi-directional communications, such as an RS-232 transceiver, that require isolated power for interface electronics. The ADuM5242, with the two signal outputs on the same side as the power input, is ideal for power supply applications that employ secondary side control and require isolated power to initiate start-up.
About ADI’s iCoupler Digital Isolators
Isolation devices are used in a wide range of applications to protect people and equipment from unsafe voltage levels and disruptive noise sources. Analog Devices’ iCoupler isolation technology employs chip-scale, micro-transformers in contrast to the LEDs and photodiodes used in optocouplers. Compared to optocouplers, iCoupler products consume less power, achieve higher data rates and provide more precise timing, yet still provide isolation ratings of up to 5 kV. Because the micro-transformer structures are integrated on semiconductor substrates, iCoupler products can achieve high levels of integration enabling greater functionality, smaller size and lower cost. Underscoring the scalability and flexibility of the iCoupler technology, isoPower is the latest development in ADI’s digital isolation product portfolio.
Pricing and Availability
The ADuM524x digital isolators are sampling to lead customers now with samples to the open market scheduled for July 2006. Each of the three devices is available in Pb-free 8-lead SOIC packaging and is priced at $2.95 per unit in 1,000-piece quantities.
Analog Devices in the Industrial Market
Analog Devices has a 40-year heritage of working in concert with its customers in the industrial manufacturing industry to define, develop and deploy complete signal chain solutions that are optimized for their applications. ADI’s legacy of supporting the industrial sector’s long product life cycles with multi-year manufacturing commitments is augmented by the company’s educated sales force, knowledgeable field applications engineers and advanced design support tools that include evaluation boards.
About Analog Devices
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.
Editor's Contact Information:
Krys Monaco
781/937-1945
781/937-1026
krys.monaco@analog.com