VARIABLE-GAIN AMPLIFIER SUPPORTS HIGH-SPEED, MULTICHANNEL DATA ACCESS IN ADVANCED CABLE EQUIPMENT

- ADI’s AD8372 VGA features industry-best accuracy, gain control and noise figure, allowing cable providers to keep pace with commercial and residential demands for increased bandwidth.
AD8372

Norwood, MA (02/12/2008) - Analog Devices, Inc. (NYSE: ADI) is introducing a general-purpose two-channel, digitally controlled VGA (variable gain amplifier)(Variable-gain amplifier) developed with specific features for today’s CMTS (Cable Modem Termination System) upstream receiver applications. The two-channel AD8372 VGA enables designers to incorporate more CMTS channels while simultaneously improving modem performance and the quality of upstream cable signals. The new VGA’s space-saving design reduces component count and board area by allowing designers to fit more channels into a given space or pack the same number of channels into a smaller area.

For wide-dynamic-range applications, the AD8372 offers a broad 41-dB gain range, with 1-dB steps and 0.2-dB resolution. The gain is programmed through a bidirectional 4-pin, 8-bit serial port, which consists of clock, latch, data input and data output lines for each channel. The 41-dB control range enables designers to keep input signals above the noise floor, while using the full-scale range of a wider variety of ADCs (analog-to-digital converters). The 41-dB gain range makes the AD8372 an essential component for multiple cable applications, including CMTS

The AD8372, which accepts differential inputs and provides differential outputs, requires no baluns. It provides better than 77-dBc second and third harmonic distortion (HD) and 55-dB common-mode rejection (CMR). Compared to competitive products, the AD8372 delivers 35 percent more gain control range and improved second harmonic distortion in roughly 20 percent of the board space.

Availability and Pricing
The AD8372 amplifier is now shipping in production quantities and is available in a compact, thermally enhanced 5-mm × 5-mm 32-lead LFCSP (lead-frame chip scale package). The device operates over a temperature range of –40 degrees Celsius to +85 degrees Celsius. The AD8372 is priced at $6.50 per unit in 1,000-piece quantities. For more information, visit http://www.analog.com/pr/AD8372.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Editor's Contact Information:

Linda Kincaid
781-937-1472

linda.kincaid@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close