Norwood, MA (09/29/2009) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal processing applications, today expanded its Advantiv® advanced television portfolio with the introduction of the first HDMI™ 1.4 (High-Definition Multimedia Interface™) transceiver for home and pro (professional) AV (audio/video) designs. ADI’s ADV7623 HDMI 1.4 transceiver incorporates Xpressview™ fast switching technology, which enables seamless, automatic switching between HDMI-enabled AV devices in a fraction of a second, eliminating up to 19 seconds of delay required by many AV systems. Designed for home theater-in-a-box (HTIB) systems, AVRs (audio/video receivers), HBR (high-bit-rate) TV, pro-AV matrix switches, and sound bar speaker systems, the ADV7623 is the only HDMI 1.4 device to integrate a 4:1 multiplexed input HDMI receiver, HDMI transmitter, and CEC (Consumer Electronics Control) buffer and controller into a single platform. Unlike competitive offerings that require multiple components, ADI’s single-chip HDMI 1.4 transceiver lowers component and board costs by 33 percent, while supporting advanced features such as OSD (on-screen display) and ARC (audio-return channel) traditionally reserved for higher priced entertainment systems.
“The ADV7623 HDMI 1.4 transceiver with Xpressview fast switching technology significantly reduces the cost, development time and complexity of home AV design,” said Martin Cotter, product line director, Advanced Television Segment, Analog Devices. “With its high-level of integration and feature-rich interface, the ADV7623 fills the considerable void between expensive, multi-chip home AV offerings and less integrated solutions that leave much of the HDMI testing and cost burden to the designer.”
Single-Chip HDMI 1.4 Transceiver Simplifies Home and Pro AV Product Design
By combining the HDMI receiver, HDMI transmitter, CEC, OSD and ARC functions on a single chip, ADI’s new transceiver relieves much of the design work involved in interfacing multiple chips together in HDCP (high-bandwidth digital content protection) repeater designs. The ADV7623 HDMI 1.4 transceiver features a complete SDK (software development kit) that includes ADI’s proven repeater driver libraries.
ADI’s Xpressview™ Fast Switching Enhances Home and Pro AV Performance
ADI’s Xpressview fast switching technology enables home AV electronics to switch between any four HDMI input ports in less than one second, eliminating the 15 to 19 second content protection authentication delay required by home AV systems such as DVRs (digital video recorders), STB (set-top boxes), game consoles and HD camcorders. ADI’s Xpressview fast switching technology minimizes software overhead, further reducing design costs and complexity.
Advanced HDMI 1.4 Functions Enhance AV Delivery and Display
The ADV7623 is the first HDMI transceiver to integrate OSD, enabling AV equipment makers to easily and affordably implement on-screen features and menus across an entire line of HDMI-enabled home AV products. ADI provides a complete OSD software development toolkit. The ADV7623 incorporates HDMI 1.4 standard features and color formats into consumer AV designs, with support for 3D TV video and HDTV formats up to 1080p. The ADV7623 additionally features the new HDMI 1.4 audio feature, ARC, which enables AVRs and other AV equipment to receive audio directly from an HDTV over the existing HDMI cable, eliminating the expense of an extra cable for audio connectivity.
Support for all HDMI 1.4 Audio Standards
The ADV7623 provides complete audio support for eight channels of I2S audio, S/PDIF (Sony/Philips Digital Interface Format) digital audio output, SACD (super audio CD) and compressed SACD with DSD (direct stream digital), and DST (direct stream transfer ) output interfaces. The HDMI transceiver also supports HBR audio streaming to allow recovery (and downstream processing) of compressed lossless audio formats, including Dolby® TrueHD and DTS-HD Master Audio™ or DTS-HD™ High Resolution Audio. The range of formats supported, in addition to the dedicated, flexible audio input and output ports, make the ADV7623 ideal for integration into advanced audio consumer products.
The ADV7623 is compatible with other Analog Devices components including Advantiv advanced television solutions portfolio HDMI switches, Blackfin® and SHARC® Processors, ADI's SoundMAX® portfolio of audio algorithms and codecs, and ADI's power-management ICs.
Availability and Pricing
per 1,000 |
||||
| ADV7623 | 144-lead LQFP |
For more information on ADI’s ADV7623, Advantiv advanced television solutions portfolio or Xpressview fast switching technology, visit http://www.analog.com/pr/ADV7623 and http://www.analog.com/pr/advantiv.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Advantiv, Blackfin, Sharc and SoundMAX are trademarks and Xpressview is a registered trademark of Analog Devices, Inc. All other trademarks are the property of their respective owners.
Follow ADI on Twitter at http://www.twitter.com/ADI_News.
Sue Martenson
781/937-1989
sue.martenson@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved