Norwood, MA (09/28/2009) - Analog Devices, Inc. (NYSE: ADI) today announced that UTAS, a provider of medical devices for patient monitoring and diagnostics, has selected ADI Blackfin® processors to ensure high-performance digital signal processing operations and robust functionality across its full line of products – highlighted by UTAS’ most recent product introduction, the UM 300 portable patient monitor. Leveraging Blackfin’s performance, low power consumption and flexible peripheral connectivity alongside complementary precision analog components also from ADI, UTAS achieved high-performance operations and a seamlessly connected signal chain in a cost effective, compact system package.
“Medical professionals depend on UTAS’ equipment to get a clear view of patient data, which enables them to make timely, more informed patient care decisions,” said Valeriy Tkachenko, Technical Director, UTAS Company. “With Blackfin at the heart of our patient monitoring and diagnostics systems, we are assured a powerful, flexible processor platform for our system designs, and our users are assured unmatched digital signal processing performance for precise measurement of patients’ vital signs.”
UTAS’ electrocardiographs, patient monitors, and pulse oximeters are distinguished by their measurement precision, reliability and affordability, and feature compact form factors and support for battery operations to ensure ease of portability. Utilized in hospitals, clinics, and emergency vehicles in more than twenty-five countries around the world, UTAS’ systems are designed for use across a broad range of patient care applications, including surgery, cardiology, intensive care, bedside care, and patient transport.
The UM 300 patient monitor leverages a dual-core Blackfin BF561 for centralized digital signal processing – real-time digital filtering, preprocessing and finish processing – as well as to control the system’s measurement virtualization capabilities and its video interface, which enables simultaneous viewing of up to eight real-time waveforms via a high-resolution color display. Blackfin BF561 is a symmetric multiprocessing configuration of two Blackfin cores, each of which is capable of operating at up to 600 MHz/1200 MMACS with 2.6 Mb of on-chip SRAM memory. Extremely high bandwidth is provided by the 32-bit external port and dual 16-channel DMA controllers. With two Blackfin cores integrated within the BF561 architecture, UTAS was afforded significant space savings which further helped to minimize design complexity and realize the UM 300’s compact form factor.
The Blackfin BF561 features on-chip, application-tuned peripherals that provide direct connectivity to an ADI AD7190 sigma-delta analog-to-digital converter (ADC) and AD7689 PulSAR® ADC within the UM 300. The system also utilizes ADI AD8605 single-supply operational amplifiers, AD8220 junction field effect transistor (JFET) input instrument amplifiers, an ADP3335 precision voltage regulator, and an ADuM2401 iCoupler® quad-channel digital isolator, comprising a seamlessly interconnected, high-performance component platform.
Blackfin processors are equipped with a range of innovative architectural features that reduce their power consumption at both the processor level and the system level, including a self contained dynamic power management scheme whereby the operating frequency and voltage can be independently manipulated to meet the performance requirements of the algorithm currently being executed. With power consumption starting as low as 0.15 mW/MMAC at 0.8 V, Blackfin’s low-power features enabled UTAS’ system designers to maximize the UM 300’s battery life, which is a critical factor for enabling portable operation.
“Medical equipment developers employ some of the most stringent standards in the electronics industry when selecting the components that will underpin their systems,” said Colin Duggan, product line director, GPDSP division, Analog Devices. “UTAS’ new UM 300 patient monitor is just the latest example of how Analog Devices is delivering high performance, feature-rich signal processing technology to enable advanced medical systems designs.”
A Convergent Future Demands Blackfin-Class Processing
Analog Devices’ Blackfin 16/32-bit embedded processors enable engineers to advance the intelligence, functionality and connectivity of any application that benefits from a convergence of digital signal processing and control processing in a unified architecture. Delivering exceptional price/performance and energy efficiency, and complemented by a rich ecosystem of development tools, applications and third-party support, Blackfin is the processor of choice for a wide range of innovative applications including industrial, medical, automotive, security, digital home entertainment and portable devices. Blackfin can be found on Twitter: @Blackfin and/or the LinkedIn Group: Analog Devices Blackfin.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Blackfin ,PulSAR and iCoupler are registered trademarks of Analog Devices, Inc. All other trademarks included herein are the property of their respective owners.
RSS Feed: http://www.analog.com/processors/news/pressreleases/index.html
Jessen Wehrwein
781/461-3337
jessen.wehrwein@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved