ENERGY METERING IC PROVIDES HIGH ACCURACY HARMONIC ANALYSIS FOR ADVANCED POWER QUALITY MONITORING

ADE7880

Norwood, MA (09/14/2011) - Analog Devices, Inc., (ADI) a global leader in high-performance semiconductors for signal processing applications, today introduced an energy metering IC (integrated circuit) that offers real-time harmonic analysis for energy meters and power quality monitoring equipment. Designed for polyphase meters, the ADE7880 energy metering IC offers complete harmonic analysis, including magnitude and phase information, and delivers better than 1 percent accuracy over a dynamic range of 2000:1 up to the 63rd harmonic. The new device is the first to use ADI's proprietary ARTM (adaptive real-time monitoring) harmonic analysis technology, which eliminates the need for custom development of sophisticated digital signal processing and reduces the demands on the system microcontroller.

"The presence of harmonics is a growing concern for energy systems worldwide as excessive harmonic currents can cause overheating of power transformers and false tripping of protective relays," said Ronn Kliger, Energy Group director, Analog Devices. "Harmonic pollution is growing as grid-connected loads and sources increasingly rely on power electronics that generate or consume harmonic power. The ADE7880 enables smart grid systems to accurately monitor harmonic pollution so that corrective action, when necessary, can be taken by utilities and their customers."

ADD Grup, a leading manufacturer specializing in smart meters, recently selected the ADE7880 energy metering IC to enable its new three-phase industrial meter. "Our high-end industrial meter required harmonic analysis along with traditional energy metering and power quality features," said Vladimir Culiuc, head of the Electric Meter Design Department, ADD Grup. "We chose the ADE7880 energy metering IC to build our design because it saved us considerable software development and validation time, which made it possible to meet an aggressive time to market schedule."

The importance of power quality monitoring continues to grow as millions of smart meters are deployed worldwide. According to Pike Research, more than 250 million smart meters will be installed worldwide by 2015. A smart meter accurately measures how much electricity is consumed or generated, and communicates with the local utility for power monitoring, billing, and other purposes. The combination of communications and power quality analysis enable smart meters to become distributed monitoring devices, creating an important diagnostic tool and extending the meter’s value as a deployed fixed asset for the electric utility.

ADE7880 Energy Metering IC Key Features

  • ARTM automatically tracks changes in the fundamental frequency, which eliminates any effects of frequency drift on accuracy of the measurements.
  • For each harmonic, computes the voltage and current rms, power factor, and active, reactive and apparent powers.
  • Computes THD+N (total harmonic distortion plus noise) ratio as well as harmonic distortion as a ratio of the fundamental.
  • Delivers active and reactive energy accuracy better than 0.2% over a dynamic range of 5000:1. Accuracy better than 0.1% is achieved over a dynamic range of 1000:1 with gain calibration only.
  • Incorporates seven sigma-delta ADCs (analog-to-digital converters), a digital integrator, voltage reference and all metrology signal processing. Suitable for class 0.2 meters.

Pricing and Availability

Product Sample Availability Full-Volume Production Price Each in 1,000 Quantities Package
ADE7880 Now November 2011 $9.47 40-lead LFCSP

The EVAL-ADE7880EBZE evaluation board for the ADE7880 is also now available and priced at $390.00. For more information, visit http://www.analog.com/energymeasurement.

Making a Difference for Energy Metering Customers

With more than 350 million energy meters using ADI's technology deployed worldwide, Analog Devices has delivered more energy measurement solutions than any other semiconductor company. Superior in quality, reliability, and performance, Analog Devices’ energy-metering ICs combine ADCs (analog-to-digital converters) with fixed-function DSPs (digital signal processors) to perform critical measurements, while providing unparalleled functionality and ease-of-use. Analog Devices offers a broad range of semiconductor solutions that solve design challenges in every aspect of metering systems, including energy measurement; data and power management; user interface; and RF, GSM/GPRS, and power-line carrier communication solutions. For more information about ADI's energy measurement products, visit http://www.analog.com/pr/Energy-Measurement. For more information about ADI's energy solutions for renewable energy generation, transmission and distribution, and metering applications, visit http://www.analog.com/energy.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Follow ADI on Twitter at: http://www.twitter.com/ADI_News

Subscribe to Analog Dialogue, ADI's monthly technical journal.

Editor's Contact Information:

Linda Kincaid
781-937-1472

linda.kincaid@analog.com

content here.
content here.