ANALOG DEVICES PAIRS 24-BIT SIGMA-DELTA ADCS WITH ARM7™ CORE FOR UNEQUALLED DATA ACQUISITION AND PROCESSING PERFORMANCE

ADuC706x precision analog microcontrollers deliver highest level of data conversion integration and performance.
ADuC706x

Norwood, MA (06/17/2008) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal-processing applications, today introduced a highly integrated microcontroller family with best-in-class data conversion performance for hardware, firmware and industrial systems engineers designing smart sensing, factory automation and instrumentation equipment. The ADuC706x family expands ADI’s precision analog microcontroller portfolio by incorporating two 24-bit sigma-delta analog-to-digital converters (ADCs) and a host of analog peripherals with a 32-bit ARM7™ core to create a solution for precision sensing applications. The unparalleled combination of small size, low operating power and Analog Devices’ industry-leading data conversion design expertise distinguish the ADuC706x from other competitive solutions, eliminating the complexity, cost and performance degradation issues associated with discrete mixed-signal solutions.

“Precision sensing requires a low noise, high resolution signal conversion architecture,” said Mike Britchfield, product line director, Precision Signal Processing, Analog Devices. “With its on-chip 24-bit sigma-delta ADCs, the ADuC706x provides the resolution required by today’s high-performance industrial and instrumentation equipment, while keeping the noise low. This performance, complemented by the simplicity of a single-chip solution, handles all data acquisition, processing and communications functions at the signal source.”

About the ADuC706x Family
Designed for 4–20 mA loop-powered applications in factory automation and for precision instruments, the ADuC706x family includes the ADuC7060 and ADuC7061. The devices feature an industry-best ADC noise performance of just 60 nV—20% better than the nearest competing part—and offer five times more processing power for a given clock rate. In addition to the 24-bit sigma-delta ADCs and ARM7 core with eight interrupt priority levels, the new precision analog microcontrollers incorporate 32 Kbytes of flash memory and 4 Kbytes of SRAM, a programmable gain amplifier, multiplexers, buffers, an auxiliary 24-bit ADC for cold junction compensation and interfacing to thermocouple applications, and SPI (serial peripheral interface), UART (universal asynchronous receivers-transmitters) and I²C ports. The devices consume just 2.6 mA with all peripherals activated.

The ADuC7060, available in a 7 mm × 7 mm 48-pin chip-scale (QFN) package, offers more analog-input channels and general-purpose I/Os than other devices in the family. The ADuC7061 comes in a 5 mm × 5 mm 32-pin chip-scale (QFN) package, ideal for space-constrained applications.

Availability and Pricing
The ADuC706x family is available in sample quantities and will be in full factory production in November 2008. The ADuC7060 and ADuC7061 precision analog microcontrollers are priced at $4.90 and $3.95 respectively, in 1,000-unit quantities. For more information on ADI’s precision analog microcontrollers, visit www.analog.com/pr/ADuC706x.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

ARM7 is a trademark of ARM Limited.

Editor's Contact Information:

Linda Kincaid
781-937-1472

linda.kincaid@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close