Norwood, MA (05/16/2011) - Analog Devices, Inc. (ADI), today introduced the ADG5212 and ADG5213 high-voltage, latch-up proof quad switches that offer guaranteed latch-up protection for industrial, instrumentation, and automotive applications operating at up to ±22 V. Latch-up, an undesirable high-current state that persists until the power supply is turned off, can lead to device failure. The new products, which contain four independent SPST (single-pole, single-throw) switches, achieve the industry’s lowest charge injection (0.07 pC) and 400 pA max leakage.
The ultra-low charge injection of the new switches makes them suitable for data acquisition and sample-and-hold applications, where low glitch and fast settling time are required. Low leakage is an advantage in audio and video signal routing where high accuracy and resolution are important. The ADG5212 and ADG5213 switches are the latest additions to ADI’s switch and multiplexer protection products portfolio, which also includes the ADG5412 and ADG5413 low Ron, 8-kV ESD (electrostatic discharge) latch-up proof quad switches.
| Product | Description | Sample Availability | Full-Volume Production | Price Each in 1,000 Quantities | Package |
|---|---|---|---|---|---|
| ADG5212 | SPST × 4 switch turns on with logic 1 | Now | Now | $2.18 | 4 mm × 4 mm 16-lead LFCSP 16-lead TSSOP |
| ADG5213 | SPST × 4 with inverted logic control | Now | Now | $2.18 | 4 mm × 4 mm 16-lead LFCSP 16-lead TSSOP |
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News.
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
Linda Kincaid
781-937-1472
linda.kincaid@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved