content here.
content here.

ANALOG DEVICES UNVEILS SINGLE-PACKAGE SOLUTION FOR MEDICAL-GRADE DATA AND POWER ISOLATION

- New iCoupler® digital isolation products provide quad-channel data isolation and 500mW power isolation with 5-kV rms isolation rating; new devices reduce both cost and board space by up to 50 percent.

Norwood, MA (05/13/2009) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications, today expanded its broad portfolio of digital isolation products with a family of four-channel devices that meet stringent medical-grade specifications for data and power isolation in patient monitoring and other medical equipment. Each device integrates ADI’s iCoupler® digital isolation technology and proprietary isoPower® dc-to-dc converter, providing both isolated power and isolated signal channels within a single package. These new iCoupler quad-channel isolators are a better choice over discrete solutions, such as optocouplers with external dc-to-dc converters, because they can both cut costs and reduce board space by as much as 50 percent, and speed time-to-market.

About the ADuM640x Quad-Channel Isolator Family
The ADuM640x quad-channel isolator family includes the ADuM6400, ADuM6401, ADuM6402, ADuM6403, and ADuM6404 digital isolation products. The quad-channel isolators offer 5-kV rms medical-grade isolation (IEC 60601-1 approvals pending) and four independent isolation channels in various channel configurations and data rates. The onboard isoPower isolated dc-to-dc converter provides up to 500 mW of regulated, isolated power and can operate at either 5.0 V or 3.3 V. This eliminates the need for a separate, isolated dc-to-dc converter in low-power, isolated designs. The ADuM640x also includes a thermal shutdown feature to ensure safe operation. For more information, please visit http://www.analog.com/pr/ADuM640x.

Also now available is the ADuM440x family of quad-channel digital isolators that feature enhanced system-level ESD (electrostatic discharge) protection with 5-kV rms medical-grade isolation (IEC 60601-1 approvals pending). The ADuM440x family includes the ADuM4400, ADuM4401, and ADuM4402 digital isolation products that differ by channel configuration. For more information, please visit http://www.analog.com/ADuM440x.

Availability, Pricing and Complementary Parts

Product
Available
Unit Price in 1,000-Piece Quantities
Packaging
Channel Configuration
ADuM6400
NOW
$6.33
16-lead SOIC (small-outline integrated circuit) package
4/0
ADuM6401
NOW
$6.33
16-lead SOIC package
3/1
ADuM6402
NOW
$6.33
16-lead SOIC package
2/2
ADuM6403
NOW
$6.33
16-lead SOIC package
1/3
ADuM6404
NOW
$6.33
16-lead SOIC package
0/4
Complementary sigma-delta ADCs (analog-to-digital converters) for the ADuM640x family include the AD7190, AD7192, AD7785, AD7792, AD7793, AD7794, and AD7795. Complementary PulSAR® SAR (successive-approximation register) ADCs include the AD7986, AD7985, AD7689, and AD7656.

iCoupler® Technology
With more than 250 million channels deployed, ADI’s proven iCoupler technology is based on chip-scale transformers, rather than on the LEDs and photodiodes found in optocouplers. Transformers support higher data rates, consume less power, and are more stable over life as compared to LEDs and photodiodes. By fabricating the transformers directly on-chip using wafer-level processing, iCoupler channels can be integrated with each other and other semiconductor functions at low cost. iCoupler transformers are planar structures formed from CMOS and gold metal layers. A high breakdown polyimide layer underneath the gold layer insulates the top transformer coil from the bottom. CMOS circuits connected to the top coil and bottom coil provide the interface between each transformer and its external signals.

isoPower DC-to-DC Converter
iCoupler digital isolators condition and drive data across transformers. ADI’s isoPower dc-to-dc converter uses the same chip-scale transformer technology, but instead of transmitting data, isoPower employs switches, rectifiers, and regulators to generate power that is isolated to the same degree as the data channels.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

iCoupler, isoPower, and PulSAR are registered trademarks of Analog Devices, Inc.

Editor's Contact Information:

Linda Kincaid
Analog Devices, Inc.

linda.kincaid@analog.com