content here.
content here.

ANALOG DEVICES INTRODUCES 18 NEW LOW-POWER ADCS FOR COMMUNICATIONS, INDUSTRIAL, PORTABLE AND INSTRUMENTATION APPLICATIONS

- ADI’s new pin-compatible, low-power, dual-channel ADCs increase channel densities and reduce power consumption; available in multiple speed grades.
Designed for power-sensitive communications, industrial, portable-electronics and instrumentation.

Norwood, MA (04/27/2009) - Analog Devices, Inc. (NYSE: ADI), the global leader in data-conversion technology, introduced today 18 power-efficient analog-to-digital converters (ADC) with resolutions ranging from 10 to 16 bits. Designed for power-sensitive communications, industrial, portable-electronics and instrumentation equipment, ADI’s new ADCs reduce power consumption by as much as 60 percent compared to many competing ADCs, while maintaining best-in-class noise performance and dynamic range. Improved power efficiency enables wireless basestations to operate more cost effectively with better system reliability. Portable medical devices benefit from longer battery life and smaller form factors. Advanced imaging picture resolution is enhanced by increasing data-conversion channel density without adding to the power budget.

“There is a growing trend to reduce total system power with each generation, and in the past, the system designer was left with making power-versus-performance tradeoffs, especially with high speed converters,” said Jon Hall, strategic marketing and applications manager, High Speed Signal Processing, Analog Devices. “Power efficiency is a requirement across a broad range of applications, and so is hitting the target system performance. ADI’s 18 newest ADCs provide low power without sacrificing the high degree of performance the industry has come to expect from ADI.”

The flagship converter in this series, the AD9268, is the industry’s first 125-MSPS (megasamples per second) 16-bit, dual-channel ADC and consumes 376 mW per channel – 60 percent less power per channel than competing devices. The new ADC’s integration and energy savings allow system engineers to increase channel counts without increasing a product’s board area or power consumption, enabling higher call volume in cellular base stations, for example, or improved image resolution in medical magnetic-resonance imaging (MRI) equipment. In handheld and other power-sensitive applications, ADI’s low-power ADCs likewise enable improved system performance while extending battery life in hand-held devices, such as portable spectrum analyzers.

Pin-Compatible, Low-Power, Dual-Channel ADCs Available in Multiple Speed Grades
The AD9268 dual-channel, 16-bit ADC is available in speed grades of 80, 105, and 125 MSPS. The 125-MSPS option achieves 78 dB SNR (signal-to-noise ratio) and 90 dB SFDR (spurious-free dynamic range) to 70 MHz analog input frequency, while consuming 376mW per channel.

Available in a Pb-Free, 9 mm x 9 mm chip-scale package, the AD9268 is pin-compatible with ADI’s other low-power ADCs. This speeds product upgrades, simplifies new-product engineering debug, and improves time-to-market by reducing the number of separate ADC pin-outs that manufacturers must support.

Another converter in the series, the AD9251 is a dual-channel 14-bit ADC and is available in the same 64-lead LFCSP pin-compatible footprint and is offered in speed grades of 20, 40, 65, and 80 MSPS. With 73.5 dB SNR and 85 dB SFDR to 70 MHz analog input frequency, the AD9251 dissipates only 86 mW per channel at 80MSPS, improving power efficiency by more than 50 percent over competing 14-bit ADCs.

All of ADI’s new low-power dual ADCs operate from a single 1.8-V analog power supply and feature a high-performance sample-and-hold circuit and on-chip voltage reference. The AD9251 family offers a separate driver supply to accommodate 1.8-V or 3.3-V CMOS logic outputs, while the AD9268 family offers 1.8-V LVDS or CMOS outputs. The ADC cores use a multi-stage, differential pipelined architecture with integrated output error-correction logic. The ADCs also contain features designed to maximize flexibility and minimize system cost, including programmable clock and data alignment and programmable digital test-pattern generation. The available digital test patterns include built-in, deterministic and pseudo-random patterns, as well as definable test patterns that users can enter via the serial port interface (SPI).

Complementary Products
Analog Devices’ new low-power ADCs are compatible with ADI’s dual-channel VGA (variable gain amplifiers), including the AD8372 programmable dual VGA and AD8376 IF dual VGA as well as the ADL5561 differential RF/IF amplifier and ADL5562 differential RF/IF amplifier. Recommended clock generators include the AD9520-0 and AD9522-0.

Pricing and Availability
ADI’s new low-power dual ADCs are sampling and available in Pb-Free, 9 mm x 9 mm, chip-scale packaging today. Production quantities will be available in June 2009.

Product
Resolution(Bits)
SampleRate(MSPS)
PriceEachPer1,000
PowerConsumption(mW/ch)
AD9204BCPZ-20
10
20
$5.00
33
AD9204BCPZ-40
10
40
$7.20
48
AD9204BCPZ-65
10
65
$7.50
68
AD9204BCPZ-80
10
80
$10.00
82
AD9231BCPZ-20
12
20
$10.00
35
AD9231BCPZ-40
12
40
$12.00
51
AD9231BCPZ-65
12
65
$18.00
71
AD9231BCPZ-80
12
80
$25.00
84
AD9251BCPZ-20
14
20
$18.50
39
AD9251BCPZ-40
14
40
$23.89
54
AD9251BCPZ-65
14
65
$35.00
74
AD9251BCPZ-80
14
80
$37.50
86
AD9258BCPZ-80
14
80
$42.50
182
AD9258BCPZ-105
14
105
$59.50
252
AD9258BCPZ-125
14
125
$80.75
376
AD9268BCPZ-80
16
80
$101.00
182
AD9268BCPZ-105
16
105
$119.00
252
AD9268BCPZ-125
16
125
$136.00
376

Data Converters: Bridging the Analog and Digital Worlds
More designers turn to Analog Devices than any other supplier for the high-performance conversion technology required to bridge the analog and digital worlds in today’s myriad electronic systems. With the industry’s leading portfolio of ADCs (analog-to-digital converters) and DACs (digital-to-analog converters), Analog Devices’ converter products feature the right combination of sampling rates and accuracy with low noise, power, and price and small package size required by industrial, medical, automotive, communications, and consumer electronics. Online evaluation tools help customers quickly validate, select, and design in the optimal data converters to reduce design complexity, development schedules, and bill-of-material costs. To view ADI’s ADC selection guide, visit http://www.analog.com/ADCsearch. For ADC drivers, visit http://www.analog.com/ADCdrivers. To view ADI’s DAC selection guide, visit http://www.analog.com/DACsearch.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' common stock is listed on the New York Stock Exchange under the ticker “ADI” and is included in the S&P 500 Index.

Editor's Contact Information:

Bob Olson
781/937-1666

bob.olson@analog.com