ANALOG DEVICES LAUNCHES HIGHEST DYNAMIC RANGE IF GAIN BLOCK AMPLIFIERS

- New ADL5535 and ADL5536 amplifiers deliver high linearity and low noise figure performance for a variety of intermediate frequency applications.

Norwood, MA (12/17/2009) - Analog Devices, Inc. (NYSE: ADI), a global leader in high-performance semiconductors for signal-processing applications and RF integrated circuits, today announced two new intermediate frequency (IF) gain block amplifiers. The ADL5535 and ADL5536 gain block amplifiers provide the highest dynamic range available from internally matched IF gain blocks by combining best-in-class linearity and noise figure performance. These versatile, multi-purpose broadband IF amplifiers, cover the 20 to 1000 MHz frequency range and are suitable for a variety of applications that require high performance specifications such as in cellular, satellite, CATV, military and instrumentation equipment.

About the ADL5535 and ADL5536 IF Gain Block Amplifiers
The ADL5535 and ADL5536 IF gain block amplifiers provide extremely low noise figures and very high OIP3 specifications simultaneously across the entire 1 GHz frequency range. The ADL5535 gain block amplifier provides an extremely flat gain of 15 dB over frequency, noise figure of 3.3 dB, a P1dB of 19.1 dBm and an output third order intercept point (OIP3) of 47.6 dBm at 190 MHz. The ADL5536 gain block amplifier provides a flat gain of 20 dB over frequency, noise figure of 2.8 dB, P1dB of 19.8 dBm and an OIP3 of 46.5 dBm at 380 MHz. Both amplifiers are internally matched to 50 Ω at the input and output, making these amplifiers easy to implement in a wide variety of applications. Only input/output ac coupling capacitors, power supply decoupling capacitors, and an external inductor are required for operation. The ADL5535 and ADL5536 IF gain block amplifiers are stable over temperature, power supply and from device to device. They are fabricated on a GaAs HBT process and have a robust ESD rating of ±1 kV (Class 1C). These IF amplifiers are assembled in a MSL-1 rated SOT-89 package, making them easy to drop-in into existing designs for evaluation. The ADL5535 consumes only 97 mA and the ADL5536 consumes only 100 mA on a single 5 V supply and are fully specified for operation from −40°C to +85°C.

Pricing, Availability and Complementary Products
The ADL5535 and ADL5536 are available now in a 3-lead SOT-89 package and are priced at $1.75 in 1,000 unit quantities. Complementary products are the ADL535X, ADL536X, and ADL580X families of mixer products. To connect with a specialist, cross reference tools, and more resources on how to use and obtain ADI products, please click here: http://www.analog.com/buy.

ADI’s RF IC Portfolio Covers Entire RF Signal Chain
Using a unique combination of design skills, system understanding and process technologies, Analog Devices offers the broadest portfolio of RF ICs covering the entire RF signal chain from industry-leading high-performance RF function blocks to highly integrated WiMAX and short-range, single-chip transceiver solutions. The RF function blocks include DDS and PLL synthesizers; TruPwr™ rms power detectors and logarithmic amplifiers; X-Amp® VGAs; power amplifiers, LNAs and other RF amplifiers, mixers and direct conversion modulator and demodulator products. These products are supported by a wide range of free design tools to ease the development of RF systems. For more information, visit: http://www.analog.com/rf.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Subscribe to ADI’s News Feed.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

Editor's Contact Information:

Colleen Cronin
781/937-1622

colleen.cronin@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close