ENERGY METERING IC DELIVERS HIGHEST ACCURACY AND PROTECTS SMART METERS AGAINST TAMPERING

- ADE7953 energy metering IC for single-phase meter configurations measures active, reactive and apparent energy along with rms voltage and current.

Norwood, MA (10/25/2010) - Supporting customers around the world who are designing smart meters and implementing smart grid systems, Analog Devices, Inc., a global leader in high-performance semiconductors for signal processing applications, today introduced an energy metering IC (integrated circuit) that enables smart meters to provide stronger protection against electricity theft, improve customer billing accuracy and reduce operating costs for utility companies. The ADE7953 energy metering IC is designed for single-phase meter configurations and can accommodate the electrical needs of homes ranging from small apartments to large residences in which many appliances and electronic devices are used. The new product measures active, reactive and apparent energy along with rms voltage and current. It also provides neutral current measurements that help designers develop tamper-proof smart meters. Download the ADE7953 data sheet or order samples.

“The ADE7953 improves customer billing accuracy, which in turn lowers utility operating costs, such as customer service,” said Ronn Kliger, Energy Group director, Analog Devices. “The neutral current measurement offered by the new device enables designers to develop more tamper-resistant smart meters, which are invaluable to utility companies that are estimated to lose billions of revenue dollars worldwide each year due to electricity theft.”

ADE7953 Single-Phase Multifunction Metering IC Features and Benefits

By achieving less than 0.1 percent error for both active and reactive energy calculations over a dynamic range of 3000:1, the ADE7953 provides the industry’s highest accuracy for single-phase metering applications worldwide. For neutral current, the device offers less than 0.1 percent error active and reactive energy over a 1000:1 dynamic range. Neutral current measurements enable meter tamper detection and improved billing accuracy. The new device also measures apparent energy along with rms voltage and current. Additionally, it provides waveform sampling, instantaneous power readings and power quality indications that include voltage sag, peak voltage and peak current. The ADE7953 incorporates three sigma-delta ADCs (analog-to-digital converters) with a high accuracy metrology engine. Each input channel supports independent and flexible gain stages, making the ADE7953 energy metering IC suitable for use with a variety of current sensors, such as low value shunt resistors and current transformers. Two on-chip integrators also facilitate the use of di/dt sensors for current inputs.

Additional features and benefits include:

  • Rms current and voltage measurements are offered with less than 0.2 percent error over a 500:1 dynamic range
  • Access to on-chip meter registers via a variety of communication interfaces including SPI (serial peripheral interface), I2C or UART (universal asynchronous receiver/transmitter)
  • Two configurable pulse output pins provide outputs that are proportional to active, reactive, or apparent energy, as well as rms current and voltage
  • A full range of power quality information, such as overcurrent, overvoltage, peak and SAG detection are accessible via the external IRQ pin
  • 3.3-V supply operation

Recommended Complementary Components

Recommended complementary components for the ADE7953 energy metering IC include the ADP121 linear regulator, AD7814 temperature sensor, ADuM141x four-channel digital isolators, ADuM120x two-channel digital isolators, ADM2484E RS485 transceiver, ADM6320 supervisory circuit, ADP5022 buck regulator, and ADF7023 RF transceiver.

ADE7953 Pricing and Availability

Sampling Volume Production Package Price Each
per 1,000
NOW January 2011 28-lead LFCSP
(Lead Frame
Chip Scale
Package)
$2.15

Making a Difference for Energy Metering Customers

With more than 250 million energy meters using ADI’s technology deployed worldwide, Analog Devices has delivered more energy measurement solutions than any other semiconductor company. Superior in quality, reliability, and performance, Analog Devices’ energy-metering ICs combine ADCs (analog-to-digital converters) with fixed-function DSPs (digital signal processors) to perform critical measurements, while providing unparalleled functionality and ease-of-use. Analog Devices offers a broad range of semiconductor solutions that solve design challenges in every aspect of metering systems, including energy measurement; data and power management; user interface; and RF, GSM/GPRS, and power-line carrier communication solutions. For more information about ADI’s energy measurement products, visit http://www.analog.com/pr/Energy-Measurement. For more information about ADI’s energy solutions for renewable energy generation, transmission and distribution, and metering applications, visit www.analog.com/energy.

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Subscribe to ADI’s News Feed.

Follow ADI on: http://www.twitter.com/ADI_News.

Editor's Contact Information:

Linda Kincaid
781/937-1472

linda.kincaid@analog.com

Send Feedback X
content here.
content here.

Send Feedback

Close