Norwood, MA (01/26/2011) - Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal processing applications, is providing its highly integrated iCoupler® digital isolation solution to Siemens Aerospace for its PowerSCOE™ system, a sophisticated satellite power protection system that will shut down kilowatts of power within the satellite within microseconds in the case of an anomaly. Serving as the advanced technology group for Siemens AG, Siemens Aerospace designed the system with other applications in mind, such as smart grid power monitoring.
A satellite's power system is critical because any malfunction can seriously damage the spacecraft and derail the mission. "With each channel containing an auxiliary analog input and digital and analog output, the most difficult challenge was ensuring each of 100 channels were individually isolated from each other," said Alfred Fuchs, PowerSCOE project manager, Siemens Aerospace. "With over 100 analog and digital I/Os present, the PCB density we were looking for required a solution beyond traditional optocouplers and DC-to-DC converters. ADI's highly integrated iCoupler digital isolators proved crucial in making our next-generation PowerSCOE protection system viable."
Analog Devices' digital isolators with integrated, isolated isoPower® DC-to-DC converters are based on ADI’s proprietary iCoupler technology. The isolator's integrated DC-to-DC converter provides up to 500 mW of regulated, isolated power at either 5.0 V from a 5.0 V input supply or 3.3 V from a 3.3 V or 5.0 V supply. The iCoupler chip-scale transformer technology is used to isolate four channels of logic signals as well as the power supply, eliminating the need for a separate, isolated DC-to-DC converter in low power, isolated designs. The result is fewer components, a smaller form factor and a more cost effective isolation solution compared to optocoupler-based and discrete solutions. For more information visit http://www.analog.com/isolation
"Delivering 500 mW of isolated power in a small surface-mount package, iCoupler digital isolators enable customers with sophisticated instrumentation challenges, such as Siemens, to put more channels of isolation into space-constrained designs at reduced cost," said David Krakauer, product line manager, Analog Devices. "Using our highly integrated digital isolators, Siemens Aerospace designers were able to increase the number of isolated data ports in a single control module without increasing the size of the module, even though each port requires its own isolated power supply. The PowerSCOE protection board has 170 iCoupler devices. If the alternatives were used, such as optocouplers and separate, isolated DC-to-DC converters, the control module would be much larger than the current dimension of 380 mm x 470 mm."
Siemens' rigorous product optimization strategy includes a broad technology mix that includes platform FPGAs (Field-programmable Gate Array), leading-edge power MOS-FETS, as well as safety relays and high-end PCB artwork. In addition to the iCoupler digital isolators, several other components from the iCoupler product family are used with the Siemens PowerSCOE protection system. These components were selected for their high performance, size and compatibility and include AD7401 isolated sigma-delta modulators, ADUM5000 isolated DC-to-DC converters and ADUM5230 isolated half-bridge gate drivers.
Siemens AG is a global powerhouse in electronics and electrical engineering, operating in the industry, energy and healthcare sectors with around 405,000 employees worldwide. For over 160 years, Siemens has stood for technological excellence, innovation, quality, reliability and internationality. The Siemens space business unit is part of the Siemens Austria segment Communications, Media & Technology, based in Vienna. http://www.siemens.at/space
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
iCoupler and isoPower are registered trademarks of Analog Devices, Inc.
PowerSCOE is a trademark of Siemens AG
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/library/analogDialogue
Howard Wisniowski
781-937-1517
howard.wisniowski@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved