Norwood, MA (11/06/2012) - Analog Devices, Inc. (ADI) today introduced a series of non-volatile single-, dual- and quad-channel digital potentiometers (digiPOTs) that improve component matching in industrial and communication control systems by featuring resistance tolerance of ± 1 percent (typ). The 11 new digiPOTs in ADI’s AD514x and AD512x series also achieve a 3-MHz bandwidth that is 50 percent higher than the closest competitor, which enables faster system response time. The new devices offer the industry’s lowest temperature coefficient performance over the widest temperature range (-40°C to 125°C).
ADI’s non-volatile digiPOT series meets a wide range of system-level requirements in single, dual, or quad, 256-tap or 128-tap, SPI or I²C interfaces, leaded and leadless packaging, all featuring 4 kV ESD protection
| Product | Sample Availability | Channel | Tap | Interface | Price Each In 1,000 Quantities | Packaging |
|---|---|---|---|---|---|---|
| AD5144 | Yes | Quad | 256 | SPI/I²C | $2.90 | 24-lead LFCSP/20-lead TSSOP |
| AD5144A | Yes | Quad | 256 | I²C | $2.90 | 20-lead TSSOP |
| AD5124 | Yes | Quad | 128 | SPI/I²C | $2.50 | 24-lead LFCSP/20-lead TSSOP |
| AD5143 | Yes | Quad | 256 | I²C | $2.85 | 16-lead LFCSP |
| AD5123 | Yes | Quad | 128 | I²C | $2.45 | 16-lead LFCSP |
| AD5142 | Yes | Dual | 256 | SPI | $1.65 | 16-lead LFCSP/16-lead TSSOP |
| AD5142A | Yes | Dual | 256 | I²C | $1.65 | 16-lead LFCSP/16-lead TSSOP |
| AD5122 | Yes | Dual | 128 | SPI | $1.45 | 16-lead LFCSP/16-lead TSSOP |
| AD5122A | Yes | Dual | 128 | I²C | $1.45 | 16-lead LFCSP/16-lead TSSOP |
| AD5141 | Yes | Single | 256 | SPI/I²C | $0.90 | 16-lead LFCSP |
| AD5121 | Yes | Single | 128 | SPI/I²C | $0.70 | 16-lead LFCSP |
The quad-channel AD5144 can be designed into circuits as the gain control for buck/boost controller power supply applications together with ADI’s ADP5034 dual-channel, 3-MHz, 1200-mA buck regulators with two 300-mA LDOs.
Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/
Grainne Murphy
353-61-495540
grainne.murphy@analog.com
© 1995 - Analog Devices, Inc. All Rights Reserved