The EVAL-AD2S1200SDZ is a fully featured evaluation kit for the AD2S1200. This board operates in standalone mode or in conjunction with the System Development Platform, EVAL-SDP-CB1Z . When operated with the System Development Platform software is provided enabling the user to perform detailed analysis of the RDC's performance. The user guide describes the operation and set up of the evaluation board in standalone operation or when operated with the System Development Platform .
The SDP Controller board is a separate list item in the ordering guide below (EVAL-SDP-CB1Z). If you have not previously purchased an SDP Controller board, please do so to ensure a full evaluation setup.
Buy© 1995 - Analog Devices, Inc. All Rights Reserved