Press Release

Contact Linda Kincaid

Analog Devices’ Wideband GaN MMIC Amplifier Offers High Gain, Power and Efficiency in Compact Design

Jun 5 2017 - Norwood, MA
  • HMC8205-PR-Image-RGB-300x300-Title-WebAnalog Devices, Inc. today introduced a wideband gallium nitride (GaN) power amplifier that offers best-in-class performance within a compact design. Covering the 300 MHz to 6 GHz spectrum, the highly integrated HMC8205 provides significant benefits for system designers of applications such as wireless infrastructure, radar, public mobile radio, and general-purpose amplification test equipment that require pulse or continuous wave (CW) support. The HMC8205 GaN MMIC amplifier offers unmatched integration, gain, efficiency, and wide bandwidth in a small footprint that requires minimal external circuitry, thereby reducing overall component count and board space.



    About the HMC8205 GaN MMIC Amplifier
    The HMC8205 combines DC feed/RF bias choke, DC blocking capacitors and driver stage on a single design, while delivering 35 Watts with up to 44 percent power added efficiency (PAE) across an instantaneous bandwidth. The HMC8205 also operates both pulse and continuous wave, unlike comparative designs.


    Pricing and Availability
    Product Frequency Range Sample Availability Full Production Price Each Per 1,000 Packaging Complementary Parts
    HMC8205 0.3 to 6 GHz Now Now $469.00 Lead Flange Mount HMC637ALP5E
    HMC8410LP2FE
    HMC788ALP2E
  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • EngineerZone is a registered trademark of Analog Devices, Inc.

    Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue
  • Editor's Contact Information
Stay Informed