Press Release

Contact Linda Kincaid

Analog Devices’ Next Generation Digital Signal Processors Provide Greater Internal Program and Data Memory for Automotive Audio Applications

May 23 2017 - Norwood, MA
  • ADAU1462-ADAU1463-ADAU1466-ADAU1467-RGB-300x300-Title-WebAnalog Devices, Inc. today announced four fixed point digital signal processors (DSPs) qualified for automotive applications. Designed to fit the emerging demands of new and improved audio algorithms, the ADAU1466 and ADAU1467 SigmaDSP® processors offer market-leading performance in fixed point DSP processors with three times the internal program memory and two times the internal data memory of the previous generation. The ADAU1463 and ADAU1467 utilize an 88-pin LFCSP package and feature eight pins that can be configured as serial data inputs or outputs. These additional pins provide greater flexibility in amplifier or head unit designs to support applications such as hands free, active noise cancellation, and acoustic noise reduction among others. Like all SigmaDSP processors, the ADAU1463 and ADAU1467 feature a unique hardware architecture optimized for efficient audio processing. Their quad Multiply-Accumulate (MAC) architecture includes audio specific hardware accelerators that optimize MIPS performance for latency sensitive applications. The ADAU146x series uses ADI's award-winning SigmaStudio graphical programming tool that allows signal flows and applications to be developed and tuned quickly and with a minimum learning curve.



    When compared to alternative DSP devices, the ADAU146x series provides unmatched parallel processing performance, flexibility and system scalability. The availability of both a cost effective 150 MHz and a 300 MHz DSP core gives alternatives to system designers for traditional and more demanding applications. The 300 MHz DSP core provides up to 1.2 GMACs, executing 6,144 instructions while running at 48 KHz audio sample. The built-in stereo asynchronous sample rate converters (ASRCs), audio signal router matrix and an on-chip RAM that is two times larger than previous generation DSPs allow for the versatile and simplified execution of very demanding algorithms. The integrated PLL and flexible clock generator hardware can generate up to 15 audio sample rates simultaneously.


    The power efficient ADAU146x series core will execute full signal flows consuming only a few hundred milliwatts (mW) and less than one watt running at maximum program load (25 deg.C). The ADAU146x DSPs are ideal replacements for larger, higher cost, general-purpose DSPs that consume more power while executing similar processing. Highly configurable serial ports, S/PDIF interfaces, multipurpose input/output pins and 10-bit auxiliary ADCs enable the ADAU146x DSPs to interface with a wide range of audio devices such as ADCs, DACs, digital audio devices, amplifiers and other control circuitry, while greatly simplifying system complexity.


    Pricing and Availability
    Product DSP Core Data/Program Memory (kWords) Full Production 1K Price Package
    ADAU1462-x 150 MHz 48/16 July 2017 $5.65 72-lead, 10 mm × 10 mm LFCSP package
    ADAU1462-x 300 MHz 48/16 July 2017 $6.66 72-lead, 10 mm × 10 mm LFCSP package
    ADAU1463-x 150 MHz 48/16 Aug. 2017 $6.22 88-lead, 12 mm × 12 mm LFCSP package
    ADAU1463-x 300 MHz 48/16 Aug. 2017 $7.32 88-lead, 12 mm × 12 mm LFCSP package
    ADAU1466-x 300 MHz 80/24 July 2017 $7.99 72-lead, 10 mm × 10 mm LFCSP package
    ADAU1467-x 300 MHz 80/24 Aug. 2017 $8.78 88-lead, 12 mm × 12 mm LFCSP package
  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • SigmaDSP and EngineerZone are registered trademarks of Analog Devices, Inc.

    SigmaStudio is a trademark of Analog Devices, Inc.

    Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue
  • Editor's Contact Information
Stay Informed