Press Release

Contact Linda Kincaid

Next Generation Advanced Instrumentation and Defense Applications Enabled by Analog Devices’ High-Speed A/D Converter

Oct 12 2017 - Norwood, MA
  • AD9689-9695-9697-RGB-300x300-Title-Web
    Analog Devices, Inc. today announced a 14-bit, 2.6 GSPS dual A/D converter which enables IF/RF sampling with superior speed and linearity. The AD9689 A/D converter features power dissipation of 1.55 W per channel, half the dissipation of comparable solutions in the market, thus further increasing suitability for many of its targeted design situations.


    In addition to the high-performance AD9689, ADI introduced two related converters: the AD9695, a dual 14-bit 1300/625 MSPS device, and the AD9697, a single 14-bit, 1300-MSPS unit. Both are lower-power, pin-compatible upgrades for existing devices. All three A/D converters include JESD204B interfaces for efficient and highest-speed interconnection to FPGAs, and share the same register map, so they can be used across multiple platforms with minimal coding efforts. Since many system architectures require complementary signal-transmission channels, Analog Devices also offers the AD9172 and AD9162 D/A converters as counterparts to the AD9689 and AD9695.


    Full-speed spur free dynamic range (SFDR) of the AD9689 is an exceptional 64 dB full scale for a 3-GHz analog input. Other features of this converter include user-programmable FIR filters which allow users to perform quadratic error correction and equalization for optimized performance, and an analog input bandwidth of 9 GHz in the BGA-packaged version to allow for RF sampling up to and beyond the 4th Nyquist zone. The AD9689 A/D converter’s JESD204B interface supports 16 GBPS/lane performance, which exceeds the 12.5 GBPS/lane requirement of the standard. Thus, the system FPGA can use fewer lanes, while freeing resources for other functions.


    Product Full Production Price Each per 1,000 Packaging
    AD9689BBPZ-2600 Now $1108.34 196-Lead CSPBGA
    AD9689BBPZ-2000 October 31 $934.86 196-Lead CSPBGA
    AD9695BCPZ-1300 Now $831.30 64-Lead LFCSP
    AD9695BCPZ-625 Now $406.26 64-Lead LFCSP


  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • Visit ADI’s multimedia gallery to review more product images: http://www.analog.com/en/about-adi/news-room/multimedia-gallery.html


    EngineerZone is a registered trademark of Analog Devices, Inc.


    Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue

  • Editor's Contact Information
Stay Informed