Press Release

Contact Linda Kincaid

Analog Devices Makes MEMS Switch Technology a Commercial Reality

Nov 8 2016 - Norwood, MA
  • ADGM1304/ADGM1004Analog Devices, Inc. (ADI) today introduced a breakthrough in switch technology that provides a long-sought replacement for electromechanical relay designs first adopted by the electronics industry more than 100 years ago. ADI’s new RF-MEMS switch technology is enabling faster, smaller, lower power, more reliable instrumentation equipment by resolving multiple performance limitations commonly attributed to relays, whose origins date to the earliest days of the electric telegraph. With the commercial release of products enabled by this technology, original equipment manufacturers (OEMs) can significantly improve the accuracy and versatility of automatic test equipment (ATE) and other instrumentation tools to help their customers reduce testing costs, power and time to market. Future products within the MEMS switch series will replace relays in aerospace and defense, healthcare, and communications infrastructure equipment, allowing OEMs in those markets to pass similar size, power and cost savings along to their customers.


    The first in a new product series, ADI’s ADGM1304 and ADGM1004 RF MEMS switches are 95 percent smaller, 30 times faster, 10 times more reliable, and use 10 times less power than conventional electromechanical relays.



    MEMS Switch Technology Delivers 0-Hz (DC) to Wideband RF Performance
    Unlike other switch alternatives such as solid-state relays, the ADGM1304 and ADGM1004 MEMS switches have superior precision and RF performance from 0 Hz (DC) to 14 GHz. ADI’s MEMS switch solution contains two die to maximize operational performance – an electrostatically actuated switch in a hermetically sealed silicon cap, and a low-voltage, low-current driver IC. The switching element has a highly conditioned, extremely reliable metal-to-metal contact that is actuated via an electrostatic force generated by the companion driver IC. The resultant co-packaged solution ensures best-in-class DC precision and RF performance, and makes the switch extremely easy to use.


    Switch Breakthrough Extends ATE Equipment Lifetime and Channel Densities
    The highly reliable ADGM1304 and ADGM1004 increase cold-switching lifetime by a factor of 10 compared to electromechanical relays, extending ATE system operating life and reducing costly downtime caused by relay failures. Additionally, the extremely small height of the ADGM1304 and ADGM1004 MEMS switch packages allow designers to surface-mount the devices on both sides of their ATE test boards to boost channel densities at reduced cost and without expanding equipment footprint. An integrated charge pump removes the need for external drivers, further reducing ATE system size, while a multiplexer configuration simplifies the fan-out structure compared to DPDT relay designs.


    Pricing and Availability
    Part Number Sample Availability Production Availability Price Each in 1,000 Units Package
    ADGM1304 Now Now $36.58 24-lead 5mm × 4mm × 0.95mm LFCSP
    ADGM1004 Now February 2017 $39.34 24-lead 5mm x 4mm x 1.45mm LFCSP

  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) designs and manufactures semiconductor products and solutions. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure and connect. Visit http://www.analog.com
  • EngineerZone is a registered trademark of Analog Devices, Inc.


    Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/

  • Editor's Contact Information
Stay Informed