LTspice: Stepping Parameters

Sep 18 2017

This video provides an overview of how to use the .STEP command to perform repeated analysis of a circuit in LTspice.

In any LTspice simulation, varying a parameter in a device or model is just as important as plotting voltages or currents, as it allows you to compare performance and develop your circuit intuition.

There are two ways to examine a circuit by changing the value of a parameter: You can either manually enter each value then re-simulate the circuit, or you can use the .STEP command to sweep across a range of values in a single simulation run and produce a side-by-side comparison.

LTspice: Stepping Parameters

Sep 18 2017

This video provides an overview of how to use the .STEP command to perform repeated analysis of a circuit in LTspice.

In any LTspice simulation, varying a parameter in a device or model is just as important as plotting voltages or currents, as it allows you to compare performance and develop your circuit intuition.

There are two ways to examine a circuit by changing the value of a parameter: You can either manually enter each value then re-simulate the circuit, or you can use the .STEP command to sweep across a range of values in a single simulation run and produce a side-by-side comparison.

Latest Media 12
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project