Designed, Built, Tested
Board pictured here has been fully assembled and tested.

製品概要

設計リソース

設計/統合ファイル

  • Schematic
  • PCB Layout
  • BOM
  • Test Results
  • Tools & Models
設計ファイルのダウンロード 3.65 M

説明

The MAXREFDES1180 is centered around the MAX17501 ultra small, high-efficiency, high-voltage, synchronous stepdown DC-DC converter with integrated MOSFETs. This design provides a -12V output and up to 150mA of load current with an input voltage range of 4.5V to 5.5V. Unlike a traditional design, this reference design is configured to work in an inverting buck-boost topology to produce negative output voltage from positive input voltage.

Industrial control equipment such as programmable logic controllers, I/O modules, mass flow controllers, and various other sensors and supporting systems use analog components like amplifiers and multiplexers that operate on negative supply voltage. The MAXREFDES1180 is designed to demonstrate the operation and principles on how to use the MAX17501 to provide a negative supply voltage.

機能と利点

  • No Schottky-synchronous operation for high efficiency and reduced cost
  • Ultra-compact layout
  • All-ceramic capacitors
  • Reduces power dissipation

使用されている製品

詳細

The MAXREFDES1180 is centered around the MAX17501 ultra small, high-efficiency, high-voltage, synchronous stepdown DC-DC converter with integrated MOSFETs. This design provides a -12V output and up to 150mA of load current with an input voltage range of 4.5V to 5.5V. Unlike a traditional design, this reference design is configured to work in an inverting buck-boost topology to produce negative output voltage from positive input voltage.

Industrial control equipment such as programmable logic controllers, I/O modules, mass flow controllers, and various other sensors and supporting systems use analog components like amplifiers and multiplexers that operate on negative supply voltage. The MAXREFDES1180 is designed to demonstrate the operation and principles on how to use the MAX17501 to provide a negative supply voltage.

Other features include the following:

  • No Schottky-Synchronous Operation for High Efficiency and Reduced Cost
  • Ultra-Compact Layout
  • All-Ceramic Capacitors
  • Reduces Power Dissipation

This reference design is a single negative output power supply using the MAX17501, which is a synchronous stepdown DC-DC converter. The power supply is designed for applications that require operation at negative supply voltage. This design can deliver up to 100mA at -12V. Table 1 shows an overview of the design specification.

Table 1. Design Specification
PARAMETER SYMBOL MIN MAX
Input Voltage VIN 4.5V 5.5V
Output Voltage VOUT -12V
Output Current IOUT 0mA 100mA
Efficiency η 87%
Switching Frequency fSW 600kHz

This document describes the hardware shown in Figure 1. It provides a detailed systematic technical guide for the design of the MAXREFDES1180 using the MAX17501 synchronous step-down DC-DC converter for applications that require negative supply voltage. See the MAX17501 data sheet for device operation details. This power supply has been built and tested, details of which follow later in this document.

Figure 1. The MAXREFDES1180 variant uses the same layout as designed in the MAXREFDES1174, but with updated components to fulfill different design requirements.
Figure 1. The MAXREFDES1180 variant uses the same layout as designed in the MAXREFDES1174, but with updated components to fulfill different design requirements.

Because the MAX17501 is used in a buck-boost configuration for this design, the formula used is for a buck-boost converter instead of the traditional buck converter formula provided in the MAX17501 data sheet. Before starting the design process, we need to determine the appropriate version for the MAX17501, the operating input voltage range, the duty ratio, and the load current capability of our design.

Part Number Selection

The MAX17501 is available in six different versions. The MAX17501A/MAX17501E and MAX17501B/MAX17501F have preset output voltages of 3.3V and 5.0V, respectively. An internal compensation network is used to produce the preset output. Because of the internal compensation, these versions cannot be used to produce the negative output voltage.

The MAX17501G/MAX17501H offer an adjustable output voltage from 0.9V to 92% VIN that can be set with a resistive voltage-divider connected from the positive terminal of the output capacitor (VOUT) to GND. Because this design is used in a negative output configuration, ensure that only version G and version H are used in the design. The switching frequency is at 600kHz for the G version and 300kHz for the H version. The MAX17501GATB+ is used in this reference design.

Operating Input Voltage Range

The MAX17501 is rated for a 4.5V to 60V input voltage range. In a negative output configuration, the input voltage seen by the part is the difference between input voltage and output voltage. Therefore, for negative output voltage, the maximum voltage input and the absolute value of the output voltage must not exceed 60V, as shown in the following equation:

V IN ( MAX ) + | V OUT | ≤ 60 V

V IN ( MAX ) ≤ 60 V − | V OUT | = 60 V − 12 V = 48 V

At -12V output, the input voltage range is from 4.5V to 55V. The 4.5V to 5.5V input voltage range used in this design is within the specifications.

Duty Ratio

Assuming the ideal situation where the power losses associated with the MOSFETs and the inductor DC resistance can be ignored, the duty ratio is expressed as follows:

| V OUT | = ( D 1 − D ) × V IN

| V OUT | = D × ( V IN + | V OUT | )

D = | V OUT | V IN + | V OUT |

At 4.5V, 5V, and 5.5V voltage input, the duty ratio is at 0.73, 0.71, and 0.69 respectively. The maximum duty ratio is at the minimum input voltage. Therefore, DMAX is at 0.73. Note that the formula used is for a buck-boost converter.

Load Current Capability

In inverting applications, the switch current is expected to be higher. Although this part is rated for 500mA output current, the maximum output current for this design will be less. With a maximum duty cycle of 52%, the maximum output current is given by the following expression:

I OUT ( MAX ) = I OUT(BUCK) × ( 1 − D MAX )

= 500 mA × ( 1 − 0.73 ) = 135 mA

The maximum output load is at 135mA, which is sufficient for the 100mA output load used in this design.

Step 1: Inductor Selection

The MAXREFDES1180 utilizes continuous current mode, where the current through the inductor never drops to 0A. The inductor is exposed to current throughout the entire switching period. The rules of thumb for inductor selection are as follows:

  1. Inductance value (L): The value must be within the value range where it is high enough to prevent excessive current, but low enough so that sufficient energy can be stored in the inductor core for current conduction.
  2. Inductor saturation current (ISAT): The saturation current rating must be above the peak current limit value (0.76A is typical for the MAX17501) to ensure that the inductor can store the required energy without saturating.
  3. DC resistance (RDCR): The DC resistance value must be as low as possible to minimize the self-heating effect and to reduce losses.

The minimum value for the inductor is calculated using the following equation:

L MIN = V IN(MIN) × D MAX f SW × Δ I L = 4.5 V × 0.73 600 kHz × 250 mA = 21.9 μH

where ∆IL can be expressed in terms of the inductor current ripple ratio (LIR):

Δ I L = LIR × I OUT(MAX) = 0.5 × 500 mA = 250 mA

where LIR is assumed to be 0.5.

The maximum value for the inductor is given by the following equation:

L MAX = ( V IN(MAX) − V OUT ) × D MIN f SW × Δ I L

= [ 5.5 − ( − 12 ) ] V × 0.69 600 kHz × 250 mA = 80.5 μH

Taking into consideration ISAT and RDCR, the inductor chosen was the SRN8040-101M rated at 100μH. Because the inductor was chosen, the ∆IL value was calculated based on the actual value chosen for the application. This ∆IL should be used in the next design requirement and is given by the following equation:

Δ I L = V IN(MIN) × D MAX f SW × L SEL = 4.5 V × 0.73 600 kHz × 100 μH = 54.8 mA

Step 2: Input Capacitor Selection

The input capacitor is important to reduce the current peaks drawn from the input supply, increase efficiency, and reduce noise injection. The value of CIN largely depends on the source impedance of the input supply. The higher the source impedance is, the higher the input capacitance required. To reduce the voltage ripple at the input, a ceramic capacitor is placed right at the input of the MAX17501. For industrial standards, an X7R ceramic capacitor is recommended. The minimum value needed for this design is given by the following equation:

C IN(MIN) = Δ I L 8 × f SW × V IN(RIPPLE)

= 54.8 mA 8 × 600 kHz × ( 1 % × 5 V ) = 0.23 μF

Considering the derating value of the capacitor, the GRM31MR71H474KA01 rated at 0.47μF/50V, 10%, X7R was chosen.

Step 3: Output Capacitor Selection

The output capacitance is important to ensure the stability of the system and is usually sized to support a step load of 50% of the maximum output current in the application, so the output-voltage deviation is contained to ±3% of the output-voltage change. A ceramic capacitor with very low ESR should be used. The minimum value required is calculated by the following equation:

C OUT(MIN) = I OUT × D MAX f SW × | V OUT(RIPPLE) |

= 100 mA × 0.73 600 kHz × ( 1 % × 12 V ) = 1.01 μF

Considering the derating value of the capacitor, GRM31CR71H225KA88 rated at 2.2μF, 50V, 10%, X7R was chosen.

Step 4: Output Voltage Settings

The output voltage can be set using the voltage-divider connected at the FB node. R4 is connected from VOUT to the FB node, while R5 is connected from FB to GND. For the MAX17501G, the parallel combination of R4 and R5 (RP) must be less than 15kΩ. To optimize efficiency and output accuracy, use the following equations to choose the values of R4 and R5:

R4 = 16.7 × | V OUT | = 16.7 × 12 V = 200.4 kΩ

R5 = R4 × 0.9 | V OUT | − 0.9 = 200.4 kΩ × 0.9 12 V − 0.9 = 16.25 kΩ

The standard resistor values chosen are 200kΩ and 16.2kΩ, respectively. The parallel combination for R4 and R5 is calculated as follows:

R P = 200 kΩ × 16.2 kΩ 200 kΩ + 16.2 kΩ = 14.9 kΩ

The RP value is less than 15kΩ, which is within the specification.

Step 5: Turn-On Voltage Input Selection

The EN/UVLO is driven high to enable the output voltage. The input voltage (undervoltage threshold) at which the device turns on can be set with a resistive voltage-divider connected from VIN to GND. R1 is connected from VIN to the EN/UVLO node, and R2 is connected from the EN/UVLO node to GND. A 3.3MΩ value was chosen for R1. The R2 value is then given by the following equation:

R2 = R1 × 1.218 V INU − 1.218 = 3.3 MΩ × 1.218 4.5 V − 1.218 = 1.22 MΩ

where VINU is 4.5V. A standard resistor value of 1.5MΩ was used in this design.

Step 6: External Loop Compensation

The switching mode power supply (SMPS) requires a feedback control to regulate the output requirements when the input of the system changes. The loop compensation is required to ensure the stability of the overall loop response and to ensure that the output voltage is kept constant, regardless of the changes in input voltage or load current. A gain margin greater than 6dB and a 45-degree phase margin typically provide stability to the system. The compensation component values, R3 and C5, are calculated by the following equations:

R3 = k × 188 × V OUT 2 × C OUT × ( 1 − D MAX ) L × I OUT × D MAX

= 2 × 188 × ( 12 ) 2 × 1.6 μF × ( 1 − 0.73 ) 100 μH × 100 mA × 0.73 = 3.2 kΩ

where k = 2 for the MAX17501 and COUT accounts for the DC voltage derated value. The DC voltage derating curves are available from all major capacitor vendors.

C5 = V OUT × C OUT R3 × I OUT × ( 1 + D MAX )

= 5 × 1.6 μF 3.2 kΩ × 100 mA × ( 1 + 0.73 ) = 33.5 nF

Using the derated value of 1.6μF for COUT, the standard values for R3 and C5 are 3.24kΩ and 33nF, respectively.

Step 7: Soft-Start Capacitor Selection

To reduce inrush current, the MAX17501 implements an adjustable soft-start operation. A capacitor connected from the SS pin to GND programs the soft-start period. For this design, the soft-start period is set at 1.2ms. The soft-start capacitor value is given by the following equation:

C SS = 5.55 nF × t SS = 5.55 nF × 1.2 ms = 6.66 nF

A standard capacitor value of 6.8nF was used in this design.

サポートおよびトレーニング

技術的なご質問についての回答は、ナレッジベースを検索してください。また、アナログ・デバイセズのアプリケーション・エンジニアの専任チームが、技術的なご質問にお答えいたします。