LTC3337:バッテリの健全性を監視するナノパワーのSOHデバイス、高精度のクーロン・カウンタを搭載
2022年01月25日
「LTC3337」は、バッテリの健全性(SOH:State of Health)の監視を可能にするICです。無限大のレベルのダイナミック・レンジを実現する高精度のクーロン・カウンタを搭載しています。また、自己消費電流が最小限に抑えられている点も特徴の1つです。あらゆる負荷条件の下で、放電量、電圧、インピーダンス、温度という重要なパラメータの値を正確に測定できます。更に、実際の負荷に依らずバッテリが最大の容量を提供できるように負荷の条件を提示することが可能です。
LTC3337:バッテリの健全性を監視するナノパワーのSOHデバイス、高精度のクーロン・カウンタを搭載
2022年01月25日
「LTC3337」は、バッテリの健全性(SOH:State of Health)の監視を可能にするICです。無限大のレベルのダイナミック・レンジを実現する高精度のクーロン・カウンタを搭載しています。また、自己消費電流が最小限に抑えられている点も特徴の1つです。あらゆる負荷条件の下で、放電量、電圧、インピーダンス、温度という重要なパラメータの値を正確に測定できます。更に、実際の負荷に依らずバッテリが最大の容量を提供できるように負荷の条件を提示することが可能です。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}