With the AD2070 and AD2071 high-performance 4½-digit microprocessor-based autoranging single-channel thermocouple meters, temperatures from −328°F to +4,200°F (−200°C to +2,315°C) can be measured accurately with a wide variety of thermocouples: J, K, T, E, R, S, C, B, J DIN, or T DIN. The AD2070 is programmed at the factory to work optimally with one of these thermocouple types, as specified by the user; the AD2071 is a universal meter that the user can switch-program to work with any of these thermocouples. Read full article