Voltage Standing Wave Ratio Definition and Formula

Nov 15 2012

Figure 1

   

Abstract

Impedance mismatches in a radio-frequency (RF) electrical transmission line cause power loss and reflected energy. Voltage standing wave ratio (VSWR) is a way to measure transmission line imperfections. This tutorial defines VSWR and explains how it is calculated. Finally, an antenna VSWR monitoring system is shown.

A similar version of this article appeared in the October 2012 issue of Power Systems Design magazine.

VSWR Definition

Voltage standing wave ratio (VSWR) is defined as the ratio between transmitted and reflected voltage standing waves in a radio frequency (RF) electrical transmission system. It is a measure of how efficiently RF power is transmitted from the power source, through a transmission line, and into the load. A common example is a power amplifier connected to an antenna through a transmission line.

SWR is, thus, the ratio between transmitted and reflected waves. A high SWR indicates poor transmission-line efficiency and reflected energy, which can damage the transmitter and decrease transmitter efficiency. Since SWR commonly refers to the voltage ratio, it is usually known as voltage standing wave ratio (VSWR).

VSWR and System Efficiency

In an ideal system, 100% of energy is transmitted from the power stages to the load. This requires an exact match between the source impedance (the characteristic impedance of the transmission line and all its connectors), and the load impedance. The signal's AC voltage will be the same from end to end since it passes through without interference.

In a real system, mismatched impedances cause some of the power to be reflected back toward the source (like an echo). These reflections cause constructive and destructive interference, leading to peaks and valleys in the voltage, varying with time and distance along the transmission line. VSWR quantifies these voltage variances, hence another commonly used definition for Voltage Standing Wave Ratio is that it is the ratio of the highest voltage to the lowest voltage, at any point on the transmission line.

For an ideal system, voltage does not vary. Therefore, its VSWR is 1.0 (or more usually expressed as a ratio of 1:1). When reflections occur, voltages vary and VSWR is higher, for example 1.2 (or 1.2: 1). Increased VSWR correlates with reduced transmission line (and therefore overall transmitter) efficiency.

Reflected Energy

When a transmitted wave hits a boundary such as the one between the lossless transmission line and load (Figure 1), some energy will be transmitted to the load and some will be reflected. The reflection coefficient relates the incoming and reflected waves as:

Γ = V-/V+

Where V- is the reflected wave and V+ is the incoming wave. VSWR is related to the magnitude of the voltage reflection coefficient (Γ) by:

VSWR = (1 + |Γ|)/(1 – |Γ|)

Figure 1. Transmission line circuit illustrating the impedance mismatch boundary between the transmission line and the load. Reflections occur at the boundary designated by Γ. The incident wave is V+ and the reflective wave is V-.

Figure 1. Transmission line circuit illustrating the impedance mismatch boundary between the transmission line and the load. Reflections occur at the boundary designated by Γ. The incident wave is V+ and the reflective wave is V-." class="img-responsive.

VSWR can be measured directly with an SWR meter. An RF test instrument such as a vector network analyzer (VNA) can be used to measure the reflection coefficients of the input port (S11) and the output port (S22). S11 and S22 are equivalent to Γ at the input and output port, respectively. The VNAs with math modes can also directly calculate and display the resulting VSWR value.

The return loss at the input and output ports can be calculated from the reflection coefficient, S11 or S22, as follows:

RLIN = 20log10|S11| dB

RLOUT = 20log10|S22| dB

The reflection coefficient is calculated from the characteristic impedance of the transmission line and the load impedance as follows:

Γ = (ZL - ZO)/(ZL + ZO)

Where ZL is the load impedance and ZO is the characteristic impedance of the transmission line (Figure 1).

VSWR can also be expressed in terms of ZL and ZO. Substituting Equation 5 into Equation 2, we obtain:

VSWR = [1 + |(ZL - ZO)/(ZL + ZO)|]/[1 - |(ZL - ZO)/(ZL + ZO)|] = (ZL + ZO + |ZL - ZO|)/(ZL + ZO - |ZL - ZO|)

For ZL > ZO, |ZL - ZO| = ZL - ZO

Therefore:

VSWR = (ZL + ZO + ZL - ZO)/(ZL + ZO - ZL + ZO) = ZL/ZO.

For ZL < ZO, |ZL - ZO| = ZO - ZL

Therefore:

VSWR = (ZL + ZO + ZO - ZL)/(ZL + ZO - ZO + ZL) = ZO/ZL.

We noted above that VSWR is a specification given in ratio form relative to 1, as an example 1.5:1. There are two special cases of VSWR, ∞:1 and 1:1. A ratio of infinity to one occurs when the load is an open circuit. A ratio of 1:1 occurs when the load is perfectly matched to the transmission-line characteristic impedance.

VSWR is defined from the standing wave that arises on the transmission line itself by:

VSWR = |VMAX|/|VMIN|

Where VMAX is the maximum amplitude and VMIN is the minimum amplitude of the standing wave. With two super-imposed waves, the maximum occurs with constructive interference between the incoming and reflected waves. Thus:

VMAX = V+ + V-

for maximum constructive interference. The minimum amplitude occurs with deconstructive interference, or:

VMIN = V+ - V-

Substituting Equations 9 and 10 into Equation 8 yields

VSWR = |VMAX|/|VMIN| = (V+ + V-)/(V+ - V-)

Substitute Equation 1 into Equation 11, we obtain:

VSWR = V+(1 + |Γ|)/(V+(1 - |Γ|) = (1 + |Γ|)/(1 – |Γ|)

Equation 12 is Equation 2 stated at the beginning of this article.

VSWR Monitoring System

The MAX2016 is a dual logarithmic detector/controller used to monitor the VSWR/return loss of an antenna, when it is paired with a circulator and attenuator. The MAX2016 outputs the difference between the two power detectors.

The MAX2016 combined with the MAX5402digital potentiometer and MAX1116/MAX1117 ADC forms a complete VSWR monitoring system (Figure 2). The digital potentiometer acts as a voltage-divider by using the MAX2016's reference voltage output. The internal reference voltage can typically source 2mA of current. This voltage sets the threshold voltage for the internal comparator (pin CSETL). An alarm can be generated when the output voltage crosses the threshold (pin COUTL). The MAX1116 ADC requires a 2.7V to 3.6V supply, while the MAX1117 ADC requires 4.5V to 5.5V. The ADC can also use an external reference voltage, provided by the MAX2016. The ADC paired with the microcontroller allows for constant monitoring of the antenna's VSWR.

Figure 2. The VSWR monitoring system consists of an ADC for real-time measurements. The external digital potentiometer enables a configurable alarm signal at the comparator's output (COUTL).

Figure 2. The VSWR monitoring system consists of an ADC for real-time measurements. The external digital potentiometer enables a configurable alarm signal at the comparator's output (COUTL).

Summary

In review, this tutorial describes SWR or VSWR as a way to measure transmission line imperfections and efficiency. VSWR is related to the reflection coefficient. A higher ratio depicts a larger mismatch, while 1:1 ratio is perfectly matched. This match or mismatch arises from the standing wave's maximum and minimum amplitude. SWR is related to the ratio between transmitted and reflected energy. The MAX2016 is shown as an example of how to create a system to monitor antenna VSWR.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Product Categories
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project