Replace Two ICs with a Combination High Efficiency Buck Controller Plus Low Noise LDO

Dec 1 2002

Need a second low-noise voltage output alongside your DC/DC converter, but don’t have the room for another IC? The LTC3700 offers a simple solution by combining a constant frequency current mode step-down DC/DC controller with a 150mA low dropout (LDO) regulator in a tiny 10-pin MSOP.

The buck controller section of the LTC3700 offers many of the features expected in a high-performance switcher: high efficiency (up to 94%), wide VIN range (2.65V to 9.8V), high constant frequency operation (550kHz), and current mode control for excellent AC and DC load and line regulation. The buck is configured for Burst Mode® operation, which reduces switching losses at light load, thereby enhancing efficiency. In dropout, the external P-channel MOSFET is turned on continuously (100% duty cycle), extending the usable voltage range of a battery source.

The LDO output is powered by an internal P-channel MOSFET pass device with an on resistance of approximately 1.5Ω (with VIN2 = 4.2V). The LDO has a separate input supply pin, which offers the versatility of powering the LDO from the buck regulator’s input supply, its own independent input supply or the buck controller’s output. The LDO is protected by both current limit and thermal shutdown circuits.

The LTC3700 provides ±2.5% output voltage accuracy for both the buck and LDO. The buck consumes only 210µA of quiescent current in normal operation with the LDO consuming an additional 50µA. In shutdown, a mere 10µA (combined) is consumed. A common “Power Good” output monitors both supplies.

5V Input Supply to 3.3V/500mA High Efficiency Output and 2.5V/150mA Low Noise Output

Figure 1 shows a dual regulated output voltage design running off of a single 5V input supply. The input to the LDO, VIN2, could connect directly to VIN, but better efficiency is obtained by running if off the 3.3V buck output.

Figure 1. 5V input to dual output: a 3.3V/500mA high efficiency output and a 2.5V/150mA low noise output.

Figure 2 shows the buck efficiency vs load current. Since the LDO’s input supply is connected to the buck output, input current to the LDO adds to the load current seen by the buck. With both outputs running at maximum current, 500mA (buck) and 150mA (LDO) for 650mA total, the measured buck efficiency was 91.4%.

Figure 2. Efficiency of the 3.3V output for the circuit in Figure 1.

About the Authors

Mark Vitunic
Mark Vitunic is a design manager in the power business unit of Analog Devices. He officially joined ADI in 2017 as part of the acquisition of Linear Technology, where he had worked for the previous 19 years. Mark manages n...

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More