HFAN-02.6.0: Reducing Noise and Wander in Low-Speed (<622Mbps) Optical Transmitters

Dec 13 2005

Figure 1

   

Abstract

This application note will discuss common causes of vertical eye closure in low speed (<622Mbps) optical transmitters. Design suggestion and tests will be provided to help diagnose the transmitter. Methods will also be provided to improve the performance. The application note will focus primarily on the MAX3735A and MAX3646 as these devices are commonly used in multi-rate (155Mbps to 2.7Gbps) and low data rate applications.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Latest Media 25
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project