Generating Greater System Efficiency for Single- to Multi-Cell Battery-Powered Designs
Generating Greater System Efficiency for Single- to Multi-Cell Battery-Powered Designs
Mar 22 2019
Abstract
Consumers want their electronics, including small, battery-powered devices, to operate for long periods between charges. The growing prevalence of devices powered by 1-, 2-, and 3-cell lithium-ion batteries has placed a spotlight on the importance of efficient power conversion in the power supplies for these applications’ hard-working processors. This white paper examines how dynamic power management capabilities in buck, or step-down, converters—key components of power supplies—can generate greater energy efficiency for the entire system. The paper also highlights how enhanced energy efficiency contributes to the extended battery runtime as well as battery life that consumers have come to expect from their electronic gadgets.
About the Authors
Related to this Article
Products
PRODUCTION
16A High-Performance Quad-Phase Buck Regulator for Multicore CPU and GPU Processors
LAST TIME BUY
9A, Three-Phase Step-Down Switching Regulator
RECOMMENDED FOR NEW DESIGNS
14V Input, 1.5A High-Efficiency Buck Converter with 9μA IQ
Product Categories
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}