SIGNALS+ NEWSLETTER SUBSCRIPTION
Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.
Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.
You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!
CloseHOW INDUSTRIAL ROBOTS ARE LEARNING TO BE DEXTEROUS MACHINES
KEY TAKEAWAYS
|
Industrial robots have long excelled at speed, strength, and repeatability, but they still struggle with dexterous manipulation tasks such as routing a cable through a tight conduit, seating a connector in a recessed socket, or threading a component into place. While these routine operations are common in data center maintenance, manufacturing, and automotive assembly, they require accurate perception, precise motion control, and real-time response to contact forces in constrained or partially occluded spaces. Together, these requirements make these tasks difficult to automate reliably with conventional systems, leaving many critical operations heavily dependent on labor performed by humans.
Industrial environments demand high reliability, which adds another layer of complexity. Data center cable manipulation, for example, involves densely packed connectors and strict uptime requirements, where even small disturbances can have cascading effects. Such data center network racks also differ widely, requiring robotic solutions that can overcome lighting and layout differences. Collectively, these constraints reveal a clear gap between the capabilities of conventional automation and the demands of modern industrial infrastructure.
Learning-based robotics is closing the gap. By moving beyond classical, rule-based systems to AI-based approaches, robots can better perceive, adapt, and manipulate objects in unconstrained environments. As the technology matures, it can improve efficiency, reduce repetitive manual work, and make increasingly complex industrial infrastructure easier and more cost-effective to automate.
WHERE AUTOMATION REACHES ITS LIMITS
The macro challenge is not that robotics has failed. It is that robotics has succeeded most visibly in structured environments, where the same motion can be repeated with minimal variation. But industrial dexterity is different. Flexible materials bend unpredictably. Connectors must be aligned precisely and snap into place. Cables can shift, twist, or disappear from view. And contact forces matter because too little pressure fails the task and too much can damage the part, the fixture, or the surrounding system.
For manufacturers, datacenter operators, and industrial equipment teams, this challenge is becoming urgent. Their systems are scaling up, growing denser, more connected, and more difficult to service, while expectations for uptime, throughput, quality, and scalability continue to rise.
That is why dexterity has become a critical frontier for industrial automation. Automating simple, repeatable tasks can improve efficiency, but automating contact-rich, precision work can unlock new operating models, from faster infrastructure maintenance to more flexible production lines.
FROM FRAGILE PRECISION TO RELIABLE PERFORMANCE
The traditional approach to robotic systems often depends on programming, relying on highly tuned pipelines that separate perception, planning, and control into sequential steps. These systems can perform well when the environment is known and tightly controlled, but they can become brittle when conditions change. A shift in lighting, a slight variation in part position, an occluded cable, or an unexpected contact force can degrade performance and even cause damage.
Brittleness limits adoption. While today’s robotic systems work well in high-volume, low-variety scenarios, they require pricey, time-consuming recalibration and programming. This limitation also prevented the adoption of robots by small and medium businesses, missing the opportunity to help them increase production. While AI offers a way to overcome such barriers, robots that accomplish some generalized tasks in lab conditions end up struggling in production. The same task must often work across different fixtures, operators, parts, geometries, and service scenarios. A system that requires extensive recalibration whenever the environment changes is difficult to scale, and a system that cannot recover from small variations is difficult to trust.
The goal, then, is not simply to make robots more accurate. It is to make them more adaptable, repeatable, and robust across diverse industrial scenarios. That requires stable, real-time control, high-quality training data, and reliable sensing. It also requires evaluation methods that can show whether a system is ready for deployment beyond a controlled demonstration.
BETTER WAYS TO SEE, FEEL, AND LEARN
Advances in robotics, sensing, and AI are giving industrial robots a richer understanding of physical tasks. A key enabler is sensor fusion, the coordinated use of multiple sensing modalities to help robots operate more effectively and robustly in real-world environments. Instead of relying on a camera and preprogrammed motion alone, dexterous systems can combine RGB images, 3D point clouds, robot joint states, tactile sensing, and force/torque feedback to see, feel, and continuously adjust as they interact with the physical world.
This multimodal approach is critical because dexterous work is rarely visual alone. A connector may appear aligned until it meets resistance. A cable may look correctly routed, while hidden slack creates tension elsewhere. A component may require a sequence of small, contact-driven adjustments to settle into place. By combining multiple forms of sensing, robots gain the real-time feedback needed to respond more effectively in complex industrial settings.
However, sensor fusion and the multimodal approach also introduce significant challenges. One of the most critical is ensuring that data from each sensor is precisely synchronized so the AI model receives an accurate, time-aligned representation of the robot and its environment. Even small timing differences between cameras, force sensors, tactile sensors, and robot joint data can reduce training quality and impair real-time decision-making.
To address this challenge, Analog Devices, Inc. (ADI) has developed a networking solution that provides precision time synchronization and deterministic data transport across distributed sensing systems. The ADIN3310 is an Ethernet time sensitive networking switch that enables distributed sensors to operate from a common time base, helping ensure that AI training and inference systems receive accurately synchronized multimodal inputs. It provides the temporal infrastructure required for reliable sensor fusion, necessary to power advanced dexterous manipulation.
Learning-based approaches add another layer of complexity. Instead of hand-coding every step of perception, planning, and control, newer systems can learn manipulation behaviors from teleoperation and even human demonstration data. End-to-end AI policies, including diffusion-based imitation learning models, can take sensory inputs and generate coordinated robot actions within a unified framework. In practical terms, this means robots can begin to learn patterns of successful manipulation rather than relying solely on rules written for one tightly defined environment.
Robotic dexterity depends not only on advanced models and hardware, but on the infrastructure needed to collect data, train systems, evaluate performance, and deploy them reliably. A common pipeline may involve high-frequency teleoperation, synchronized multisensor data capture, real-time control, GPU-based inference, and early benchmarking methods. These methods give teams a consistent way to test whether different sensing and learning approaches improve performance under comparable conditions and iteratively enhance robotic dexterity in real-world industrial environments. As these capabilities mature together, industrial robots move closer to reliable operation in tasks once considered too variable or delicate to automate.
WHY INDUSTRIAL DEXTERITY MATTERS
The business value of industrial dexterity comes from expanding the relevance of robotic solutions to new and broader application areas where manual work today is repetitive, risky, or expensive. In mission-critical settings such as data centers, even routine service tasks require careful handling in dense, high-precision spaces where small mistakes can affect availability. Automating tasks like network cable cleaning and re-wiring can offer faster maintenance, more consistent execution, and lower total cost of ownership.
It can also shift human effort away from repetitive, precision-intensive, and physically constrained tasks toward higher-value work such as supervision, optimization, maintenance planning, and exception handling. Over time, better benchmarking, more reliable maintenance, and more repeatable development methods can help infrastructure operate more efficiently and reduce trial-and-error in system design. As robotic systems become easier to evaluate and improve, innovation cycles can become more efficient across the broader ecosystem.
To help advance this effort, ADI is collaborating with industry partners and developing an industrial dexterity benchmarking framework designed to evaluate how sensing, AI, and real-time control perform together in realistic manipulation tasks.
A MORE MEASURABLE PATH FORWARD
As mentioned above, industrial dexterity is advancing from theory toward solving everyday industrial tasks. Learning-based robotics is being evaluated against real-world production problems that limit automation today. But how do you consistently compare solutions to such problems?
The next step requires making progress easier to measure and compare. Industrial dexterity needs standardized benchmarking frameworks that reflect real-world constraints, including tight tolerances, limited visibility, flexible materials, and contact-rich interaction. NIST-inspired assembly task boards and newer manipulation benchmarks point in this direction by creating reproducible ways to test skills such as insertion, routing, fastening, and handling deformable objects.
Benchmarks do more than rank performance. They help teams understand where a system is strong, where it fails, and help identify which sensing or learning approaches are most effective for specific tasks. They also give researchers, suppliers, and end-customers a shared language for measuring progress.
As this evaluation foundation improves, robots will be better able to learn from real task data, combine multiple sensing inputs, adapt to variation, and demonstrate readiness through consistent testing. The result is a shift from robots that simply repeat motions faster to systems that can play a more capable role in maintaining, building, and scaling the infrastructure modern industries depend on.