Electrochemical Impedance Spectroscopy (EIS): Deeper Battery Insight Enables Smarter Design
SIGNALS+ NEWSLETTER SUBSCRIPTION
Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.
Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.
You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!
CloseELECTROCHEMICAL IMPEDANCE SPECTROSCOPY (EIS): DEEPER BATTERY INSIGHT ENABLES SMARTER DESIGN
October 26, 2026
KEY TAKEAWAYS
|
Across electrified systems—from EVs and industrial robots to energy storage systems and medical devices—batteries must now deliver more energy, charge faster, and last longer, while meeting ever-higher expectations for safety, reliability, and value. Yet the signals traditionally used to manage these batteries have not evolved at the same pace.
In fact, an EV’s battery pack accounts for about 30% to 40% of total vehicle cost, meaning even modest overbuffering, conservative operating limits, or premature degradation can translate into billions of dollars in lost value across a fleet.1
As performance margins shrink, traditional time-domain vs. impedance frequency domain signals are no longer enough. Voltage, current, and temperature remain essential, but they often reveal the symptoms of internal change rather than the change itself. By the time these signals shift, the underlying electrochemical behavior may already be affecting safety, performance, or lifetime. This leaves engineers managing uncertainty when they need deeper visibility into the physical state of the battery.
Electrochemical impedance spectroscopy (EIS) helps close this observability gap by enabling direct insight into the physics inside the battery cell itself. By probing batteries across multiple frequencies, EIS provides a richer view of internal cell behavior, revealing real-time physical state and transforming battery management beyond reactive protection into predictive, adaptive system intelligence. EIS marks the shift from observing batteries to understanding them, enabling a new class of adaptive, software-defined energy systems.
WHAT IS EIS?
|
EIS is a safe, nondestructive technique that probes a battery across multiple frequencies to reveal internal degradation, thermal risk, and failure modes early. |
A small electrical stimulus is applied to the battery, and the resulting voltage and current response are measured. Repeating this process at different frequencies produces an impedance spectrum containing information linked to different physical and electrochemical processes within the cell.
The resulting information can help identify changes associated with factors such as:
- Temperature
- Aging and degradation
- Charge-transfer behavior
- Diffusion within the cell
- Changes in internal resistance
- Abnormal or developing operating conditions
EIS does not, by itself, diagnose a battery or control its operation. It provides a richer measurement of internal battery behavior. Signal-processing software, battery models, and application algorithms can then convert that measurement into usable information to drive improved diagnostics, performance, and safety.
“EIS is no longer just a measurement technique…it’s the foundation that allows AI to understand, predict, and ultimately optimize how batteries behave in the real world.”Chirag K. Patel
Managing Director & GM, Automotive Electrification | Analog Devices, Inc.
EIS vs. Traditional BMS Signals
| Aspect | Traditional BMS | EIS-Enabled Intelligence |
|---|---|---|
| Primary measurements | Voltage, current, and temperature | Frequency-dependent impedance |
| View of the battery | External operating behavior | Rich view of internal cell behavior |
| Fault detection | Often reactive | Predictive, early stage |
| Degradation insight | Indirect, trend based | Mechanism specific (aging, plating, thermal abuse) |
| Fast charging optimization | Conservative rule and margins | Adaptive, condition aware |
| Data richness | Low dimensional | Frequency resolved and feature rich |
| Path to AI | Constrained by available observability | Strong foundation for physics-informed models and AI-assisted insights |
Traditional BMS answers “Is the battery still operating within limits?”
EIS answers “What is happening inside the battery—and what will happen next?”
EIS Impact Across Industries
By bringing EIS onboard, embedded battery systems can access deeper cell-level insight throughout operation, unlocking new safety, performance, and lifecycle value across industries.
Automotive and Electrified Mobility
- See risks sooner: EIS reveals changes linked to degradation and developing faults that conventional signals alone may miss, supporting safer operation and longer battery life.
- Charge faster, with confidence: By revealing internal impedance changes in seconds rather than minutes or hours, EIS enables dynamic adjustment of charge profiles, reducing degradation while maximizing charge speed.
- Protect lifetime value: Impedance-based diagnostics improve understanding of battery health and remaining life, supporting better warranty, service, and second-life decisions.
Industrial Energy and Infrastructure
- Maximize asset performance: EIS enables operators to protect usable capacity, improve uptime and extend asset life through earlier visibility into aging, imbalance and abnormal battery behavior.
- Prevent unplanned downtime: In industrial power systems and data centers, impedance-based monitoring is used to move from periodic inspection to continuous condition monitoring, reducing unplanned downtime.
- Strengthen operational resilience: EIS is particularly valuable in industrial environments where physical access is limited, and failures are costly, such as offshore energy, rail, or backup power installations.
Healthcare and Medical Devices
- Safeguard critical operation: EIS has long been used in biomedical diagnostics and is increasingly relevant for battery health monitoring in critical medical devices, where early detection of degradation is essential for safety and regulatory compliance.
- Reduce unexpected failures: For devices reliant on rechargeable batteries (for example, infusion pumps and imaging carts), EIS-based diagnostics can improve reliability and reduce unexpected failures during clinical use.
FROM EIS DATA TO PHYSICAL INTELLIGENCE
Physical Intelligence brings AI and machine learning into the physical world, enabling systems to perceive, interpret, and act on real-world conditions. In a battery system, this begins with accurately understanding the battery’s internal physical state.
EIS strengthens that perception by revealing internal cell behavior that voltage, current, and temperature alone may not expose. This information can directly support diagnostics, state estimation, charging strategies, and safety functions. It also provides AI and machine-learning models with a richer, physics-grounded view of the battery.
AI and machine learning can extract meaningful features from frequency-dependent impedance signatures and combine them with temperature, operating conditions, and usage history to support:
- Health and life prediction: Improve estimates of degradation, battery health, and remaining useful life.
- Anomaly detection: Identify patterns associated with abnormal or developing battery behavior.
- Adaptive operation: Support condition-aware charging, power limits, and safety strategies.
- Continuous improvement: Use field and fleet data to evaluate and refine battery models over time.
The effectiveness of battery AI depends on the quality of the physical information upon which it is built. More data or computing power cannot fully compensate for limited battery observability. By giving AI and machine learning richer, physics-grounded information, EIS helps battery systems move beyond fixed rules and reactive protection towards more predictive, adaptive, and intelligent operation.
TURNING BATTERY PHYSICS INTO ENGINEERING ADVANTAGE
As batteries become the backbone of modern mobility and infrastructure, engineers need deeper visibility—not wider safety margins. EIS provides that visibility by revealing internal cell behavior that conventional signals alone may not expose.
This richer physical understanding creates value immediately through better diagnostics, state estimation, and control. It also provides AI and machine-learning models with the physics-grounded information needed to predict change, adapt operation, and improve battery performance over time.
That is Physical Intelligence in action.
The future of battery management will not be defined only by keeping batteries within fixed operating limits. It will be defined by how effectively systems understand and adapt to the battery’s internal physical state.
1 The Future of Affordable EVs: Breakthroughs in Battery Pack Costs.” McKinsey & Co., 2026.