signals header
Autonomous warehouse robots transporting packages with digital navigation overlays in smart logistics system
Autonomous warehouse robots transporting packages with digital navigation overlays in smart logistics system

SIGNALS+ NEWSLETTER SUBSCRIPTION

Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.

By clicking “Subscribe”, you consent to receive marketing communications from Analog Devices, Inc. and its subsidiaries and agree to our Privacy Policy. Unsubscribe any time in your Privacy Settings.

Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.

You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!

Close

CONNECT TECH: DRIVING INDUSTRIAL AUTONOMY THROUGH ADVANCED GMSL CONNECTIVITY

July 29, 2025

With an estimated 40% of warehouses understaffed1, rising energy efficiency regulations, and automation-driven safety concerns, manufacturers are under unprecedented pressure. To address these challenges, many turn to an ever-growing mix of robots, cobots, and autonomous mobile robots (AMRs) to enhance flexibility, cut costs, and help maintain safe, efficient operations.

These intelligent machines have their own challenges: operating reliably in extreme temperatures, dust, shock/vibration, all while processing precise, real-time vision data. Additionally, growing demands for high resolution, multicamera, vision technology for navigation, and limited data transmission can cause performance bottlenecks.

The variety of applications and types of robots these vision systems must enable makes it challenging to create modular and scalable platforms that can be customized to application needs.

Such was the case with Connect Tech, a leader in embedded-edge AI hardware for industrial applications. Fortunately, their longtime, trusted partner, Analog Devices (ADI), had a next-generation connectivity solution, Gigabit Multimedia Serial Link (GMSL™).

Picture of Rob Callaghan, Chief Product Officer Connect Tech
“Our partnership with ADI strengthens Connect Tech’s ability to deliver high-performance GMSL connectivity for advanced autonomous systems. This collaboration enables our customers to reach new levels of autonomy with reliable, scalable solutions.”

Rob Callaghan

Chief Product Officer | Connect Tech

AT A GLANCE

COMPANY

Connect Tech is a leading manufacturer of rugged, embedded-edge AI hardware for industrial applications. Specializing in compact, durable solutions, Connect Tech’s agile engineering team delivers custom designs when off-the-shelf won’t suffice. Committed to innovation and customer success, Connect Tech strives to exceed expectations and push the boundaries of excellence.

GOAL

Develop camera vision subsystems and platforms to process camera vision technology and data from multiple, high resolution cameras. This enables digitalization, autonomy, and seamless, machine-to-machine interoperability in sensor-rich applications like smart factories, agriculture, and mining.

CHALLENGE

Connect Tech needed a deterministic, high speed, low latency video link that supports multiple high resolution cameras placed remotely from the processor. This requires a high bandwidth video link to transmit data to the processor, ideally using standard interconnects for scalability. These applications are often space-constrained, such as in robotic arms, so minimizing bulkiness from wiring is crucial.

SOLUTION

GMSL is a cost-efficient, simple, and scalable serializer and deserializer (SERDES) technology designed to achieve a new level of performance for high speed video links. It provides reliable transport of high resolution digital video for camera and display-based applications. It supports power over coax (PoC), making it suitable for applications with space, weight, and size constraints.

2.1 Million

EST. SHORTAGE IN SKILLED MANUFACTURING WORKERS BY 20302

Mobile and fixed robots fill labor gaps, reduce costs, and help improve efficiency, but manufacturers must carefully select motor drives, vision technology, connectivity, and power sources while planning their placement in the factory.

A LONG-LASTING RELATIONSHIP WITH LASTING IMPLICATIONS

Since 2016, ADI has been a trusted partner of Connect Tech, providing high performance, reliable, DC-to-DC power supply and video link (GMSL) solutions to enable Connect Tech’s camera vision solutions.

With GMSL, Connect Tech experiences two distinct advantages over competitor solutions: higher speed (12 Gbps with GMSL3 vs. roughly 7 Gbps on forward channel from competitor serial links); and adaptive equalization to maintain signal integrity for robust operation across long distances, harsh environments, and cable aging/bending. In addition, GMSL provides a budget-conscious solution, as video, audio, control, data, and power can all be transported on a single channel.

Beyond this, because ADI controls the GMSL roadmap, Connect Tech can co-develop features that support innovations or streamline designs to cut costs and accelerate time to market. This allows Connect Tech to rapidly expand and tailor its portfolio to meet evolving market demands.

ACCELERATING AUTONOMY ON THE CONNECTIVITY HIGHWAY

Now in its 3rd generation, ADI’s GMSL3 technology enables high speed data transfer over long distances, making it an ideal solution for Connect Tech’s high performance, rugged, industrial, and autonomous applications.

Connect Tech’s GMSL3 camera platform is an expansion board that allows up to 8 cameras to be connected to the Jetson AGX Orin system-on-module (SOM). Since many different types of GMSL cameras are available, the platform has user selectable options to interface with GMSL3 protocols at different operating frequencies.

Paired with Connect Tech’s Anvil-RX Rugged System, the combined solution delivers reliable, high bandwidth, vision processing capable of handling mission-critical deployments in extreme environments. It supports multiple GMSL3 camera inputs and is ideal for AMRs, agricultural, mining, and industrial automation.

Rugged industrial computer with multiple I/O ports for edge AI and real-time data processing
The Connect Tech Anvil-RX Rugged System Powered Solution paired with GMSL.
Picture of Preyksha Rajan Senior Engineer, Field Applications Analog Devices
“Connect Tech is integrating cameras, GMSL, and NVIDIA SoMs (system on modules) into a robust vision system. GMSL acts as a ‘connectivity highway.’ Combined in a system that can process all the data GMSL transfers, is what makes it desirable and a powerful physical layer and useful for such vision-based autonomous systems (like AMRs).”

Preyksha Rajan

Senior Engineer, Field Applications - Analog Devices

CONNECT TECH’S AUTONOMOUS APPLICATIONS USING GMSL

APPLICATION DESCRIPTION CONNECT TECH/ADI GMSL SOLUTION
Mining Autonomous mining vehicles operate in remote, rugged environments with high levels of dust, vibration, and temperature extremes.
  • Provides high bandwidth, long-distance data transfer for multiple high resolution cameras.
  • Lower latency communication to enable real-time obstacle detection and navigation.
  • Rugged hardware and mechanical design to withstand harsh environments while maintaining reliable performance.
Agriculture Autonomous agricultural equipment (drones, ground vehicles) requires high resolution, real-time imaging to monitor crop health, detect pests, and optimize resource usage across large farmlands.
  • Early detection of issues through real-time image analysis leads to more efficient and targeted interventions.
  • Precise application of water, fertilizers, and pesticides reduces consumption and minimizes environmental impact.
  • Reduces labor costs and allows for continuous operation, even in challenging weather or field conditions.
Warehouse/Logistics Modern warehouses require AMRs to navigate complex environments, avoid obstacles, and optimize inventory movement in real time.
  • Multicamera integration—Supports multiple, high res cameras with 360-degree situational awareness.
  • Lower latency processing—Real-time decision for dynamic path planning and object recognition.
  • Rugged design—Industrial-grade hardware ensures reliable operation in fast-paced, high vibration conditions.
  • Scalable platform—Customized to fit AMRs of different sizes and use cases.

ADI GMSL: REAL-TIME SENSOR AND PERCEPTION DATA THROUGH A SINGLE CHANNEL

Real-time sensor interface with data visualizations for smart warehouse automation and inventory tracking

ADI’s GMSL3 is a high speed, SERDES solution that transmits ultrahigh resolution video, audio, control, and power over a single cable with microsecond latency. Supporting up to 12 Gbps per lane, it simplifies system design while enabling real-time, AI-driven vision in automation, robotics, agriculture, and manufacturing. All GMSL parts are also AECQ-100 automotive-grade.

Camera/Sensor To Processor

Diagram of camera sensor system transmitting visual data to processor for AI-powered warehouse analysis

Processor to Display

Visual flowchart showing data transfer from processor to display in smart warehouse monitoring system

GMSL3 supports complex video routing, ASIL-B functional safety support, and diagnostics, while meeting strict EMI/EMC standards for enhanced safety. Its low latency and precise synchronization help power autonomous navigation, defect detection, and precision pick-and-place. Deployed in millions of automotive links, GMSL3 is scalable and ready for industrial, healthcare, aerospace, and consumer applications—driving smarter decision-making, reducing downtime, and improving safety and sustainability.

GMSL CONNECTIVITY TECHNOLOGY BENEFITS

Reduce Cabling Infrastructure

  • Up to 12 Gbps over a single wire
  • Simultaneous transmission of video, control, and audio topology
  • Sensor data aggregation (video, audio, LIDAR, radar, etc.)
  • Video splitting
  • Power over coax
  • Low latency and low bit error

Scalable System Design

  • Interoperability, highly configurable
  • Pin compatible for 3 Gbps/6 Gbps/12 Gbps speed options
  • Backward compatible with previous GMSL generation

Supports Highest Resolutions

  • Up to 15 MP camera, 4k+ displays

Safety, Security, and Sustainability

  • Real-time link diagnostics, data integrity checks
  • Real-time, adaptive equalization
  • Meets stringent EMI/EMC requirements
  • ASIL-B functional safety rated options

The Value of GMSL

•  High bandwidth data transfer with bidirectional control and power
•  Single wire solution, reducing cable infrastructure
•  Easily integrate multiple sensors
•  Low bit error and low deterministic latency (in microseconds)
•  ASIL-B reliable solution with many robust error monitoring tools
•  Real-time, adaptive equalization

VISION AND CONNECTIVITY TECHNOLOGIES FOR ADVANCED, INDUSTRIAL AUTONOMY

Person using tablet to monitor automated warehouse robots sorting packages via smart vision system

As manufacturers continue to face staffing challenges, evolving regulations, rising productivity demands, and rapid AI advancements, Connect Tech and ADI have risen to the challenge. Leveraging the GMSL3 connectivity solution has enabled Connect Tech to help bridge the gap between increasingly complex vision technology and the need for reliable, high performance , and adaptable AMRs, especially in challenging environments, like industrial manufacturing.


References

1 “2024 State of Warehouse Labor Report.” Instawork.

2 “Creating Pathways for Tomorrow’s Workforce Today: Beyond Reskilling in Manufacturing.” Deloitte Insights, Manufacturing Institute, May 2021.