High-Frequency Noise in the Buck Regulator VOUT Ripple Measurement

Jun 7 2026

Figure 1

   

Key Takeaways

  • Your probe may be the problem. Vertical placement acts as an antenna, capturing up to 8x more radiated flux—making VOUT ripple appear far worse than reality.
  • Inductor parasitics and fast switching transients generate hundreds-of-MHz noise spikes. If they align with your ADC or FPGA clock, expect failures—learn to isolate real ripple from artifacts.

Abstract

Switch-mode power supplies have excellent efficiencies and high-power capabilities compared with low-dropout (LDO) regulators. But at the same time, the fast switching transients of power FETs induce electromagnetic noise radiating to the surroundings. These radiated noises could be picked up when measuring output voltage ripples, shown as high-frequency noises. An improper setup may compromise the performance of the switch-mode power supply. This article analyzes the root cause of high-frequency noises shown during the voltage measurement and explains whether this noise is a real concern for customers. The Ansys Maxwell simulation is used to emulate the radiated flux distribution around the power supply to visualize the effect. Furthermore, this article proposes a method to measure real output voltage ripples on the circuit and identify the potential issue caused by high-frequency noises.

Introduction

In many applications, a switch-mode power supply is the only choice because of its excellent performance like high efficiency and high power capability. A buck step-down power converter is the most popular topology adopted in a variety of applications. The switching characteristics controlled by pulse width modulation (PWM) help to regulate power transfer. But at the same time, the fast switching transients of power FETs within several nanoseconds or tens of nanoseconds could induce high-frequency noises. For example, in noise-sensitive applications, if the high-frequency voltage spikes caused by the power supply are aligned with the clock signal, it will cause failure or malfunction of the load devices such as ADCs, ASICs, or FPGAs. So, it is important to understand the root causes of high-frequency noises, identify the noise issues, and then find the potential solution to attenuate or eliminate the influence of high-frequency noises. The correct noise/ripple measurement method is critical.

Typical VOUT Ripple in a Buck Converter

For a typical buck converter, the inductor and the capacitor work as a filter to provide the conductive path for the AC signal generated by the switching action. The inductor current contains the AC component and the DC component. Most of the AC components will flow into the output capacitor, and the DC component will only flow into the load. Without considering component parasitics as shown in Figure 1a, the output voltage ripple across the output capacitor is a smooth waveform shown in Figure 1b.

Buck Converter Circuit And Switching Waveforms
Figure 1. Simplified buck converter: (a) circuit without parasitics; (b) switching waveforms.

If considering the parasitic resistance and the parasitic inductance of the output capacitors in Figure 2a, the output voltage ripple could change significantly as shown in Figure 2b.

Output Capacitor Parasitic Parameters And Voltage Waveforms
Figure 2. Output capacitor with parasitic parameters: (a) simplified circuit; (b) output voltage waveforms.

The AC components of the waveform in Figure 2b are mainly distributed around the switching frequency, which is around hundreds of kHz to several MHz. But the actual output voltage in the test will usually show some even higher frequency components, which are around hundreds of MHz. The parasitic capacitor of the power inductor could provide the conductive path for these hundreds of MHz signals from the switching node to the output as shown in Figure 3.

Output Voltage Ripple Inductor Parasitic Capacitance
Figure 3. Output voltage ripple considering the parasitic capacitance of the inductor: (a) conductive path from switching node to output; (b) switching waveforms.

An example of the output voltage measurement based on the LTM4628 µModule® buck regulator is shown in Figure 4a. The switching frequency waveform and the high-frequency spikes can be easily observed. But when changing the position of the probe from vertical to horizontal to the board, the measured output voltage ripple reduced from 54mV to 42mV as shown in Figure 4b. Figure 5 shows how the output voltage is measured. If only considering the output voltage ripple generated on the conductive path, the measurement result should not change with the probe position. Meanwhile, the high-frequency noise captured by the probe is aligned with the switching actions. So, the additional high-frequency noise captured by the probe could be the radiation noise induced by high di/dt in the hot loop during the fast switching transient.

Output Voltage Ripple Measurement Setup Probe Orientation
Figure 4. Measured output voltage ripple on the LTM4628 with the general passive probe: (a) probe vertical to the demo board; (b) probe horizontal to the demo board.
 
Output Voltage Ripple Measurement Setup Probe Orientation
Figure 5. Output voltage ripple measurement setup: (a) probe vertical to the demo board; (b) probe horizontal to the demo board.

To further verify the presence of these differences caused by the probe position, the different probes are applied to measure the output voltage ripple, including a general probe, a BNC cable, and an active differential probe, shown in Figure 6. As shown in the figure, the general probe needs the extra spring as the ground return path, which means the measurement loop is larger.

Probe Types General BNC Differential
Figure 6. Different probes: (a) general probe; (b) BNC cable; (c) differential probe.

The measurement results with different probes are provided in Table 1. Compared with the vertical probe measurement, the horizontal probe measurement always shows the lower high-frequency spike. Also, the measurement result of the horizontal method based on the general probe is higher than the BNC cable and the differential probe.

Table 1. Output Voltage Ripple Measured by Different Probes with Vertical and Horizontal Measurement Methods
Probe Position Vertical to Demo Board Horizontal to Demo Board
 General Probe 54mV  42mV
 BNC Cable (50Ω Termination) 48mV 28mV
 Differential Probe 114mV 28mV

To understand the unexpected phenomena during the output voltage ripple measurement, the Maxwell simulation model is developed as shown in Figure 7a based on the simplified LTM4628 physical structure. Hot loop 1 is formed by the MOSFETs and the internal input capacitors inside the module. Hot loop 2 is composed of the MOSFETs and the external input capacitors near the module on the demo board. The conceptual currents at 300MHz are injected into both hot loop 1 and hot loop 2 to emulate the high di/dt in the hot loop during the switching transient. Figure 7b shows the H field distribution around the module. The H field is much stronger in the module surrounding the area on the top of the demo board, which indicates the flux generated by the hot loop could be easily captured by the probe measurement loop.

Maxwell FEA Simulation Model H Field Distribution
Figure 7. Maxwell finite element analysis (FEA) simulation: (a) simulation model; (b) H field distribution.

As for the root cause of the different results by different probe positions, the zoomed-in H field distribution is provided in Figure 8 for a more detailed explanation. In Figure 8, the equivalent vertical measurement loop surface can capture around 8× more flux than the horizontal measurement loop surface. This is because the demo board with a thick copper polygon provides the attenuation to the high-frequency flux to prevent the flux from going through. So, most of the flux will flow horizontally along the demo board surface.

Flux Distribution Output Capacitors
Figure 8. Detailed flux distribution around the output capacitors.

Figure 9 shows a more straightforward illustration of how the vertical measurement loop captures more flux generated by the hot loop. The positive tip, the negative or ground tip, and the return path inside the probe form a loop like an antenna that could capture the high-frequency flux surrounding the switching regulators.

Radiation Noise Vout Measurement Loop
Figure 9. Extra radiation noise captured by the VOUT measurement loop.

To further verify this concept, the same probe with the shielding is also used to measure the VOUT ripple as shown in Figure 10. A copper foil is manually rotated around the differential probe to form a shielding layer. The probe is also vertical to the demo board.

Vout Measurement Differential Probe Shielding Comparison
Figure 10. VOUT measurement with differential probe: (a) no shielding; (b) with copper foil shielding.

As a result, with the shielded probe, the high-frequency noise is much reduced in Figure 10b compared with the unshielded measurement in Figure 10a. Except for the high-frequency noise, the switching frequency ripples in both figures are quite similar. Also, as discussed based on Figure 3, there will be high-frequency ripple across the output capacitor because of the parasitic capacitor of the inductor like the waveform in Figure 10b.

Vout Measurement Result Shielding Vs No Shielding
Figure 11. VOUT measurement result: (a) 114.4mV without shielding; (b) 27.2mV with shielding.

Conclusion

The fast switching transient induces the high di/dt in the hot loop. For the output voltage ripple of a buck converter, there will be high-frequency noise caused by this high di/dt through the conductive path formed by the parasitic capacitor of the inductor.

But in the real VOUT ripple measurement, there will be even higher frequency noise captured, which is also aligned with the switching actions. This extra ripple is the radiation noise also caused by the high di/dt in the hot loop. And the high-frequency spike can vary with the position of the probe on the demo board. The Ansys simulation proves that the vertical measurement configuration can capture much higher-frequency flux generated by the hot loop than the horizontal configuration.

To further verify this theory, the VOUT ripple is also measured by the shielded probe. The high-frequency noise is much reduced by the shielded probe than the nonshielded probe result, which turns out there will be additional radiational high-frequency noise captured by the probe. The real VOUT ripple presenting across the COUT on the board will be smaller than the VOUT ripple measured by the probes.

 

About the Authors

Yu Yan
Yu Yan received his Ph.D. degree in electrical engineering from the University of Tennessee. He joined Analog Devices in 2022 as an application engineer. His expertise includes DC-to-DC converters, AC-to-DC converters, and
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Technology Solutions
Product Categories